proc PortConfigStaticLanHlt { port portConfigParams } { # This API is for scaling L2 only and without Protocol Interface config. # No protocol configurations on the host. upvar $portConfigParams params # Starting with HLT version 4.81, it requires this new parameter #set paramList {-lan_range_count 1 } foreach {properties values} [array get params $port,*] { set property [lindex [split $properties ,] end] append paramList "$property $values " } puts "\nPortConfigStaticLanHlt: $port" set interfaceConfigStatus [eval ::ixia::interface_config $paramList] if {[keylget interfaceConfigStatus status] != $::SUCCESS} { puts "\nError PortConfigStaticLan:\n$interfaceConfigStatus\n" return 1 } # ::ixNet::OBJ-/vport:1/protocols/static/lan:1 set interfaceHandle [keylget interfaceConfigStatus interface_handle] return $interfaceHandle }