def configDhcpServerV4(self, obj, **kwargs): """ Description Create or modify DHCP v4 Server in NGPF. To create a new DCHP v4 server stack in NGPF, pass in the IPv4 object. To modify an existing DHCP V4 server stack in NGPF, pass in the dhcpv4server object. Parameters obj: : To create new DHCP: /api/v1/sessions/1/ixnetwork/topology/1/deviceGroup/1/ethernet/1/ipv4/1 obj: : To modify DHCP server: /api/v1/sessions/1/ixnetwork/topology/1/deviceGroup/1/ethernet/1/ipv4/1/dhcpv4server/1 useRapidCommit: : Default=False multiplier: : Default-1 subnetAddrAssign: : Default=False