def performGenericOperation(connection, url, payloadDict): ''' This will perform a generic operation on the given url, it will wait for it to finish. Args: - connection is the connection object that manages the HTTP data transfers between the client and the REST API - url is the address of where the operation will be performed - payloadDict is the python dict with the parameters for the operation ''' data = json.dumps(payloadDict) reply = connection.httpPost(url=url, data=data) if not reply.ok: raise Exception(reply.text) waitForActionToFinish(connection, reply, url) return reply