################################################################################# # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 12-09-2005 LRaicea # ################################################################################# ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures a PPPoE tunnel with 20 sessions between the # # SRC port and the DUT. Traffic is sent bidirectional. After that a few statistics are being retrieved. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # # ################################################################################ ################################################################################ # DUT configuration: # # # no aaa new-model # vpdn enable # # VPDN configuration 1: # # bba-group pppoe global # # virtual-template 16 # # sessions per-vc limit 1000 # # sessions per-mac limit 1000 # # or # # VPDN configuration 2: # # vpdn-group 1 # # accept-dialin # # protocol pppoe # # virtual-template 16 # # ip multicast-routing # # ip local pool pppoe 16.16.16.2 16.16.16.254 # # interface FastEthernet2/0 # ip address 16.16.16.1 255.255.255.0 # ip pim dense-mode # ip igmp version 2 # no ip route-cache cef # no ip route-cache # pppoe enable # no shutdown # # interface FastEthernet4/0 # ip address 18.18.18.1 255.255.255.0 # ip pim dense-mode # ip igmp version 2 # no ip route-cache cef # no ip route-cache # no shutdown # # interface Virtual-Template16 # mtu 1492 # ip unnumbered FastEthernet2/0 # ip pim version 1 # ip pim dense-mode # peer default ip address pool pppoe # ppp ipcp address required # no keepalive # ppp max-bad-auth 20 # ppp timeout retry 10 # # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 8/1 8/2] set sess_count 20 # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set port_src_handle [lindex $port_handle 0] set port_dst_handle [lindex $port_handle 1] puts "Ixia port handles are $port_handle " ######################################## # Configure SRC interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_src_handle \ -mode config \ -speed ether100 \ -phy_mode copper \ -autonegotiation 1 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ######################################## # Configure DST interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_dst_handle \ -mode config \ -speed ether100 \ -phy_mode copper \ -autonegotiation 1 \ -intf_ip_addr 18.18.18.18 \ -gateway 18.18.18.1 \ -netmask 255.255.255.0 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ######################################### # Configure sessions # ######################################### set config_status [::ixia::pppox_config \ -port_handle $port_src_handle \ -protocol pppoe \ -encap ethernet_ii \ -num_sessions $sess_count \ -disconnect_rate 10 \ -auth_req_timeout 10 \ -enable_multicast 1 \ -mc_group_id mcGroupId \ -start_group_ip 225.1.0.1 \ -group_ip_count 5 \ -group_ip_step 0.1.0.1 \ -igmp_version IGMPv2 \ -watch_duration 60 ] if {[keylget config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget config_status log]" } set pppox_handle [keylget config_status handle] puts "Ixia pppox_handle is $pppox_handle " ######################################### # Connect sessions # ######################################### set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action connect ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } puts "Sessions going up..." set pppoe_attempts 0 set pppoe_sessions_up 0 while {($pppoe_attempts < 20) && ($pppoe_sessions_up < $sess_count)} { after 10000 set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] puts "pppoe_sessions_up=$pppoe_sessions_up" incr pppoe_attempts } if {$pppoe_sessions_up < $sess_count} { return "FAIL - $test_name - Not all sessions are up." } set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_src_handle \ -emulation_src_handle $pppox_handle \ -ip_src_mode emulation ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_dst_handle \ -emulation_dst_handle $pppox_handle \ -ip_dst_mode emulation ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ######################################### # Configure traffic # ######################################### set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_src_handle \ -port_handle2 $port_dst_handle \ -bidirectional 1 \ -l3_protocol ipv4 \ -ip_src_mode emulation \ -ip_src_count $sess_count \ -emulation_src_handle $pppox_handle \ -ip_dst_mode fixed \ -ip_dst_addr 18.18.18.18 \ -l3_length 1000 \ -rate_percent 1 \ -transmit_mode continuous \ -mac_dst_mode discovery \ -ip_precedence 4 \ -ip_cost 0 \ -ip_delay 0 \ -ip_reliability 0 \ -ip_reserved 0 \ -ip_throughput 0 \ -enable_voice 1 \ -enable_data 1 \ -voice_tos 64 \ -data_tos 32 \ -duration 60 ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ######################################### # Clear traffic stats # ######################################### set control_status [::ixia::traffic_control \ -port_handle $port_handle \ -action clear_stats ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } puts "Starting to transmit traffic over tunnels..." ######################################### # Start traffic # ######################################### set control_status [::ixia::traffic_control \ -port_handle $port_handle \ -action run ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } after 30000 puts "Ixia multicast stats ... " ######################################### # Retrieve multicast stats # ######################################### set session_status [::ixia::emulation_igmp_info \ -port_handle $port_src_handle \ -mode all \ -type igmp_over_ppp ] if {[keylget session_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget session_status log]" } set mcAddresses [keylkeys session_status $port_src_handle.igmpoppp.group] set key $port_src_handle.igmpoppp.group puts [format "%15s %15s %15s %15s %15s %15s %15s" \ "Mc Addr" \ "Min Join Lat" \ "Max Join Lat" \ "Avg Join Lat" \ "Min Leave Lat" \ "Max Leave Lat" \ "Avg Leave Lat" ] foreach {mcAddr} $mcAddresses { regsub -all { } $mcAddr {.} mcAddress puts [format "%15s %15s %15s %15s %15s %15s %15s" \ $mcAddress \ [keylget session_status $key.$mcAddr.rx.min_join_latency ] \ [keylget session_status $key.$mcAddr.rx.max_join_latency ] \ [keylget session_status $key.$mcAddr.rx.avg_join_latency ] \ [keylget session_status $key.$mcAddr.rx.min_leave_latency ] \ [keylget session_status $key.$mcAddr.rx.max_leave_latency ] \ [keylget session_status $key.$mcAddr.rx.avg_leave_latency ]] } set key $port_src_handle.igmpoppp.aggregate set mc_groups_query_rx [keylget session_status $key.rx.mc_groups_query] set mc_groups_query_tx [keylget session_status $key.tx.mc_groups_query] set mc_groups_report_rx [keylget session_status $key.rx.mc_groups_report] set mc_groups_report_tx [keylget session_status $key.tx.mc_groups_report] set mc_groups_leave [keylget session_status $key.tx.mc_groups_leave] puts "\nIGMPoPPP aggregate statistics:" puts " Groups Query RX = $mc_groups_query_rx" puts " Groups Query TX = $mc_groups_query_tx" puts " Groups Report RX = $mc_groups_report_rx" puts " Groups Report TX = $mc_groups_report_tx" puts " Groups Leave = $mc_groups_leave" after 30000 ######################################### # Retrieve multicast stats # ######################################### set session_status [::ixia::emulation_igmp_info \ -port_handle $port_src_handle \ -mode all \ -type igmp_over_ppp ] if {[keylget session_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget session_status log]" } set mcAddresses [keylkeys session_status $port_src_handle.igmpoppp.group] set key $port_src_handle.igmpoppp.group puts [format "%15s %15s %15s %15s %15s %15s %15s" \ "Mc Addr" \ "Min Join Lat" \ "Max Join Lat" \ "Avg Join Lat" \ "Min Leave Lat" \ "Max Leave Lat" \ "Avg Leave Lat" ] foreach {mcAddr} $mcAddresses { regsub -all { } $mcAddr {.} mcAddress puts [format "%15s %15s %15s %15s %15s %15s %15s" \ $mcAddress \ [keylget session_status $key.$mcAddr.rx.min_join_latency ] \ [keylget session_status $key.$mcAddr.rx.max_join_latency ] \ [keylget session_status $key.$mcAddr.rx.avg_join_latency ] \ [keylget session_status $key.$mcAddr.rx.min_leave_latency ] \ [keylget session_status $key.$mcAddr.rx.max_leave_latency ] \ [keylget session_status $key.$mcAddr.rx.avg_leave_latency ]] } set key $port_src_handle.igmpoppp.aggregate set mc_groups_query_rx [keylget session_status $key.rx.mc_groups_query] set mc_groups_query_tx [keylget session_status $key.tx.mc_groups_query] set mc_groups_report_rx [keylget session_status $key.rx.mc_groups_report] set mc_groups_report_tx [keylget session_status $key.tx.mc_groups_report] set mc_groups_leave [keylget session_status $key.tx.mc_groups_leave] puts "\nIGMPoPPP aggregate statistics:" puts " Groups Query RX = $mc_groups_query_rx" puts " Groups Query TX = $mc_groups_query_tx" puts " Groups Report RX = $mc_groups_report_rx" puts " Groups Report TX = $mc_groups_report_tx" puts " Groups Leave = $mc_groups_leave" ######################################### # Stop traffic # ######################################### set control_status [::ixia::traffic_control \ -port_handle $port_handle \ -action stop ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } ######################################### # Retrieve SRC aggregate traffic stats # ######################################### set aggr_stats [::ixia::traffic_stats -port_handle $port_src_handle] if {[keylget aggr_stats status] == $::FAILURE} { return "FAIL - $test_name - [keylget aggr_stats log]" } set aggr_tx [keylget aggr_stats $port_src_handle.aggregate.tx.pkt_count ] puts "Port $port_src_handle Tx count Results = $aggr_tx frames " set aggr2_stats [::ixia::traffic_stats \ -port_handle $port_src_handle \ -mode igmp_over_ppp ] if {[keylget aggr2_stats status] == $::FAILURE} { return "FAIL - $test_name - [keylget aggr2_stats log]" } set key $port_src_handle.igmpoppp set mc_total_bytes_rx [keylget aggr2_stats $key.rx.mc_total_bytes] set mc_total_bytes_tx [keylget aggr2_stats $key.tx.mc_total_bytes] set mc_total_frames_rx [keylget aggr2_stats $key.rx.mc_total_frames] set mc_total_frames_tx [keylget aggr2_stats $key.tx.mc_total_frames] puts "\nIGMPoPPP aggregate statistics $port_src_handle:" puts " Total Bytes RX = $mc_total_bytes_rx" puts " Total Bytes TX = $mc_total_bytes_tx" puts " Total Frames RX = $mc_total_frames_rx" puts " Total Frames TX = $mc_total_frames_tx" ######################################### # Retrieve DST aggregate traffic stats # ######################################### set aggr_stats [::ixia::traffic_stats -port_handle $port_dst_handle] if {[keylget aggr_stats status] == $::FAILURE} { return "FAIL - $test_name - [keylget aggr_stats log]" } set aggr_rx [keylget aggr_stats $port_dst_handle.aggregate.rx.raw_pkt_count ] puts "Port $port_dst_handle Rx count Results = $aggr_rx frames " ######################################### # Retrieve aggregate session stats # ######################################### set aggr_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget aggr_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggr_status log]" } set sess_num [keylget aggr_status aggregate.num_sessions] set sess_count_up [keylget aggr_status aggregate.connected] set sess_min_setup [keylget aggr_status aggregate.min_setup_time] set sess_max_setup [keylget aggr_status aggregate.max_setup_time] set sess_avg_setup [keylget aggr_status aggregate.avg_setup_time] puts "Ixia Test Results ... " puts " Number of sessions = $sess_num " puts " Number of connected sessions = $sess_count_up " puts " Minimum Setup Time (ms) = $sess_min_setup " puts " Maximum Setup Time (ms) = $sess_max_setup " puts " Average Setup Time (ms) = $sess_avg_setup " ######################################### # Disconnect sessions # ######################################### if {1} { puts "Disconnecting $sess_count_up sessions. " set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action disconnect ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } } set control_status [::ixia::cleanup_session \ -handle $port_handle ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"