################################################################################# # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2007 by IXIA # All Rights Reserved. # # Revision Log: # 05-22-2007 LRaicea # ################################################################################# ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures a PPPoE tunnel with 20 sessions between the # # SRC port and the DUT. The flapping of the sessions is started. # # After that a few statistics are being retrieved. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # # ################################################################################ ################################################################################ # DUT configuration: # # # # aaa new-model # # aaa authentication ppp default none # # aaa session-id common # # # # vpdn enable # # # # bba-group pppoe global # # virtual-template 1 # # sessions per-vc limit 1000 # # sessions per-mac limit 1000 # # # # interface Loopback1 # # ip address 10.10.10.1 255.255.255.0 # # # # ip local pool pppoe 10.10.10.2 10.10.10.254 # # # # interface FastEthernet1/0 # # no ip address # # no ip route-cache cef # # no ip route-cache # # duplex half # # pppoe enable # # no shut # # # # interface FastEthernet3/0 # # ip address 11.11.11.1 255.255.255.0 # # duplex half # # no shut # # # # interface Virtual-Template1 # # mtu 1492 # # ip unnumbered Loopback1 # # peer default ip address pool pppoe # # no keepalive # # ppp max-bad-auth 20 # # ppp timeout retry 10 # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 4/3] set sess_count 20 # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set port_src_handle [lindex $port_handle 0] ixPuts "Ixia port handles are $port_handle " ################################################################################ # Configure source interface in the test ################################################################################ set interface_status [::ixia::interface_config \ -port_handle $port_src_handle \ -mode config \ -speed auto \ -duplex auto \ -phy_mode copper \ -autonegotiation 1 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ################################################################################ # Configure PPPoE sessions ################################################################################ set flap_rate [expr $sess_count / 2] set flap_repeat_count 3 set flap_hold_time 30 set flap_cool_off_time 10 set config_status [::ixia::pppox_config \ -port_handle $port_src_handle \ -protocol pppoe \ -encap ethernet_ii \ -num_sessions $sess_count \ -auth_req_timeout 10 \ -disconnect_rate $flap_rate \ -attempt_rate $flap_rate \ -flap_rate $flap_rate \ -flap_repeat_count $flap_repeat_count \ -hold_time $flap_hold_time \ -cool_off_time $flap_cool_off_time ] if {[keylget config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget config_status log]" } set pppox_handle [keylget config_status handle] ixPuts "Ixia pppox_handle is $pppox_handle " ################################################################################ # Start flapping sessions ################################################################################ set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action start_flapping ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } ixPuts "Sessions going up..." set pppoe_attempts 0 set pppoe_sessions_up 0 set pppoe_retries 60 while {($pppoe_attempts < $pppoe_retries) && ($pppoe_sessions_up < $sess_count)} { set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] ixPuts "Sessions up: $pppoe_sessions_up ..." after 1000 } for {set num_flap 0} {$num_flap < $flap_repeat_count} {incr num_flap} { ixPuts "" ixPuts "" ixPuts "-------------------- Flap Iteration [expr $num_flap + 1] -------------------- " ixPuts "Hold sessions up for ${flap_hold_time} (s)..." set pppoe_attempts 0 set pppoe_retries 60 ixPuts -nonewline "Sessions up - $pppoe_sessions_up" while {($pppoe_attempts < $pppoe_retries) && ($pppoe_sessions_up >= $sess_count)} { set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] ixPuts -nonewline " - $pppoe_sessions_up" after 500 } ixPuts " sessions ..." ixPuts "Started to teardown sessions ..." set pppoe_attempts 0 set pppoe_retries 60 ixPuts -nonewline "Sessions up - $pppoe_sessions_up" while {($pppoe_attempts < $pppoe_retries) && ($pppoe_sessions_up > 0)} { set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] ixPuts -nonewline " - $pppoe_sessions_up" after 500 } ixPuts " sessions ..." ixPuts "Teardown successful ..." ixPuts "Hold sessions down for ${flap_cool_off_time} (s) ..." set pppoe_attempts 0 set pppoe_retries 60 ixPuts -nonewline "Sessions up - $pppoe_sessions_up" while {($pppoe_attempts < $pppoe_retries) && ($pppoe_sessions_up < 1)} { set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] ixPuts -nonewline " - $pppoe_sessions_up" after 500 } ixPuts " sessions ..." ixPuts "Started to setup sessions ..." set pppoe_attempts 0 set pppoe_retries 60 ixPuts -nonewline "Sessions up - $pppoe_sessions_up" while {($pppoe_attempts < $pppoe_retries) && ($pppoe_sessions_up < $sess_count)} { set pppox_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget pppox_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_status log]" } set aggregate_stats [keylget pppox_status aggregate] set pppoe_sessions_up [keylget aggregate_stats sessions_up] ixPuts -nonewline " - $pppoe_sessions_up" after 500 } ixPuts " sessions ..." } ################################################################################ # Stop flapping ################################################################################ ixPuts "Disconnecting $pppoe_sessions_up sessions. " set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action stop_flapping ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } ::ixia::cleanup_session -port_handle $port_handle return "SUCCESS - $test_name - [clock format [clock seconds]]"