################################################################################# # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 12-08-2005 LRaicea # ################################################################################# ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures a PPPoE tunnel with 5 sessions. # # Then it connects to the DUT(Cisco7206) and retrieves a few statistics. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # # ################################################################################ ################################################################################ # DUT configuration: # # # # aaa new-model # # aaa authentication ppp default none # # aaa session-id common # # # # vpdn enable # # # # bba-group pppoe global # # virtual-template 1 # # sessions per-vc limit 1000 # # sessions per-mac limit 1000 # # # # interface Loopback1 # # ip address 10.10.10.1 255.255.255.0 # # # # ip local pool pppoe 10.10.10.2 10.10.10.254 # # # # interface FastEthernet1/0 # # no ip address # # no ip route-cache cef # # no ip route-cache # # duplex half # # pppoe enable # # no shut # # # # interface Virtual-Template1 # # mtu 1492 # # ip unnumbered Loopback1 # # peer default ip address pool pppoe # # no keepalive # # ppp max-bad-auth 20 # # ppp timeout retry 10 # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 4/1] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [keylget connect_status port_handle.$chassisIP.$port_list] ################################################ # Configure session # ################################################ set pppox_config_status [::ixia::pppox_config \ -port_handle $port_handle \ -protocol pppoe \ -encap ethernet_ii \ -num_sessions 5 \ -auth_req_timeout 10 \ -auth_mode none \ ] if {[keylget pppox_config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_config_status log]" } set pppox_handle [keylget pppox_config_status handle] ################################################ # Setup session # ################################################ set pppox_control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action connect \ ] if {[keylget pppox_control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pppox_control_status log]" } after 10000 ################################################ # Stats # ################################################ set aggr_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode aggregate ] if {[keylget aggr_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggr_status log]" } set sess_num [keylget aggr_status aggregate.num_sessions] set sess_count_up [keylget aggr_status aggregate.connected] set sess_min_setup [keylget aggr_status aggregate.min_setup_time] set sess_max_setup [keylget aggr_status aggregate.max_setup_time] set sess_avg_setup [keylget aggr_status aggregate.avg_setup_time] puts "Ixia Test Results ... " puts " Number of sessions = $sess_num " puts " Number of connected sessions = $sess_count_up " puts " Minimum Setup Time (ms) = $sess_min_setup " puts " Maximum Setup Time (ms) = $sess_max_setup " puts " Average Setup Time (ms) = $sess_avg_setup " set session_status [::ixia::pppox_stats \ -handle $pppox_handle \ -mode session ] if {[keylget session_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget session_status log]" } set sessionIdList [keylkeys session_status session] puts "Ixia per session stats ... " foreach sessid $sessionIdList { if {![catch {set per_sess_ipcp_cfg_req_tx \ [keylget session_status \ session.${sessid}.ipcp_cfg_req_tx]}]} { puts "Session $sessid IPCP CFG ReQ Tx Count =\ $per_sess_ipcp_cfg_req_tx " } else { puts "Session $sessid IPCP CFG ReQ Tx Count = N/A " } } return "SUCCESS - $test_name - [clock format [clock seconds]]"