################################################################################ # Version 1.0 $Revision: 1 $ # # Copyright © 1997 - 2006 by IXIA # All Rights Reserved. # # Revision Log: # 7-24-2007 : Mircea Hasegan # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures a PPPoE tunnel with 100 sessions between the # # SRC port and the DST port. Vlan and Authentication with wildcards are used# # After that a statistics are being retrieved. # # Traffic is sent over the tunnel and the DUT sends # # it to the DST port. After that a few statistics are being retrieved. # # # # Module: # # The sample was tested on a LM1000STXS4 module . # # # ################################################################################ ################################################################################ # DUT configuration: # # conf t # aaa new-model # aaa authentication ppp default local # aaa session-id common # end # # tclsh # conf t # for {set pound 1; set question 1} {$pound < 101} {incr pound} { # username ixia${pound}${question} password 0 pwd${pound}${question} # if {$question == 10} { # set question 1 # } else { # incr question # } # } # end # tclquit # # conf t # # vpdn enable # bba-group pppoe global # virtual-template 20 # sessions per-vc limit 1000 # sessions per-mac limit 1000 # # interface Loopback20 # ip address 20.20.1.1 255.255.0.0 # # interface gigabitEthernet 0/2 # no ip address # duplex full # no shutdown # # interface gigabitEthernet 0/2.100 # encapsulation dot1Q 100 # no ip route-cache # pppoe enable # # interface gi 0/3 # ip address 11.11.11.1 255.255.255.0 # duplex half # no shut # # interface Virtual-Template20 # mtu 1492 # ip unnumbered Loopback20 # peer default ip address pool pppoe_vlan_pool # no keepalive # ppp max-bad-auth 20 # ppp timeout retry 10 # ppp authentication chap pap # # ip local pool pppoe_vlan_pool 20.20.1.2 20.20.255.254 # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 3/3 3/4] set sess_count 100 # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -ixnetwork_tcl_server localhost \ -device $chassisIP \ -port_list $port_list ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set port_src_handle [lindex $port_handle 0] set port_dst_handle [lindex $port_handle 1] puts "Ixia port handles are $port_handle " ######################################## # Configure SRC interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_src_handle \ -mode config \ -speed ether100 \ -phy_mode copper \ -autonegotiation 1 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ######################################## # Configure DST interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_dst_handle \ -mode config \ -speed ether100 \ -phy_mode copper \ -autonegotiation 1 \ -intf_ip_addr 11.11.11.110 \ -gateway 11.11.11.1 \ -netmask 255.255.255.0 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set int_handle [keylget interface_status interface_handle] ######################################### # Configure sessions # ######################################### set config_status [::ixia::pppox_config \ -mode add \ -port_handle $port_src_handle \ -protocol pppoe \ -encap ethernet_ii_vlan \ -num_sessions $sess_count \ -port_role access \ -disconnect_rate 10 \ -redial 1 \ -redial_max 10 \ -redial_timeout 20 \ -ip_cp ipv4_cp \ -vlan_id 100 \ -vlan_id_count 1 \ -auth_mode pap_or_chap \ -username "ixia#?"\ -password "pwd#?" \ -username_wildcard 1 \ -password_wildcard 1 \ -wildcard_pound_start 1 \ -wildcard_pound_end 100 \ -wildcard_question_start 1 \ -wildcard_question_end 10 \ ] if {[keylget config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget config_status log]" } set pppox_handle [keylget config_status handle] puts "Ixia pppox_handle is $pppox_handle " ######################################### # Connect sessions # ######################################### set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action connect ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } puts "Sessions..." ######################################### # Retrieve aggregate session stats # ######################################### set aggr_status [::ixia::pppox_stats \ -port_handle $port_src_handle\ -mode aggregate ] if {[keylget aggr_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggr_status log]" } set sess_num [keylget aggr_status ${port_src_handle}.aggregate.num_sessions] set sess_count_up [keylget aggr_status ${port_src_handle}.aggregate.connected] set sess_min_setup [keylget aggr_status ${port_src_handle}.aggregate.min_setup_time] set sess_max_setup [keylget aggr_status ${port_src_handle}.aggregate.max_setup_time] set sess_avg_setup [keylget aggr_status ${port_src_handle}.aggregate.avg_setup_time] set sess_num [keylget aggr_status ${port_src_handle}.aggregate.num_sessions] set chap_auth_fail_tx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_fail_tx] set chap_auth_succ_tx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_succ_tx] set chap_auth_rsp_rx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_rsp_rx] set chap_auth_chal_rx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_chal_rx] set chap_auth_fail_rx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_fail_rx] set chap_auth_succ_rx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_succ_rx] set chap_auth_rsp_tx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_rsp_tx] set chap_auth_chal_tx [keylget aggr_status ${port_src_handle}.aggregate.chap_auth_chal_tx] set pap_auth_ack_rx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_ack_rx] set pap_auth_nak_tx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_nak_tx] set pap_auth_req_rx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_req_rx] set pap_auth_ack_tx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_ack_tx] set pap_auth_nak_rx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_nak_rx] set pap_auth_req_tx [keylget aggr_status ${port_src_handle}.aggregate.pap_auth_req_tx] puts "Ixia Test Results ... " puts " Number of sessions = $sess_num " puts " Number of connected sessions = $sess_count_up " puts " Minimum Setup Time (ms) = $sess_min_setup " puts " Maximum Setup Time (ms) = $sess_max_setup " puts " Average Setup Time (ms) = $sess_avg_setup " puts "" puts " Chap Auth Fail TX = $chap_auth_fail_tx " puts " Chap Auth Fail RX = $chap_auth_fail_rx " puts " Chap Auth Succ TX = $chap_auth_succ_tx " puts " Chap Auth Succ RX = $chap_auth_succ_rx " puts " Chap Auth Rsp TX = $chap_auth_rsp_tx " puts " Chap Auth RSP RX = $chap_auth_rsp_rx " puts " Chap Auth Chal TX = $chap_auth_chal_tx " puts " Chap Auth Chal RX = $chap_auth_chal_rx " puts "" puts " Pap Auth Ack TX = $pap_auth_ack_tx " puts " Pap Auth Ack RX = $pap_auth_ack_rx " puts " Pap Auth NAck TX = $pap_auth_nak_tx " puts " Pap Auth NAck RX = $pap_auth_nak_rx " puts " Pap Auth Req TX = $pap_auth_req_tx " puts " Pap Auth Req RX = $pap_auth_req_rx " ################################################################################ # Delete all the streams first # ################################################################################ set traffic_status [::ixia::traffic_control \ -action reset \ -traffic_generator ixnetwork \ ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ######################################### # Configure traffic # ######################################### set traffic_status [::ixia::traffic_config \ -mode create \ -traffic_generator ixnetwork \ -bidirectional 1 \ -emulation_dst_handle $int_handle \ -emulation_src_handle $pppox_handle \ -track_by endpoint_pair \ -circuit_endpoint_type ipv4 \ -transmit_mode return_to_id_for_count \ -loop_count 10 \ -stream_packing one_stream_per_endpoint_pair \ -length_mode increment \ -frame_size_step 1 \ -frame_size_min 800 \ -frame_size_max 1500 \ -pkts_per_burst 2 \ -rate_percent 4.5 \ -enforce_min_gap 9 \ -tx_delay 10 \ -inter_frame_gap 8 \ -inter_burst_gap 11 \ -inter_stream_gap 12 \ ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ################################################################################ # Start the traffic # ################################################################################ set traffic_status [::ixia::traffic_control \ -action run \ -traffic_generator ixnetwork \ ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ################################################################################ # The traffic must flow! # ################################################################################ after 5000 ################################################################################ # Stop the traffic # ################################################################################ set traffic_status [::ixia::traffic_control \ -action stop \ -traffic_generator ixnetwork \ ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } ################################################################################ # Wait for the traffic to stop # ################################################################################ after 15000 ################################################################################ # Gather and display traffic statistics # ################################################################################ set aggregated_traffic_status [::ixia::traffic_stats \ -mode aggregate \ -traffic_generator ixnetwork \ ] if {[keylget aggregated_traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggregated_traffic_status log]" } set aggregated_traffic_results [list \ "Scheduled Frames Tx." aggregate.tx.scheduled_pkt_count \ "Scheduled Frames Tx. Rate" aggregate.tx.scheduled_pkt_rate \ "Line Speed" aggregate.tx.line_speed \ "Frames Tx." aggregate.tx.pkt_count \ "Total Frames Tx." aggregate.tx.total_pkts \ "Frames Tx. Rate" aggregate.tx.pkt_rate \ "Frames Tx. Rate" aggregate.tx.total_pkt_rate \ "Bytes Tx." aggregate.tx.pkt_byte_count \ "Bytes Tx. Rate" aggregate.tx.pkt_byte_rate \ "Tx. Rate (bps)" aggregate.tx.pkt_bit_rate \ "Tx. Rate (Kbps)" aggregate.tx.pkt_kbit_rate \ "Tx. Rate (Mbps)" aggregate.tx.pkt_mbit_rate \ "Bytes Rx." aggregate.rx.pkt_byte_count \ "Bytes Rx. Rate" aggregate.rx.pkt_byte_rate \ "Rx. Rate (bps)" aggregate.rx.pkt_bit_rate \ "Rx. Rate (Kbps)" aggregate.rx.pkt_kbit_rate \ "Rx. Rate (Mbps)" aggregate.rx.pkt_mbit_rate \ "Data Integrity Frames Rx." aggregate.rx.data_int_frames_count \ "Data Integrity Errors" aggregate.rx.data_int_errors_count \ "Collisions" aggregate.rx.collisions_count \ "Valid Frames Rx." aggregate.rx.pkt_count \ "Valid Frames Rx. Rate" aggregate.rx.pkt_rate \ ] foreach port $port_handle { puts "Port $port:" puts "\tAggregated statistics:" foreach {name key} $aggregated_traffic_results { puts "\t\t$name: [keylget aggregated_traffic_status\ $port.$key]" } } set stream_traffic_status [::ixia::traffic_stats \ -mode stream \ -traffic_generator ixnetwork \ ] if {[keylget stream_traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget stream_traffic_status log]" } set stream_tx_results [list \ "Tx Frames" total_pkts \ "Tx Frame Rate" total_pkt_rate \ ] set stream_rx_results [list \ "Rx Frames" total_pkts \ "Frames Delta" loss_pkts \ "Rx Frame Rate" total_pkt_rate \ "Loss %" loss_percent \ "Rx Bytes" total_pkts_bytes \ "Rx Rate (Bps)" total_pkt_byte_rate \ "Rx Rate (bps)" total_pkt_bit_rate \ "Rx Rate (Kbps)" total_pkt_kbit_rate \ "Rx Rate (Mbps)" total_pkt_mbit_rate \ "Avg Latency (ns)" avg_delay \ "Min Latency (ns)" min_delay \ "Max Latency (ns)" max_delay \ "First Timestamp" first_tstamp \ "Last Timestamp" last_tstamp \ ] foreach port $port_handle { puts "Port $port:" set streams [keylget stream_traffic_status \ $port.stream] foreach stream [keylkeys streams] { set stream_key [keylget stream_traffic_status \ $port.stream.$stream] foreach dir [keylkeys stream_key] { puts "\tStream $stream - $dir:" foreach {name key} [subst $[subst stream_${dir}_results]] { puts "\t\t$name: [keylget stream_traffic_status\ $port.stream.$stream.$dir.$key]" } } } } ######################################### # Disconnect sessions # ######################################### set control_status [::ixia::pppox_control \ -handle $pppox_handle \ -action disconnect ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } set cleanup_status [::ixia::cleanup_session -port_handle $port_handle] if {[keylget cleanup_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget cleanup_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"