################################################################################ # Version 1 $Revision: 3 $ # $Author: MChakravarthy $ # # Copyright © 1997 - 2013 by IXIA # All Rights Reserved. # # Revision Log: # 07-20-2007 Mchakravarthy - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures checks port link state # # and validates it # # # # Module: # # The sample was tested on a LM1000TXS4 module. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set test_name [info script] set cfgError 0 set chassis_ip 10.205.16.54 set port_list [list 2/5 2/6] set break_locks 1 set tcl_server 127.0.0.1 set ixnetwork_tcl_server 127.0.0.1 set port_count 2 ################################################################################ # START - Connect to the chassis ################################################################################ # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect puts "Starting - $test_name - [clock format [clock seconds]]" puts "Start connecting to chassis ..." set connect_status [::ixia::connect \ -reset \ -break_locks $break_locks \ -vport_count $port_count \ -tcl_server $tcl_server \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -interactive 1 \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] set port_handle [keylget connect_status vport_list] set i 0 puts "Ixia port handles are:" foreach port $port_handle { set port_$i $port puts $port incr i } puts "End connecting to chassis ..." ################################################################################ # END - Connect to the chassis ################################################################################ ################################################################################ # LINK STATUS - Check port link status - unassigned ################################################################################ puts "check port link state desired status - unassigned" set port_link_status [::ixia::test_control -action check_link_state -port_handle $port_handle -desired_status unassigned] if {[keylget port_link_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget port_link_status log]" return 0 } foreach port $port_handle { set port_status [keylget port_link_status $port.state] if {$port_status != "unassigned"} { puts "Error: Port $port doesnt have desired state set" incr cfgError } else { puts "Port $port State : $port_status" } } ################################################################################ # RESET - Reset and connect to the chassis ################################################################################ set connect_status [::ixia::connect \ -reset \ -port_list $port_list \ -device $chassis_ip \ -break_locks $break_locks \ -tcl_server $tcl_server \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -interactive 1 \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassis_ip.$port} \ temp_port]} { lappend port_handle $temp_port } } set i 0 puts "Ixia port handles are:" foreach port $port_handle { set port_$i $port puts $port incr i } puts "End connecting to chassis ..." ################################################################################ # END - Connect to the chassis ################################################################################ ################################################################################ # START - Interface configuration - Port 0 ################################################################################ puts "Start interface configuration for Port:$port_0" set interface_status_0 [::ixia::interface_config \ -port_handle $port_0 \ -l23_config_type protocol_interface \ -intf_ip_addr 11.1.1.1 \ -gateway 11.1.1.2 \ -netmask 255.255.255.0 \ -arp_on_linkup 1 \ -ns_on_linkup 1 \ -single_arp_per_gateway 1 \ -single_ns_per_gateway 1 \ -autonegotiation 1 \ -duplex auto \ -speed auto \ -intf_mode ethernet ] if {[keylget interface_status_0 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status_0 log]" return 0 } set interface_handle_0 [keylget interface_status_0 interface_handle] puts "Interface Handle: $interface_handle_0" puts "End interface configuration for Port:$port_0" ################################################################################ # START - Interface configuration - Port 1 ################################################################################ puts "Start interface configuration for Port:$port_1" set interface_status_1 [::ixia::interface_config \ -port_handle $port_1 \ -l23_config_type protocol_interface \ -intf_ip_addr 11.1.1.2 \ -gateway 11.1.1.1 \ -netmask 255.255.255.0 \ -arp_on_linkup 1 \ -ns_on_linkup 1 \ -single_arp_per_gateway 1 \ -single_ns_per_gateway 1 \ -autonegotiation 1 \ -duplex auto \ -speed auto \ -intf_mode ethernet ] if {[keylget interface_status_1 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status_1 log]" return 0 } set interface_handle_1 [keylget interface_status_1 interface_handle] puts "Interface Handle: $interface_handle_1" puts "End interface configuration for Port:$port_1" ################################################################################ # LINK STATUS - Check port link status - up ################################################################################ # Default value for desired status = up puts "check port link state desired status - up" set port_link_status [::ixia::test_control -action check_link_state -port_handle $port_handle] if {[keylget port_link_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget port_link_status log]" return 0 } foreach port $port_handle { set port_status [keylget port_link_status $port.state] if {$port_status != "up"} { puts "Error: Port $port doesnt have desired state set" incr cfgError } else { puts "Port $port State : $port_status" } } ################################################################################ # START - Modify Interface configuration - Port 0 ################################################################################ puts "Start interface configuration for Port:$port_0" set interface_status_0 [::ixia::interface_config \ -port_handle $port_0 \ -mode modify \ -autonegotiation 0 \ -speed ether100 \ -intf_mode ethernet ] if {[keylget interface_status_0 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status_0 log]" return 0 } ################################################################################ # START - Modify Interface configuration - Port 1 ################################################################################ puts "Start interface configuration for Port:$port_1" set interface_status_1 [::ixia::interface_config \ -port_handle $port_1 \ -mode modify \ -autonegotiation 0 \ -speed ether1000 \ -intf_mode ethernet ] if {[keylget interface_status_1 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status_1 log]" return 0 } ################################################################################ # LINK STATUS - Check port link status - down ################################################################################ puts "check port link state desired status - down" set port_link_status [::ixia::test_control -action check_link_state -port_handle $port_handle -desired_status down] if {[keylget port_link_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget port_link_status log]" return 0 } foreach port $port_handle { set port_status [keylget port_link_status $port.state] if {$port_status != "down"} { puts "Error: Port $port doesnt have desired state set" incr cfgError } else { puts "Port $port State : $port_status" } } ################################################################################ # LINK STATUS - Check port link status - timeout ################################################################################ puts "Polling for desired status - timeout 60s - [clock format [clock seconds]]" set port_link_status [::ixia::test_control -action check_link_state -port_handle $port_handle -desired_status up] puts "Polled for desired status - timeout 60s - [clock format [clock seconds]]" if {[keylget port_link_status status] != $::FAILURE} { puts "FAIL - $test_name - Return value should be $::FAILURE if ports are not in desired state" return 0 } foreach port $port_handle { set port_status [keylget port_link_status $port.state] if {$port_status != "down"} { puts "Error: Port $port doesnt have desired state set" incr cfgError } else { puts "Port $port State : $port_status" } } ############################### SUCCESS or FAILURE ############################# if {$cfgError == 0} { puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1 } else { puts "FAILURE - $test_name - [clock format [clock seconds]]" return 0 } ################################################################################