################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Eduard Tutescu $ # # Copyright © 1997 - 2013 by IXIA # All Rights Reserved. # # Revision Log: # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample configures two ports in IxNetwork and retrieve the ports # # owner, type and name through the device_info procedure call # # # # Module: # # The sample was tested on a 10/100/1000 STX4-256MB module. # # # ################################################################################ package require Ixia proc keylprint {keylist {space ""}} { upvar $keylist kl set result "" foreach key [keylkeys kl] { set value [keylget kl $key] if {[catch {keylkeys value}]} { append result "$space$key: $value\n" } else { set newspace "$space " append result "$space$key:\n[keylprint value $newspace]" } } return $result } set test_name [info script] set chassis_ip [list 10.205.16.98] set port_list [list 7/1 7/2] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -username ixiaApiUser \ -ixnetwork_tcl_server localhost \ ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set i 0 foreach port $port_list { set port_${i} [keylget connect_status port_handle.$chassis_ip.$port] incr i } set port_list_info [list $port_0 $port_1] # Getting information about the specified ports set device_stat [::ixia::device_info \ -ports $port_list_info \ -port_handle $port_list_info \ ] if {[keylget device_stat status] != $::SUCCESS} { return "FAIL - $test_name - [keylget device_stat log]" } puts [keylprint device_stat] puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1