################################################################################ # Version 1.0 $Revision: 1 $ # $Author: M Ridichie $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 6-02-2006 MRidichie # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample collects the ATM stats. # # # # Module: # # The sample was tested on a LM622MR module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester ######## # IpV4 # ######## set port_list "3/1 3/2" ################################################################################# # START TEST # ################################################################################# # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_one [keylget connect_status \ port_handle.$chassisIP.[lindex $port_list 0]] set port_two [keylget connect_status \ port_handle.$chassisIP.[lindex $port_list 1]] set port_handle [list $port_one $port_two] ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_one \ -intf_ip_addr 1.1.1.1 \ -gateway 1.1.1.2 \ -netmask 255.255.255.0 \ -atm_enable_coset 1 \ -atm_enable_pattern_matching 1 \ -atm_filler_cell idle \ -atm_interface_type nni \ -atm_packet_decode_mode cell \ -atm_reassembly_timeout 111] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_two \ -intf_ip_addr 1.1.1.2 \ -gateway 1.1.1.1 \ -netmask 255.255.255.0 \ -atm_enable_coset 1 \ -atm_enable_pattern_matching 1 \ -atm_filler_cell idle \ -atm_interface_type nni \ -atm_packet_decode_mode cell \ -atm_reassembly_timeout 111] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ######################################## # Stream configuration # # IPv4 # ######################################## # Delete all the streams first set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_one ] set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_two ] set stream_index_list "" # Configure first stream on the IpV4 port set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_one \ -l3_protocol ipv4 \ -ip_src_addr 1.1.1.1 \ -ip_dst_addr 1.1.1.2 \ -rate_percent 50.0 \ -l3_length 100 \ -vpi 10 \ -vci 20 \ -atm_header_aal5error no_error \ -atm_header_cell_loss_priority 1 \ -atm_header_enable_cpcs_length 1 \ -atm_header_cpcs_length 100 \ -atm_header_enable_auto_vpi_vci 0 \ -atm_header_enable_cl 1 \ -atm_header_encapsulation llc_routed_clip \ -atm_header_generic_flow_ctrl 14 \ -atm_header_hec_errors 0 \ -atm_counter_vpi_type fixed \ -atm_counter_vci_type fixed ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_two \ -l3_protocol ipv4 \ -ip_src_addr 1.1.1.2 \ -ip_dst_addr 1.1.1.1 \ -rate_percent 50.0 \ -l3_length 100 \ -vpi 10 \ -vci 20 \ -atm_header_aal5error no_error \ -atm_header_cell_loss_priority 1 \ -atm_header_enable_cpcs_length 1 \ -atm_header_cpcs_length 100 \ -atm_header_enable_auto_vpi_vci 0 \ -atm_header_enable_cl 1 \ -atm_header_encapsulation llc_routed_clip \ -atm_header_generic_flow_ctrl 14 \ -atm_header_hec_errors 0 \ -atm_counter_vpi_type fixed \ -atm_counter_vci_type fixed ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } # Clear stats before sending traffic set clear_stats_status [::ixia::traffic_control \ -port_handle $port_handle \ -action clear_stats ] if {[keylget clear_stats_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget clear_stats_status log]" } set traffic_start_status [::ixia::traffic_stats \ -port_handle $port_one \ -mode add_atm_stats \ -vpi 10 \ -vci 20 \ -atm_counter_vpi_type fixed \ -atm_counter_vci_type fixed \ -atm_reassembly_enable_iptcpudp_checksum 0 \ -atm_reassembly_enable_ip_qos 0 \ -atm_reassembly_encapsulation llc_routed_clip ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } set traffic_start_status [::ixia::traffic_stats \ -port_handle $port_two \ -mode add_atm_stats \ -vpi 10 \ -vci 20 \ -atm_counter_vpi_type fixed \ -atm_counter_vci_type fixed \ -atm_reassembly_enable_iptcpudp_checksum 0 \ -atm_reassembly_enable_ip_qos 0 \ -atm_reassembly_encapsulation llc_routed_clip ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } # Start the traffic on TX port set traffic_start_status [::ixia::traffic_control \ -port_handle $port_one \ -action run ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } set traffic_start_status [::ixia::traffic_control \ -port_handle $port_two \ -action run ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } # Sleep 5 seconds ixia_sleep 5000 set traffic_start_status [::ixia::traffic_control \ -port_handle $port_one \ -action stop ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } set traffic_start_status [::ixia::traffic_control \ -port_handle $port_two \ -action stop ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } set vpi 10 set vci 20 set aggregate_stats [::ixia::traffic_stats -port_handle $port_one] if {[keylget aggregate_stats status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggregate_stats log]" } puts "" puts "*************************Port $port_one*************************" puts "" puts "Aggregate TX stats on ATM port $port_one: (vpi,vci) = $vpi/$vci" puts "--------------------------------------------------" foreach statName [keylkeys aggregate_stats ${port_one}.aggregate.tx.${vpi}.${vci}] { puts [format "%31s %-20s" "$statName" [keylget aggregate_stats ${port_one}.aggregate.tx.${vpi}.${vci}.${statName}]] } puts "" puts "Aggregate RX stats on ATM port $port_one: (vpi,vci) = $vpi/$vci" puts "--------------------------------------------------" foreach statName [keylkeys aggregate_stats ${port_one}.aggregate.rx.${vpi}.${vci}] { puts [format "%31s %-20s" "$statName" [keylget aggregate_stats ${port_one}.aggregate.rx.${vpi}.${vci}.${statName}]] } set aggregate_stats [::ixia::traffic_stats -port_handle $port_two] if {[keylget aggregate_stats status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggregate_stats log]" } puts "" puts "*************************Port $port_two*************************" puts "" puts "Aggregate RX stats on ATM port $port_two: (vpi,vci) = $vpi/$vci" puts "--------------------------------------------------" foreach statName [keylkeys aggregate_stats ${port_two}.aggregate.rx.${vpi}.${vci}] { puts [format "%31s %-20s" "$statName" [keylget aggregate_stats ${port_two}.aggregate.rx.${vpi}.${vci}.${statName}]] } puts "" puts "Aggregate TX stats on ATM port $port_two: (vpi,vci) = $vpi/$vci" puts "--------------------------------------------------" foreach statName [keylkeys aggregate_stats ${port_two}.aggregate.tx.${vpi}.${vci}] { puts [format "%31s %-20s" "$statName" [keylget aggregate_stats ${port_two}.aggregate.tx.${vpi}.${vci}.${statName}]] } return "SUCCESS - $test_name - [clock format [clock seconds]]"