################################################################################ # Version 1.0 $Revision: 1 $ # # Copyright © 1997 - 2006 by IXIA # All Rights Reserved. # # Revision Log: # 3-13-2006 : M. Githens # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates an IGMP v2 host. It creates a multicast group pool # # and adds it to the host. The point though is that the interfaces used # # in the routing protocol are created with the interface_config call, and # # then the -interface_handle is used in the IGMP call # # # # Module: # # The sample was tested on a LM1000TXS4 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP 127.0.0.1 set port_list 1/1 # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [keylget connect_status port_handle.$chassisIP.$port_list] ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -intf_ip_addr 10.42.1.2 \ -gateway 10.42.1.1 \ -netmask 255.255.255.0 \ -autonegotiation 1 \ -src_mac_addr 0000.0005.0001 \ -op_mode normal \ -vlan $false \ -duplex auto \ -speed auto \ -intf_mode ethernet ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set intf_handle [keylget interface_status interface_handle] ################################################## # Configure interfaces and create IGMP sessions # ################################################## set igmp_status [::ixia::emulation_igmp_config \ -port_handle $port_handle \ -mode create \ -interface_handle $intf_handle \ -reset \ -msg_interval 167 \ -igmp_version v2 \ -ip_router_alert 0 \ -general_query 0 \ -group_query 0 \ -count 1 \ -intf_ip_addr 10.42.1.2 \ -neighbor_intf_ip_addr 10.42.1.1 \ -intf_prefix_len 24 ] if {[keylget igmp_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget igmp_status log]" } set session [keylget igmp_status handle] # Create multicast group pool set multicast_status [::ixia::emulation_multicast_group_config \ -mode create \ -num_groups 20 \ -ip_addr_start 225.0.1.1 \ -ip_addr_step 0.0.0.1 \ -ip_prefix_len 24 ] if {[keylget multicast_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget multicast_status log]" } set group [keylget multicast_status handle] # Create IGMP group member by asociating a multicast group pool to a session set group_status [::ixia::emulation_igmp_group_config \ -mode create \ -session_handle $session \ -group_pool_handle $group ] if {[keylget group_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget group_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"