################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Matei-Eugen Vasile $ # # Copyright © 1997 - 2007 by IXIA # All Rights Reserved. # # Revision Log: # 1-31-2003 Matei-Eugen Vasile # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample configures multiple interfaces on an Ethernet port with # # multiple calls to ::ixia::interface_config. The interfaces are IPv4, IPv6 # # and IPv4/IPv6. # # # # Module: # # The sample was tested on a TXS4 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP 10.205.19.96 set port_list [list 2/1 2/2] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser \ ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle1 [keylget connect_status port_handle.$chassisIP.[lindex $port_list 0]] set port_handle2 [keylget connect_status port_handle.$chassisIP.[lindex $port_list 1]] set interface_status [::ixia::interface_config \ -port_handle $port_handle1 \ -intf_ip_addr 12.1.3.2 \ -gateway 12.1.3.1 \ -netmask 255.255.255.0 \ -autonegotiation 1 \ -src_mac_addr 0000.0005.0001 \ -vlan $true \ -vlan_id 99 \ -vlan_user_priority 7 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_handle1 \ -intf_ip_addr 13.1.3.2 \ -gateway 13.1.3.1 \ -netmask 255.255.255.0 \ -autonegotiation 1 \ -src_mac_addr 0000.0005.0101 \ -vlan $true \ -vlan_id 100 \ -vlan_user_priority 7 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_handle1 \ -ipv6_intf_addr 121::2 \ -ipv6_prefix_length 64 \ -autonegotiation 1 \ -src_mac_addr 0000.0005.0011 \ -vlan $true \ -vlan_id 100 \ -vlan_user_priority 5 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_handle1 \ -ipv6_intf_addr 127::2 \ -ipv6_prefix_length 69 \ -autonegotiation 1 \ -src_mac_addr 0000.0005.0101 \ -vlan $true \ -vlan_id 80 \ -vlan_user_priority 7 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_handle2 \ -ipv6_intf_addr 12C::2 \ -ipv6_prefix_length 63 \ -autonegotiation 1 \ -intf_ip_addr 66.6.3.2 \ -gateway 66.6.4.1 \ -netmask 255.255.0.0 \ -src_mac_addr 0000.0005.0010 \ -vlan $true \ -vlan_id 100 \ -vlan_user_priority 7 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set interface_status [::ixia::interface_config \ -port_handle $port_handle2 \ -ipv6_intf_addr 12C::2 \ -ipv6_prefix_length 63 \ -autonegotiation 1 \ -intf_ip_addr 66.6.3.2 \ -gateway 66.6.4.1 \ -netmask 255.255.0.0 \ -src_mac_addr 0000.0005.0010 \ -vlan $true \ -vlan_id 10 \ -vlan_user_priority 3 \ ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"