################################################################################ # Version 1.0 $Revision: 1 $ # $Author: etutescu $ # # Copyright © 1997 - 2009 by IXIA # All Rights Reserved. # # Revision Log: # 05-24-2013 etutescu # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This script creates a traffic item and runs traffic between 2 ports. It # # prints flow stats. # # Module: # # The sample was tested on an STXS4 module. # # # ################################################################################ package require Ixia proc KeylPrint {keylist {space ""}} { upvar $keylist kl set result "" foreach key [keylkeys kl] { set value [keylget kl $key] if {[catch {keylkeys value}]} { append result "$space$key: $value\n" } else { set newspace "$space " append result "$space$key:\n[KeylPrint value $newspace]" } } return $result } set test_name [info script] set chassis_ip ixro-hlt-xm2-06 set ixnetwork_tcl_server localhost set username ixiaApiUser set port_list [list 2/1 2/2] set connectStatus [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -username $username \ -tcl_server $chassis_ip \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ ] if {[keylget connectStatus status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connectStatus log]" } set port_array [keylget connectStatus port_handle.$chassis_ip] set port_0 [keylget port_array [lindex $port_list 0]] set port_1 [keylget port_array [lindex $port_list 1]] set interface_status1 [::ixia::interface_config \ -port_handle $port_0 \ -intf_ip_addr 172.16.31.1 \ -gateway 172.16.31.2 \ -netmask 255.255.255.0 \ -op_mode normal \ -vlan $true \ -vlan_id 100 \ -vlan_user_priority 7 \ -port_rx_mode capture_and_measure \ ] if {[keylget interface_status1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } set intf_h0 [keylget interface_status1 interface_handle] set interfaceStatus2 [::ixia::interface_config \ -port_handle $port_1 \ -intf_ip_addr 172.16.31.2 \ -gateway 172.16.31.1 \ -netmask 255.255.255.0 \ -op_mode normal \ -vlan $true \ -vlan_id 100 \ -vlan_user_priority 7 \ -port_rx_mode capture_and_measure \ ] if {[keylget interfaceStatus2 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interfaceStatus2 log]" } set intf_h1 [keylget interfaceStatus2 interface_handle] set trafficStatus1 [::ixia::traffic_config \ -circuit_endpoint_type ipv4 \ -mode create \ -emulation_src_handle $intf_h0 \ -emulation_dst_handle $intf_h1 \ -l3_protocol ipv4 \ -qos_type_ixn custom \ -qos_value_ixn 5 \ -qos_value_ixn_mode incr \ -qos_value_ixn_step 2 \ -qos_value_ixn_count 2 \ -qos_value_ixn_tracking 1 \ -track_by "flowGroup0 ethernet_ii_pfc_queue" \ ] if {[keylget trafficStatus1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget trafficStatus1 log]" } set trafficStatus2 [::ixia::traffic_config \ -circuit_endpoint_type ipv4 \ -mode create \ -emulation_src_handle $intf_h0 \ -emulation_dst_handle $intf_h1 \ -l3_protocol ipv4 \ -qos_type_ixn tos \ -ip_precedence {0 3} \ -ip_precedence_mode list \ -ip_precedence_tracking 1 \ -track_by "flowGroup0 ipv4_precedence" \ ] if {[keylget trafficStatus2 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget trafficStatus2 log]" } set trafficStatus3 [::ixia::traffic_config \ -circuit_endpoint_type ipv4 \ -mode create \ -emulation_src_handle $intf_h0 \ -emulation_dst_handle $intf_h1 \ -l3_protocol ipv4 \ -qos_type_ixn dscp \ -qos_value_ixn dscp_default \ -ip_dscp 60 \ -ip_dscp_mode decr \ -ip_dscp_count 3 \ -ip_dscp_step 10 \ -ip_dscp_tracking 1 \ -track_by "flowGroup0 default_phb" \ ] if {[keylget trafficStatus3 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget trafficStatus3 log]" } set trafficStatus4 [::ixia::traffic_config \ -circuit_endpoint_type ipv4 \ -mode create \ -emulation_src_handle $intf_h0 \ -emulation_dst_handle $intf_h1 \ -l3_protocol ipv4 \ -qos_type_ixn dscp \ -qos_value_ixn {af_class1_low_precedence af_class2_high_precedence} \ -qos_value_ixn_mode list \ -qos_value_ixn_tracking 1 \ -track_by "flowGroup0 assured_forwarding_phb" \ ] if {[keylget trafficStatus4 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget trafficStatus4 log]" } set trafficStatus5 [::ixia::traffic_config \ -circuit_endpoint_type ipv4 \ -mode create \ -emulation_src_handle $intf_h0 \ -emulation_dst_handle $intf_h1 \ -l3_protocol ipv4 \ -qos_type_ixn dscp \ -qos_value_ixn {cs_precedence1 cs_precedence2} \ -qos_value_ixn_mode list \ -qos_value_ixn_tracking 1 \ -track_by "flowGroup0 class_selector_phb" \ ] if {[keylget trafficStatus5 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget trafficStatus5 log]" } set item [keylget trafficStatus5 traffic_item] set trafficStatus [::ixia::traffic_control \ -action run \ -traffic_generator ixnetwork \ ] if {[keylget trafficStatus status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget trafficStatus log]" return 0 } after 5000 ################################################################################ # Stop the traffic # ################################################################################ set traffic_status [::ixia::traffic_control \ -action stop \ -traffic_generator ixnetwork \ ] if {[keylget traffic_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_status log]" return 0 } set flow_traffic_status [::ixia::traffic_stats \ -mode flow \ -traffic_generator ixnetwork \ ] if {[keylget flow_traffic_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget flow_traffic_status log]" return 0 } ################################################################################ # Wait for the traffic to stop # ################################################################################ after 30000 set flow_results [list \ "Tracking Name" tracking_name \ "Tracking Value" tracking_value \ ] set flows [keylget flow_traffic_status flow] foreach flow [keylkeys flows] { set flow_key [keylget flow_traffic_status flow.$flow] puts "\tFlow $flow: [keylget flow_traffic_status flow.$flow.flow_name]" puts "\t\tTracking Count: [keylget flow_traffic_status flow.$flow.tracking.count]" for {set index 1} {$index <= [keylget flow_traffic_status flow.$flow.tracking.count]} {incr index} { puts "\t\tTracking item $index" foreach {name key} [subst $[subst flow_results]] { puts "\t\t\t$name: [keylget flow_traffic_status flow.$flow.tracking.$index.$key]" } } } puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1