################################################################################ # Version 1.0 $Revision: 1 $ # $Author: cnicutar$ # # Copyright © 1997 - 2009 by IXIA # All Rights Reserved. # # Revision Log: # 4-25-2009 # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates a traffic item using circuit_type quick_flows and udf # # parameters and the runs traffic between the 2 ports and prints flow stats # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested with HLTSET55. # # # ################################################################################ package require Ixia proc print_flow_stats {flow_traffic_status} { set flow_results [list \ "Tx Frames" tx.total_pkts \ "Rx Frames" rx.total_pkts \ "Tx pkt_rate" tx.total_pkt_rate \ "Loss %" rx.loss_percent \ ] set flows [keylget flow_traffic_status flow] foreach flow [keylkeys flows] { set flow_key [keylget flow_traffic_status flow.$flow] puts "\tFlow $flow" foreach {name key} [subst $[subst flow_results]] { puts "\t\t$name: [keylget flow_traffic_status flow.$flow.$key]" } } } set test_name [info script] set chassisIP sylvester ######## # IpV4 # ######## set ipV4_port_list "7/1 7/2" set ipV4_ixia_list "1.1.1.2 1.1.1.1" set ipV4_gateway_list "1.1.1.1 1.1.1.2" set ipV4_netmask_list "255.255.255.0 255.255.255.0" set ipV4_mac_list "0000.0000.0001 0000.0000.0002" set ipV4_version_list "4 4" set ipV4_autoneg_list "0 0" set ipV4_duplex_list "full full" set ipV4_speed_list "ether100 ether100" set file_name "ip_flows_test_results.txt" # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -ixnetwork_tcl_server localhost \ -device $chassisIP \ -port_list $ipV4_port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle_tx [keylget connect_status \ port_handle.$chassisIP.[lindex $ipV4_port_list 0]] set port_handle_rx [keylget connect_status \ port_handle.$chassisIP.[lindex $ipV4_port_list 1]] set port_handle_list [list $port_handle_tx $port_handle_rx] ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle_list \ -intf_ip_addr $ipV4_ixia_list \ -gateway $ipV4_gateway_list \ -netmask $ipV4_netmask_list \ -autonegotiation $ipV4_autoneg_list \ -duplex $ipV4_duplex_list \ -src_mac_addr $ipV4_mac_list \ -speed $ipV4_speed_list ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ################################## # Configure streams on TX port # ################################## set flow_count 10 # Configure the streams on the first IpV4 port set traffic_status1 [::ixia::traffic_config \ -traffic_generator ixnetwork_540 \ -mode create \ -circuit_type quick_flows \ -port_handle $port_handle_tx \ -port_handle2 $port_handle_rx \ -l3_protocol ipv4 \ -ip_src_addr 1.1.1.1 \ -ip_src_mode fixed \ -ip_dst_addr 1.1.1.2 \ -ip_dst_mode increment \ -ip_dst_step 0.0.0.1 \ -ip_dst_count $flow_count \ -l3_length 46 \ -rate_percent 100 \ -mac_dst_mode discovery \ -enable_udf4 1 \ -udf4_mode nested \ -udf4_offset 26 \ -udf4_counter_type 32 \ -udf4_counter_init_value 12.1.1.1 \ -udf4_counter_step 1 \ -udf4_counter_mode count \ -udf4_counter_repeat_count $flow_count \ -udf4_inner_repeat_value $flow_count \ -udf4_inner_repeat_count $flow_count \ -udf4_inner_step 1 \ -enable_udf3 1 \ -udf3_mode counter \ -udf3_offset 52 \ -udf3_counter_type 16 \ -udf3_counter_init_value 1 \ -udf3_counter_repeat_count [mpexpr $flow_count * $flow_count] \ -udf3_counter_step 1 \ -udf3_counter_mode count \ -track_by dest_endpoint] if {[keylget traffic_status1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status1 log]" } ######################### # Start traffic on port # ######################### # Clear stats before sending traffic set clear_stats_status [::ixia::traffic_control \ -traffic_generator ixnetwork_540 \ -port_handle $port_handle_list \ -action clear_stats ] if {[keylget clear_stats_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget clear_stats_status log]" } set traffic_control_status [::ixia::traffic_control \ -traffic_generator ixnetwork_540 \ -port_handle $port_handle_tx \ -action run ] if {[keylget traffic_control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_control_status log]" } ixia_sleep 10000 ############################################ # Get traffic statistics for all the PGIDs # ############################################ set flow_statistics_list [::ixia::traffic_stats \ -traffic_generator ixnetwork_540 \ -mode flow \ ] if {[keylget flow_statistics_list status] != $::SUCCESS} { return "FAIL - $test_name - [keylget flow_statistics_list log]" } ######################## # Stop traffic on port # ######################## set traffic_control_status [::ixia::traffic_control \ -traffic_generator ixnetwork_540 \ -port_handle $port_handle_tx \ -action stop ] if {[keylget traffic_control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_control_status log]" } print_flow_stats $flow_statistics_list update idletasks puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1