################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Eduard Tutescu $ # # Copyright © 1997 - 2013 by IXIA # All Rights Reserved. # # Revision Log: # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample configures two ports in IxNetwork, configures a traffic item # # and performs a packet_stats procedure call in order to get the first data # # frame. # # # # Module: # # The sample was tested on a 10/100/1000 STX4-256MB module. # # # ################################################################################ package require Ixia set test_name [info script] set chassis_ip ixro-hlt-xm2-02 set tcl_server ixro-hlt-xm2-02 set ixnetwork_tcl_server localhost set port_list [list 1/1 1/2] set cfgErrors 0 # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -tcl_server $tcl_server \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassis_ip.$port} temp_port]} { lappend port_handle $temp_port } } set port_src_handle [lindex $port_handle 0] set port_dst_handle [lindex $port_handle 1] puts "Ixia port handles are $port_handle ..." ################################################################################ # Configure Protocol Interfaces on both ports # ################################################################################ set interface_status [::ixia::interface_config \ -mode config \ -port_handle $port_src_handle \ -transmit_clock_source external \ -internal_ppm_adjust 0 \ -data_integrity 1 \ -intf_mode ethernet \ -speed ether100 \ -duplex full \ -autonegotiation 1 \ -phy_mode copper \ -transmit_mode advanced \ -port_rx_mode capture_and_measure \ -tx_gap_control_mode fixed \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return 0 } set _result_ [::ixia::interface_config \ -mode config \ -port_handle $port_dst_handle \ -transmit_clock_source external \ -internal_ppm_adjust 0 \ -data_integrity 1 \ -intf_mode ethernet \ -speed ether100 \ -duplex full \ -autonegotiation 1 \ -phy_mode copper \ -transmit_mode advanced \ -port_rx_mode capture_and_measure \ -tx_gap_control_mode fixed \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return 0 } set _result_ [::ixia::interface_config \ -mode modify \ -port_handle $port_src_handle \ -vlan 0 \ -l23_config_type protocol_interface \ -mtu 1500 \ -gateway 20.0.0.1 \ -intf_ip_addr 20.0.0.2 \ -netmask 255.255.255.0 \ -check_opposite_ip_version 0 \ -src_mac_addr 0000.0107.4232 \ -arp_on_linkup 0 \ -ns_on_linkup 0 \ -single_arp_per_gateway 1 \ -single_ns_per_gateway 1 \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return 0 } set _result_ [::ixia::interface_config \ -mode modify \ -port_handle $port_dst_handle \ -vlan 0 \ -l23_config_type protocol_interface \ -mtu 1500 \ -gateway 20.0.0.2 \ -intf_ip_addr 20.0.0.1 \ -netmask 255.255.255.0 \ -check_opposite_ip_version 0 \ -src_mac_addr 0000.0107.4233 \ -arp_on_linkup 0 \ -ns_on_linkup 0 \ -single_arp_per_gateway 1 \ -single_ns_per_gateway 1 \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return 0 } ################################################################################ # Configure Traffic on ports # ################################################################################ puts "Configure Traffic..." set traffic_status [::ixia::traffic_control \ -action reset \ -traffic_generator ixnetwork_540 \ -cpdp_convergence_enable 0 \ -delay_variation_enable 0 \ -packet_loss_duration_enable 0 \ -latency_bins 3 \ -latency_values {1.5 3 6.8} \ -latency_control store_and_forward \ ] if {[keylget traffic_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_status log]" return 0 } set ti_src ::ixNet::OBJ-/vport:1/protocols set ti_dst ::ixNet::OBJ-/vport:2/protocols set traffic_result [::ixia::traffic_config \ -mode create \ -traffic_generator ixnetwork_540 \ -endpointset_count 1 \ -emulation_src_handle $ti_src \ -emulation_dst_handle $ti_dst \ -global_dest_mac_retry_count 1 \ -global_dest_mac_retry_delay 5 \ -enable_data_integrity 1 \ -global_enable_dest_mac_retry 1 \ -global_enable_min_frame_size 0 \ -global_enable_staggered_transmit 0 \ -global_enable_stream_ordering 0 \ -global_stream_control continuous \ -global_stream_control_iterations 1 \ -global_large_error_threshhold 2 \ -global_enable_mac_change_on_fly 0 \ -global_max_traffic_generation_queries 500 \ -global_mpls_label_learning_timeout 30 \ -global_refresh_learned_info_before_apply 0 \ -global_use_tx_rx_sync 1 \ -global_wait_time 1 \ -global_display_mpls_current_label_value 0 \ -frame_sequencing disable \ -frame_sequencing_mode rx_threshold \ -src_dest_mesh one_to_one \ -route_mesh one_to_one \ -bidirectional 0 \ -allow_self_destined 0 \ -enable_dynamic_mpls_labels 0 \ -hosts_per_net 1 \ -name Traffic_Item_1 \ -source_filter all \ -destination_filter all \ -merge_destinations 1 \ -circuit_endpoint_type ipv4 \ -egress_tracking none \ ] if {[keylget traffic_result status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_result log]" return 0 } set current_config_element [keylget traffic_result traffic_item] set stack_handle [lindex [keylget traffic_result $current_config_element.headers] 0] set stream_id1 [keylget traffic_result stream_id] set traffic_result2 [::ixia::traffic_config \ -mode create \ -traffic_generator ixnetwork_540 \ -endpointset_count 1 \ -emulation_src_handle $ti_src \ -emulation_dst_handle $ti_dst \ -global_dest_mac_retry_count 1 \ -global_dest_mac_retry_delay 5 \ -enable_data_integrity 1 \ -global_enable_dest_mac_retry 1 \ -global_enable_min_frame_size 0 \ -global_enable_staggered_transmit 0 \ -global_enable_stream_ordering 0 \ -global_stream_control continuous \ -global_stream_control_iterations 1 \ -global_large_error_threshhold 2 \ -global_enable_mac_change_on_fly 0 \ -global_max_traffic_generation_queries 500 \ -global_mpls_label_learning_timeout 30 \ -global_refresh_learned_info_before_apply 0 \ -global_use_tx_rx_sync 1 \ -global_wait_time 1 \ -global_display_mpls_current_label_value 0 \ -frame_sequencing disable \ -frame_sequencing_mode rx_threshold \ -src_dest_mesh one_to_one \ -route_mesh one_to_one \ -bidirectional 0 \ -allow_self_destined 0 \ -enable_dynamic_mpls_labels 0 \ -hosts_per_net 1 \ -name Traffic_Item_2 \ -source_filter all \ -destination_filter all \ -merge_destinations 1 \ -circuit_endpoint_type ipv4 \ -egress_tracking none \ ] if {[keylget traffic_result2 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_result2 log]" return 0 } set current_config_element2 [keylget traffic_result2 traffic_item] set stack_handle2 [lindex [keylget traffic_result2 $current_config_element2.headers] 0] set stream_id2 [keylget traffic_result2 stream_id] set titem_1 {::ixNet::OBJ-/traffic/trafficItem:1} set titem_2 {::ixNet::OBJ-/traffic/trafficItem:2} set traffic_item [keylget traffic_result stream_id] set traffic_item2 [keylget traffic_result2 stream_id] set run_traffic [::ixia::traffic_control \ -action run \ -handle [list $traffic_item $traffic_item2] \ ] if {[keylget run_traffic status] != $::SUCCESS} { puts "error in traffic_control: [keylget run_traffic log]" return 0 } after 5000 set run_traffic [::ixia::traffic_control \ -action stop \ -handle $traffic_item \ ] if {[keylget run_traffic status] != $::SUCCESS} { puts "error in traffic_control: [keylget run_traffic log]" return 0 } puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1