################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Enache Adrian $ # # Copyright © 1997 - 2011 by IXIA # All Rights Reserved. # # Revision Log: # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample configures a port in IxNetwork and sets the vport name. # # Then verifies the name and returns the real port handle. # # # # Module: # # The sample was tested on a 10/100/1000 STX4-256MB module. # # # ################################################################################ set env(IXIA_VERSION) HLTSET105 package require Ixia #set ixia::debug 3 set test_name [info script] set chassisIP sylvester set port_list {2/1} # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser \ -ixnetwork_tcl_server localhost \ -tcl_server $chassisIP ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [keylget connect_status port_handle.$chassisIP.$port_list] ######################################## # Configure interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -autonegotiation 1 \ -duplex full \ -speed ether100 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ######################################### # Set a vport name and then get it back # # and compare # ######################################### puts "Setting the vport name..." set port_name {custom_name_p1} set ret [ixia::vport_info \ -mode set_info \ -port_list [list $port_handle] \ -port_name_list $port_name ] if {[keylget ret status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set ret [ixia::vport_info \ -mode get_info \ -port_list [list $port_handle] ] if {[keylget ret status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } if {[keylget ret $port_handle.port_name] != $port_name} { return "FAIL - $test_name - [keylget connect_status log]" } puts "Name was set ok" puts "Port is connected to [keylget ret $port_handle.real_port_handle]" puts "SUCCESS - [info script] - [clock format [clock seconds]]" return 1