################################################################################ # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2006 by IXIA # All Rights Reserved. # # Revision Log: # 06-06-2006 LRaicea # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures 2 ports with the auto detect instrumentation # # feature and then creates a stream on each port. # # Bidirectional traffic is run and stats are being retrieved. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested with HLTSET26. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester ################################################################################ # Interface configuration settings ################################################################################ set port_list "3/1 3/2" set ixia_list "1.1.1.1 1.1.1.2" set gateway_list "1.1.1.2 1.1.1.1" set netmask_list "255.255.255.0 255.255.255.0" set mac_list "0000.debb.0001 0000.debb.0002" set autoneg_list "1 1" set duplex_list "full full" set speed_list "ether100 ether100" set port_rx_list "auto_detect_instrumentation auto_detect_instrumentation" set seq_checking_list "1 1" set data_integrity_list "1 1" set signature_list { {AA BB AA BB AA BB AA BB AA BB AA BB} {CC DD CC DD CC DD CC DD CC DD CC DD} } set signature_start_list "2 2" # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_one [keylget connect_status \ port_handle.$chassisIP.[lindex $port_list 0]] set port_two [keylget connect_status \ port_handle.$chassisIP.[lindex $port_list 1]] set port_handle [list $port_one $port_two] ################################################################################ # Configure interface in the test IPv4 ################################################################################ set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -intf_ip_addr $ixia_list \ -gateway $gateway_list \ -netmask $netmask_list \ -autonegotiation $autoneg_list \ -duplex $duplex_list \ -src_mac_addr $mac_list \ -speed $speed_list \ -port_rx_mode $port_rx_list \ -signature $signature_list \ -signature_start_offset $signature_start_list \ -sequence_checking $seq_checking_list \ -data_integrity $data_integrity_list ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ################################################################################ # Delete all the streams first ################################################################################ set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_handle ] set stream_index_list "" ################################################################################ # Configure first stream on the IpV4 port ################################################################################ set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_one \ -l3_protocol ipv4 \ -ip_src_addr [lindex $ixia_list 0] \ -ip_dst_addr [lindex $ixia_list 1] \ -l3_length 64 \ -rate_percent 50 \ -mac_dst_mode discovery \ -mac_src [lindex $mac_list 0] \ -enable_auto_detect_instrumentation 1 \ -signature [lindex $signature_list 1] \ -frame_sequencing enable \ -enable_data_integrity 1 \ -integrity_signature EE.AA ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } lappend stream_index_list [keylget traffic_status stream_id] ################################################################################ # Configure second stream on the IpV4 port ################################################################################ set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_two \ -l3_protocol ipv4 \ -ip_src_addr [lindex $ixia_list 1] \ -ip_dst_addr [lindex $ixia_list 0] \ -l3_length 64 \ -rate_percent 50 \ -mac_dst_mode discovery \ -mac_src [lindex $mac_list 1] \ -enable_auto_detect_instrumentation 1 \ -signature [lindex $signature_list 0] \ -frame_sequencing enable \ -enable_data_integrity 1 \ -integrity_signature EE.BB ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } lappend stream_index_list [keylget traffic_status stream_id] set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -arp_send_req 1 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } foreach port $port_handle { if {[catch {set failed_arp [keylget interface_status \ $port.arp_request_success]}] || $failed_arp == 0} { set returnLog "FAIL - $test_name arp send request failed. " if {![catch {set intf_list [keylget \ interface_status $port.arp_ipv4_interfaces_failed]}]} { append returnLog "ARP failed on interfaces: $intf_list." } return $returnLog } } ################################################################################ # Clear stats before sending traffic ################################################################################ set clear_stats_status [::ixia::traffic_control \ -port_handle $port_handle \ -action clear_stats ] if {[keylget clear_stats_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget clear_stats_status log]" } ################################################################################ # Start the traffic ################################################################################ set traffic_start_status [::ixia::traffic_control \ -port_handle $port_handle \ -action run ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } # Wait 15 seconds after 15000 proc post_stats {port_handle label key_list stat_key {stream ""}} { puts -nonewline [format "%-32s" $label] foreach port $port_handle { if {$stream != ""} { set key $port.stream.$stream.$stat_key } else { set key $port.$stat_key } if {[catch {keylget key_list $key}]} { puts -nonewline "[format "%-16s" N/A]" } else { puts -nonewline "[format "%-16s" [keylget key_list $key]]" } } puts "" } ################################################################################ # Stop traffic on the TX port ################################################################################ set traffic_stop_status [::ixia::traffic_control \ -port_handle $port_handle \ -action stop ] if {[keylget traffic_stop_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_stop_status log]" } ############################################################################### # Get aggregrate stats for all ports ############################################################################### set aggregate_stats [::ixia::traffic_stats -port_handle $port_handle] if {[keylget aggregate_stats status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggregate_stats log]" } puts "\n\t\t########################" puts "\t\t# STATIC STATS #" puts "\t\t########################" puts "\n******************* FINAL COUNT STATS **********************" puts "\t\t\t\t$port_one\t\t$port_two" puts "\t\t\t\t-----\t\t-----" post_stats $port_handle "Elapsed Time" $aggregate_stats \ aggregate.tx.elapsed_time post_stats $port_handle "Packets Tx" $aggregate_stats \ aggregate.tx.pkt_count post_stats $port_handle "Raw Packets Tx" $aggregate_stats \ aggregate.tx.raw_pkt_count post_stats $port_handle "Bytes Tx" $aggregate_stats \ aggregate.tx.pkt_byte_count post_stats $port_handle "Bits Tx" $aggregate_stats \ aggregate.tx.pkt_bit_count post_stats $port_handle "Packets Rx" $aggregate_stats \ aggregate.rx.pkt_count post_stats $port_handle "Raw Packets Rx" $aggregate_stats \ aggregate.rx.raw_pkt_count post_stats $port_handle "Collisions" $aggregate_stats \ aggregate.rx.collisions_count post_stats $port_handle "Dribble Errors" $aggregate_stats \ aggregate.rx.dribble_errors_count post_stats $port_handle "CRCs" $aggregate_stats \ aggregate.rx.crc_errors_count post_stats $port_handle "Oversizes" $aggregate_stats \ aggregate.rx.oversize_count post_stats $port_handle "Undersizes" $aggregate_stats \ aggregate.rx.undersize_count post_stats $port_handle "Data Integrity Frames" $aggregate_stats \ aggregate.rx.data_int_frames_count post_stats $port_handle "Data Integrity Error" $aggregate_stats \ aggregate.rx.data_int_errors_count post_stats $port_handle "Sequence Frames" $aggregate_stats \ aggregate.rx.sequence_frames_count post_stats $port_handle "Sequence Error" $aggregate_stats \ aggregate.rx.sequence_errors_count puts "******************************************************\n" ################################################################################ # Get per stream stats ################################################################################ set rx_stream_stats [::ixia::traffic_stats \ -port_handle $port_handle \ -mode streams \ -streams $stream_index_list ] foreach {stream} $stream_index_list { puts "\n********** PER-STREAM STATS - STREAM $stream**********" puts [format "%-15s %-15s %-15s" [string repeat " " 15] \ $port_one $port_two] puts [format "%-15s %-15s %-15s" [string repeat " " 15] \ [string repeat "-" 5] [string repeat "-" 5]] post_stats $port_handle "Packets Tx" $rx_stream_stats tx.total_pkts \ $stream post_stats $port_handle "Time Tx" $rx_stream_stats tx.elapsed_time \ $stream post_stats $port_handle "Packets Rx" $rx_stream_stats rx.total_pkts \ $stream post_stats $port_handle "Bytes Rx" $rx_stream_stats rx.total_pkt_bytes \ $stream post_stats $port_handle "Bits Rate" $rx_stream_stats rx.total_pkt_bit_rate \ $stream post_stats $port_handle "Line Rate" $rx_stream_stats rx.line_rate_percentage \ $stream post_stats $port_handle "Average Delay" $rx_stream_stats rx.avg_delay \ $stream post_stats $port_handle "Min. Delay" $rx_stream_stats rx.min_delay \ $stream post_stats $port_handle "Max. Delay" $rx_stream_stats rx.max_delay \ $stream puts "******************************************************\n" } return "SUCCESS - $test_name - [clock format [clock seconds]]"