################################################################################ # Version 1.0 $Revision: 1 $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. ## # Description: Configures tx and rx ports for sequence checking. Prints # out the statistics on the sequence_frames and sequence_errors # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample configures two ports for Qos stats, creates a stream and # # starts it. Then prints the qos stats. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested with HLTSET26. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 2/3 2/4] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set tx_port [lindex $port_handle 0] set rx_port [lindex $port_handle 1] ######## # IpV4 # ######## set ipV4_ixia_list "1.1.1.2 1.1.1.1" set ipV4_gateway_list "1.1.1.1 1.1.1.2" set ipV4_netmask_list "255.255.255.0 255.255.255.0" set ipV4_mac_list "0000.debb.0001 0000.debb.0002" set ipV4_version_list "4 4" set ipV4_autoneg_list "1 1" set ipV4_duplex_list "full full" set ipV4_speed_list "ether100 ether100" ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -intf_ip_addr $ipV4_ixia_list \ -gateway $ipV4_gateway_list \ -netmask $ipV4_netmask_list \ -autonegotiation $ipV4_autoneg_list \ -duplex $ipV4_duplex_list \ -src_mac_addr $ipV4_mac_list \ -port_rx_mode {packet_group} \ -sequence_checking 0 \ -signature a1b1c1d1 \ -signature_offset 80 \ -pgid_offset 84 \ -qos_stats 1 \ -speed $ipV4_speed_list ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } # Delete all the streams first set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $tx_port ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } # Configure stream 1 set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $tx_port \ -l3_protocol ipv4 \ -ip_src_addr 12.1.1.1 \ -ip_dst_addr 12.1.1.2 \ -l3_length 100 \ -rate_percent 50 \ -mac_dst_mode discovery \ -mac_src 0000.0005.0001 \ -signature a1b1c1d1 \ -signature_offset 80 \ -enable_pgid 1 \ -pgid_value 7 \ ] if {[keylget traffic_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_status log]" } set interface_status [::ixia::interface_config \ -port_handle $tx_port \ -arp_send_req 1 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } if {[catch {set failed_arp [keylget interface_status \ $tx_port.arp_request_success]}] || $failed_arp == 0} { set returnLog "FAIL - $test_name arp send request failed. " if {![catch {set intf_list [keylget interface_status $tx_port.arp_ipv4_interfaces_failed]}]} { append returnLog "ARP failed on interfaces: $intf_list." } return $returnLog } ######################################## # Traffic control # ######################################## # Clear stats before sending traffic set clear_stats_status [::ixia::traffic_control \ -port_handle $port_handle \ -action clear_stats ] if {[keylget clear_stats_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget clear_stats_status log]" } # Start the traffic on TX port set traffic_start_status [::ixia::traffic_control \ -port_handle $tx_port \ -action run ] if {[keylget traffic_start_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_start_status log]" } # Sleep 5 seconds ixia_sleep 5000 # Stop traffic on the TX port set traffic_stop_status [::ixia::traffic_control \ -port_handle $tx_port \ -action stop ] if {[keylget traffic_stop_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget traffic_stop_status log]" } ############################################################################### # Retrieve stats after stopped ############################################################################### # Get aggregrate stats for all ports set aggregate_stats [::ixia::traffic_stats -port_handle $port_handle -qos_stats] if {[keylget aggregate_stats status] != $::SUCCESS} { return "FAIL - $test_name - [keylget aggregate_stats log]" } proc post_stats {port_handle label key_list stat_key {stream ""}} { puts -nonewline [format "%-25s" $label] foreach port $port_handle { if {$stream != ""} { set key $port.stream.$stream.$stat_key } else { set key $port.$stat_key } puts -nonewline "[format "%-16s" [keylget key_list $key]]" } puts "" } puts "\n\t\t########################" puts "\t\t# STATIC STATS #" puts "\t\t########################" puts "\n******************* STATS **********************" puts "[format "%30s%16s" $tx_port $rx_port]" puts "[format "%30s%16s" ----- -----]" post_stats $port_handle "Elapsed Time" $aggregate_stats \ aggregate.tx.elapsed_time post_stats $port_handle "Packets Tx" $aggregate_stats aggregate.tx.pkt_count post_stats $port_handle "Packets Rx" $aggregate_stats aggregate.rx.pkt_count post_stats $port_handle "Qos0 count" $aggregate_stats aggregate.rx.qos0_count post_stats $port_handle "Qos1 count" $aggregate_stats aggregate.rx.qos1_count post_stats $port_handle "Qos2 count" $aggregate_stats aggregate.rx.qos2_count post_stats $port_handle "Qos3 count" $aggregate_stats aggregate.rx.qos3_count post_stats $port_handle "Qos4 count" $aggregate_stats aggregate.rx.qos4_count post_stats $port_handle "Qos5 count" $aggregate_stats aggregate.rx.qos5_count post_stats $port_handle "Qos6 count" $aggregate_stats aggregate.rx.qos6_count post_stats $port_handle "Qos7 count" $aggregate_stats aggregate.rx.qos7_count post_stats $port_handle "Qos0 rate" $aggregate_stats aggregate.rx.qos0_rate post_stats $port_handle "Qos1 rate" $aggregate_stats aggregate.rx.qos1_rate post_stats $port_handle "Qos2 rate" $aggregate_stats aggregate.rx.qos2_rate post_stats $port_handle "Qos3 rate" $aggregate_stats aggregate.rx.qos3_rate post_stats $port_handle "Qos4 rate" $aggregate_stats aggregate.rx.qos4_rate post_stats $port_handle "Qos5 rate" $aggregate_stats aggregate.rx.qos5_rate post_stats $port_handle "Qos6 rate" $aggregate_stats aggregate.rx.qos6_rate post_stats $port_handle "Qos7 rate" $aggregate_stats aggregate.rx.qos7_rate puts "*************************************************" return "SUCCESS - $test_name - [clock format [clock seconds]]"