################################################################################ # Version 1.0 $Revision: 1 $ # Author: Radu Antonescu # # Copyright © 1997 - 2007 by IXIA # All Rights Reserved. # # Revision Log: # 07-03-2007 RAntonescu - created sample # 10-17-2007 LRaicea - corected indentation and validated returned keys # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates two IPv4 streams on a port. # # # # Module: # # The sample was tested on a 2.5G MSM POS/SPR/RPR module. # # The sample was tested with HLTSET26. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 1/1 2/1] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle_list [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle_list $temp_port } } set port_0 [lindex $port_handle_list 0] set port_1 [lindex $port_handle_list 1] ################################################################################ # Configure interface in the test ################################################################################ set interface_status [::ixia::interface_config \ -port_handle [list $port_0 $port_1 ] \ -intf_mode [list frame_relay2427 frame_relay2427] \ -speed [list oc48 oc48 ] \ -phy_mode [list fiber fiber ] \ -rx_scrambling [list 0 0 ] \ -tx_scrambling [list 0 0 ] \ -data_integrity [list 0 0 ] \ -transmit_mode [list advanced advanced ] \ -intf_ip_addr [list 12.1.3.2 12.1.3.1 ] \ -gateway [list 12.1.3.1 12.1.3.2 ] \ -netmask [list 255.255.255.0 255.255.255.0 ] \ -autonegotiation [list 0 0 ] \ -src_mac_addr [list 0000.0005.0001 0000.0001.0002 ] ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ################################################################################ # Delete all the streams first ################################################################################ set traffic_status [::ixia::traffic_config \ -mode reset \ -port_handle $port_0 ] if {[keylget traffic_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_status log]" return } ################################################################################ # Configure stream ################################################################################ set traffic_status [::ixia::traffic_config \ -mode create \ -port_handle $port_0 \ -l3_protocol ipv4 \ -ip_src_addr 12.1.1.1 \ -ip_dst_addr 12.1.1.2 \ -rate_percent 50 \ -length_mode fixed \ -frame_size 128 \ -l2_encap ietf_framerelay \ -enable_time_stamp 0 \ -dlci_value 750 \ -dlci_count_mode increment \ -dlci_repeat_count 10 \ -fecn 1 \ -discard_eligible 1 \ ] if {[keylget traffic_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_status log]" return } ################################################################################ # Clear stats ################################################################################ set stat_control [::ixia::traffic_control \ -port_handle $port_1 \ -action clear_stats ] if {[keylget stat_control status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget stat_control log]" return } ################################################################################ # Start traffic ################################################################################ set traffic_control [::ixia::traffic_control \ -port_handle $port_0 \ -action run ] if {[keylget traffic_control status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_control log]" return } after 5000 ################################################################################ # Stop traffic ################################################################################ set traffic_control [::ixia::traffic_control \ -port_handle $port_0 \ -action stop ] if {[keylget traffic_control status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget traffic_control log]" return } ################################################################################ # Retrive statistics ################################################################################ set stat_status [::ixia::traffic_stats \ -port_handle $port_1 \ -mode aggregate ] if {[keylget stat_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget stat_status log]" return } puts "Packets received: [keylget stat_status $port_1.aggregate.rx.pkt_count]" return "SUCCESS - $test_name - [clock format [clock seconds]]"