################################################################################# # Version 1 $Revision: 1 $ # $Author: RCsutak $ # # Copyright © 1997 - 2014 by IXIA # All Rights Reserved. # # Revision Log: # 08-18-2014 RCsutak - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script connects to a star topology chassis chain, displays the # # information retrieved and demonstrates a few key retrievals. # # # # Module: # # The sample was tested on a LSM XMVDC16NG module. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } set test_name [info script] set chassis_ip [list master_chassis slave_1 slave_2 slave_3 slave_4] set ixnetwork_tcl_server localhost set port_list [list [list 4/1] [list] [list] [list 4/1] [list]] set master_chassis [list none master_chassis master_chassis master_chassis master_chassis] set chain_type star set errors 0 set chain_cables_length [list 0 3 6 3 6] if {$chain_type == "star"} { set connect_status [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -master_device $master_chassis \ -chain_type $chain_type \ -chain_cables_length $chain_cables_length \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } puts "Connected with star topology..." } else { set connect_status [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -tcl_server $tcl_server \ -master_device $master_chassis \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } puts "Connected with daisy topology..." } puts "\nPrinting full connection information tree ...\n" ::ixia::keylprint connect_status set port_1 [keylget connect_status port_handle.[lindex $chassis_ip 0].[lindex $port_list 0]] set port_2 [keylget connect_status port_handle.[lindex $chassis_ip 3].[lindex $port_list 3]] set port_handle [list $port_1 $port_2] set check_master [keylget connect_status connection.chassis.[lindex $chassis_ip 0].is_master_chassis] set check_chain_type [keylget connect_status connection.chassis.[lindex $chassis_ip 0].chain_type] puts "Script ran SUCCESSFULLY!" return 1