################################################################################ # Version 1.0 $Revision: 1 $ # # Copyright © 1997 - 2006 by IXIA # All Rights Reserved. # # Revision Log: # 02-26-2008 : Mircea Hasegan # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates SIP client and server configurations # # using TCP and BHCA. # # Client is simulating an ORIGINATECALL scenario an ENDCALL sccenario. # # At the end statistics are being retrieved. # # # # Module: # # The sample was tested on a ALM1000T8 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set tclServer sylvester set port_list [list 2/3 2/4] set error "" catch { set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" } set client_port [keylget \ connect_status port_handle.$chassisIP.[lindex $port_list 0]] set server_port [keylget \ connect_status port_handle.$chassisIP.[lindex $port_list 1]] ################################################################################ # Client network ################################################################################ set client_network [::ixia::L47_network \ -target client \ -property network \ -mode add \ -port_handle $client_port \ -grat_arp_enable 0 ] if {[keylget client_network status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_network log]" } set client_network_handle [keylget client_network network_handle] ################################################################################ # Client network pool ################################################################################ set client_network_range [::ixia::L47_network \ -handle $client_network_handle \ -property network_pool \ -mode add \ -np_first_ip "198.18.0.1" \ -np_network_mask "255.255.0.0" \ -np_ip_incr_step "0.0.0.1" \ -np_first_mac "00:C6:12:02:01:00" \ -np_mac_incr_step "00.00.00.00.00.01" \ -np_ip_count 2000 ] if {[keylget client_network_range status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_network_range log]" } set client_network_range_handle [keylget client_network_range network_pool_handle] ################################################################################ # Server network ################################################################################ set server_network [::ixia::L47_network \ -target server \ -property network \ -mode add \ -port_handle $server_port \ -grat_arp_enable 0 ] if {[keylget server_network status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_network log]" } set server_network_handle [keylget server_network network_handle] ################################################################################ # Server network pool ################################################################################ set server_network_range [::ixia::L47_network \ -handle $server_network_handle \ -property network_pool \ -mode add \ -np_first_ip "198.18.101.0" \ -np_ip_count 2000 \ -np_network_mask "255.255.0.0" \ -np_gateway "0.0.0.0" \ -np_ip_incr_step "0.0.0.1" \ -np_first_mac "10:C6:12:02:02:00" \ -np_mac_incr_step "00.00.00.00.00.01" ] if {[keylget server_network_range status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_network_range log]" } set server_network_range_handle [keylget server_network_range network_pool_handle] ################################################################################ # Server traffic agent ################################################################################ set server_agent [::ixia::L47_sip_server \ -mode add \ -property server \ -sz_auth_domain "domain\[0000-\]"\ -sz_transport tcp \ -sz_auth_username "user\[0000-\]" \ -sz_auth_password "password\[0000-\]"\ -n_peer_dtmf_duration 100 \ -sz_peer_codec_name "G711ALaw" \ -sz_peer_codec_details "BF160PT20" \ -sz_peer_dtmf_seq "12345" \ -sz_codec_descr "ITU-T G.711 is a standard to represent 8 \ bit compressed pulse code modulation (PCM) \ samples for signals of voice frequencies, \ sampled at the rate of 8000 samples/second. \ G.711 encoder will create a 64 Kbps \ bitstream. A-Law G.711 PCM encoder converts \ 13 bit linear PCM samples into 8 bit \ compressed PCM (logarithmic form) samples, \ and the decoder does the conversion vice \ versa." \ -n_peer_dtmf_interdigits 40 \ -sz_codec_details "BF160PT20" \ -sz_contact "" \ -sz_from "" \ -sz_to "" \ ] if {[keylget server_agent status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_agent log]" } set server_traffic_handle [keylget server_agent server_handle] set server_agent_handle [keylget server_agent agent_handle] set server_status [::ixia::L47_sip_server \ -mode add \ -property scenarios \ -scenarios_id RECEIVEUSING180 \ -handle $server_agent_handle \ ] if {[keylget server_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget server_status log]" return } ################################################################################ # Client agent ################################################################################ set client_agent [::ixia::L47_sip_client \ -mode add \ -property client \ -sz_auth_domain "domain\[0000-\]"\ -sz_transport tcp \ -sz_auth_username "user\[0000-\]" \ -sz_auth_password "password\[0000-\]"\ -n_peer_dtmf_duration 100 \ -sz_peer_codec_name "G711ALaw" \ -sz_peer_codec_details "BF160PT20" \ -sz_peer_dtmf_seq "12345" \ -sz_codec_descr "ITU-T G.711 is a standard to represent 8 \ bit compressed pulse code modulation (PCM) \ samples for signals of voice frequencies, \ sampled at the rate of 8000 samples/second. \ G.711 encoder will create a 64 Kbps \ bitstream. A-Law G.711 PCM encoder converts \ 13 bit linear PCM samples into 8 bit \ compressed PCM (logarithmic form) samples, \ and the decoder does the conversion vice \ versa." \ -n_peer_dtmf_interdigits 40 \ -sz_codec_details "BF160PT20" \ -sz_contact "" \ -sz_from "" \ -sz_to "" \ -sz_requesturi "sip:id\[50000-\]@IP" \ ] if {[keylget client_agent status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget client_agent log]" return } set client_traffic_handle [keylget client_agent client_handle] set client_agent_handle [keylget client_agent agent_handle] ################################################################################ # Client commands ################################################################################ set scenario_1 [::ixia::L47_sip_client \ -mode add \ -property scenarios \ -scenarios_id ORIGINATECALL \ -handle $client_agent_handle \ -sym_destination $server_agent_handle \ ] if {[keylget scenario_1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget scenario_1 log]" } set scenario_handle1 [keylget scenario_1 scenarios_handle] set scenario_2 [::ixia::L47_sip_client \ -mode add \ -property scenarios \ -handle $client_agent_handle \ -scenarios_id ENDCALL \ ] if {[keylget scenario_2 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget scenario_2 log]" } set scenario_handle2 [keylget scenario_2 scenarios_handle] ################################################################################ # Client traffic-network mapping ################################################################################ set map_status [::ixia::L47_client_mapping \ -mode add \ -client_network_handle $client_network_handle \ -client_traffic_handle $client_traffic_handle \ -objective_type users \ -objective_value 200 ] if {[keylget map_status status] != $::SUCCESS} { return "FAIL - map_status - [keylget map_status log]" } set client_map1 [keylget map_status handles] ################################################################################ # Server traffic-network mapping ################################################################################ set map_status [::ixia::L47_server_mapping \ -mode add \ -server_network_handle $server_network_handle \ -server_traffic_handle $server_traffic_handle \ -match_client_total_time 1 \ ] if {[keylget map_status status] != $::SUCCESS} { return "FAIL - map_status - [keylget map_status log]" } set server_map1 [keylget map_status handles] ################################################################################ # Test settings ################################################################################ set results_dir [pwd]/results/[clock seconds] set control_status [::ixia::L47_test \ -mode add \ -map_handle [list \ $client_map1 $server_map1]\ -force_ownership_enable 1 \ -reset_ports_enable 1 \ -stats_required 1 \ -results_dir_enable 1 \ -results_dir $results_dir ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } set test_handle [keylget control_status handles] ################################################################################ # Client statistics ################################################################################ set client_stats_list { sip_simulated_users sip_calls_initiated sip_calls_completed sip_calls_active } set stats_result [::ixia::L47_stats \ -mode add \ -aggregation_type sum \ -stat_name $client_stats_list \ -stat_type client \ -protocol sip ] if {[keylget stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget stats_result log]" } set client_stat_handle [keylget stats_result handles] ################################################################################ # Server statitics ################################################################################ set server_stats_list { sip_calls_received sip_calls_completed sip_calls_active } set stats_result [::ixia::L47_stats \ -mode add \ -aggregation_type sum \ -stat_name $server_stats_list \ -stat_type server \ -protocol sip ] if {[keylget stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget stats_result log]" } set server_stat_handle [keylget stats_result handles] ################################################################################ # Start test ################################################################################ set control_status [::ixia::L47_test \ -handle $test_handle \ -mode start ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } ################################################################################ # Get statistics ################################################################################ set client_stats_result [::ixia::L47_stats \ -mode get \ -handle $client_stat_handle ] if {[keylget client_stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_stats_result log]" } set server_stats_result [::ixia::L47_stats \ -mode get \ -handle $server_stat_handle ] if {[keylget server_stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_stats_result log]" } ################################################################################ # Print client statistics ################################################################################ # The stat_required variable can be changed to print only one of the statistics # e.g set stat_required telnet_active_conn set stat_required "all" puts "CLIENT STATISTICS:" foreach {stat_handle} [keylkeys client_stats_result] { if {$stat_handle != "status"} { set stat_handle_kl [keylget client_stats_result $stat_handle] foreach {stat_type} [keylkeys stat_handle_kl] { set stat_type_kl [keylget stat_handle_kl $stat_type] foreach {stat_name} [keylkeys stat_type_kl] { if {$stat_name != $stat_required && $stat_required != "all" } { continue } set stat_name_kl [keylget stat_type_kl $stat_name] foreach {time_stamp} $stat_name_kl { foreach {key value} $time_stamp { if {$key == ""} { set key N/A } if {$value == ""} { set value N/A } puts -nonewline [format \ "%10s %10s %40s" $stat_handle $stat_type $stat_name] puts [format "%15s %15s" $key $value] } } } } } } ################################################################################ # Print server statistics ################################################################################ set stat_required "all" puts "Server STATISTICS:" foreach {stat_handle} [keylkeys server_stats_result] { if {$stat_handle != "status"} { set stat_handle_kl [keylget server_stats_result $stat_handle] foreach {stat_type} [keylkeys stat_handle_kl] { set stat_type_kl [keylget stat_handle_kl $stat_type] foreach {stat_name} [keylkeys stat_type_kl] { if {$stat_name != $stat_required && $stat_required != "all" } { continue } set stat_name_kl [keylget stat_type_kl $stat_name] foreach {time_stamp} $stat_name_kl { foreach {key value} $time_stamp { if {$key == ""} { set key N/A } if {$value == ""} { set value N/A } puts -nonewline [format \ "%10s %10s %40s" $stat_handle $stat_type $stat_name] puts [format "%15s %15s" $key $value] } } } } } } } error set cleanup_status [::ixia::cleanup_session ] if {[keylget cleanup_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget cleanup_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"