################################################################################ # Version 1.0 $Revision: 1 $ # # Copyright © 1997 - 2006 by IXIA # All Rights Reserved. # # Revision Log: # 3-09-2007 : Mircea Hasegan # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates a Telnet client and server basic configuration. # # Client is simulating the following commands: OPEN, LOGIN, PASSWORD, THINK # # and EXIT. # # Telnet traffic is sent from clent side to server side. # # At the end statistics are being retrieved. # # # # Module: # # The sample was tested on a ALM1000T8 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set tclServer winston-400t set port_list [list 4/1 4/2] set error "" catch { set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" } set client_port [keylget \ connect_status port_handle.$chassisIP.[lindex $port_list 0]] set server_port [keylget \ connect_status port_handle.$chassisIP.[lindex $port_list 1]] ################################################################################ # Client network ################################################################################ set client_network [::ixia::L47_network \ -target client \ -property network \ -mode add \ -port_handle $client_port \ -grat_arp_enable 0 ] if {[keylget client_network status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_network log]" } set client_network_handle [keylget client_network network_handle] ################################################################################ # Client network pool ################################################################################ set client_network_range [::ixia::L47_network \ -handle $client_network_handle \ -property network_pool \ -mode add \ -np_first_ip "198.18.2.1" \ -np_network_mask "255.255.0.0" \ -np_ip_incr_step "0.0.0.1" \ -np_first_mac "00:C6:12:02:01:00" \ -np_mac_incr_step "00.00.00.00.00.01" \ -np_ip_count 100 \ -np_gateway "0.0.0.0" \ -np_enable_stats 1 ] if {[keylget client_network_range status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_network_range log]" } set client_network_range_handle [keylget client_network_range network_pool_handle] ################################################################################ # Server network ################################################################################ set server_network [::ixia::L47_network \ -target server \ -property network \ -mode add \ -port_handle $server_port \ -grat_arp_enable 0 ] if {[keylget server_network status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_network log]" } set server_network_handle [keylget server_network network_handle] ################################################################################ # Server network pool ################################################################################ set server_network_range [::ixia::L47_network \ -handle $server_network_handle \ -property network_pool \ -mode add \ -np_first_ip "198.18.200.1" \ -np_ip_count 1 \ -np_network_mask "255.255.0.0" \ -np_gateway "0.0.0.0" \ -np_ip_incr_step "0.0.0.1" \ -np_first_mac "00:C6:12:02:02:00" \ -np_mac_incr_step "00.00.00.00.00.01" ] if {[keylget server_network_range status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_network_range log]" } set server_network_range_handle [keylget server_network_range network_pool_handle] ################################################################################ # Server traffic agent ################################################################################ set server_agent [::ixia::L47_telnet_server \ -property server \ -mode add \ -close_command exit \ -command_prompt # \ -echo_enable 1 \ -linemode_enable 1 \ -suppress_go_ahead 0 \ -listen_port 23 ] if {[keylget server_agent status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_agent log]" } set server_traffic_handle [keylget server_agent server_handle] set server_agent_handle [keylget server_agent agent_handle] ################################################################################ # Server traffic-network mapping ################################################################################ set map_status [::ixia::L47_server_mapping \ -mode add \ -server_network_handle $server_network_handle \ -server_traffic_handle $server_traffic_handle \ -match_client_total_time 1 \ ] if {[keylget map_status status] != $::SUCCESS} { return "FAIL - map_status - [keylget map_status log]" } set server_map1 [keylget map_status handles] ################################################################################ # Client agent ################################################################################ set client_agent [::ixia::L47_telnet_client \ -property client \ -mode add \ -options_enable 1 \ -command_prompt # \ -expect_timeout 10 ] if {[keylget client_agent status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_agent log]" } set client_traffic_handle [keylget client_agent client_handle] set client_agent_handle [keylget client_agent agent_handle] ################################################################################ # Client commands ################################################################################ set command_1 [::ixia::L47_telnet_client \ -handle $client_agent_handle \ -property command \ -mode add \ -c_id open \ -c_expect login: \ -c_server_ip "198.18.200.1" ] if {[keylget command_1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget command_1 log]" } set command_handle1 [keylget command_1 command_handle] set command_2 [::ixia::L47_telnet_client \ -handle $client_agent_handle \ -mode add \ -property command \ -c_id login \ -c_send ixia \ -c_expect password: ] if {[keylget command_2 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget command_2 log]" } set command_handle2 [keylget command_2 command_handle] set command_3 [::ixia::L47_telnet_client \ -handle $client_agent_handle \ -mode add \ -property command \ -c_id password \ -c_send ixia \ -c_expect # ] if {[keylget command_3 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget command_3 log]" } set command_handle3 [keylget command_3 command_handle] set command_4 [::ixia::L47_telnet_client \ -handle $client_agent_handle \ -mode add \ -property command \ -c_id think \ -c_max_interval 10000 \ -c_min_interval 10000 ] if {[keylget command_4 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget command_4 log]" } set command_handle4 [keylget command_4 command_handle] set command_5 [::ixia::L47_telnet_client\ -handle $client_agent_handle \ -mode add \ -property command \ -c_id exit \ -c_send exit ] if {[keylget command_5 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget command_5 log]" } set command_handle5 [keylget command_5 command_handle] ################################################################################ # Client traffic-network mapping ################################################################################ set map_status [::ixia::L47_client_mapping \ -mode add \ -client_network_handle $client_network_handle \ -client_traffic_handle $client_traffic_handle \ -objective_type users \ -objective_value 20 \ -ramp_up_value 5 \ -sustain_time 20 \ -ramp_down_time 20 \ -agent_handle $client_agent_handle \ -objective_type_for_activity crate \ -objective_value_for_activity 200 \ -port_map_for_activity mesh ] if {[keylget map_status status] != $::SUCCESS} { return "FAIL - map_status - [keylget map_status log]" } set client_map1 [keylget map_status handles] ################################################################################ # Test settings ################################################################################ set results_dir [pwd]/results/[clock seconds] set control_status [::ixia::L47_test \ -mode add \ -map_handle [list \ $client_map1 $server_map1]\ -force_ownership_enable 1 \ -reset_ports_enable 1 \ -stats_required 0 \ -results_dir_enable 1 \ -results_dir $results_dir ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } set test_handle [keylget control_status handles] ################################################################################ # Client statistics ################################################################################ set client_stats_list { telnet_active_conn telnet_total_conn_requested telnet_total_conn_succeeded telnet_total_conn_failed telnet_total_bytes_sent telnet_total_bytes_received telnet_total_bytes_sent_and_received } set stats_result [::ixia::L47_stats \ -mode add \ -aggregation_type sum \ -stat_name $client_stats_list \ -stat_type client \ -protocol telnet ] if {[keylget stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget stats_result log]" } set client_stat_handle [keylget stats_result handles] ################################################################################ # Server statitics ################################################################################ set server_stats_list { telnet_active_conn telnet_total_accepted_conn telnet_total_bytes_sent telnet_total_bytes_received } set stats_result [::ixia::L47_stats \ -mode add \ -aggregation_type sum \ -stat_name $server_stats_list \ -stat_type server \ -protocol telnet ] if {[keylget stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget stats_result log]" } set server_stat_handle [keylget stats_result handles] ################################################################################ # Start test ################################################################################ set control_status [::ixia::L47_test \ -handle $test_handle \ -mode start ] if {[keylget control_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget control_status log]" } ################################################################################ # Get statistics ################################################################################ set client_stats_result [::ixia::L47_stats \ -mode get \ -handle $client_stat_handle ] if {[keylget client_stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget client_stats_result log]" } set server_stats_result [::ixia::L47_stats \ -mode get \ -handle $server_stat_handle ] if {[keylget server_stats_result status] != $::SUCCESS} { return "FAIL - $test_name - [keylget server_stats_result log]" } ################################################################################ # Print client statistics ################################################################################ # The stat_required variable can be changed to print only one of the statistics # e.g set stat_required telnet_active_conn set stat_required "all" puts "CLIENT STATISTICS:" foreach {stat_handle} [keylkeys client_stats_result] { if {$stat_handle != "status"} { set stat_handle_kl [keylget client_stats_result $stat_handle] foreach {stat_type} [keylkeys stat_handle_kl] { set stat_type_kl [keylget stat_handle_kl $stat_type] foreach {stat_name} [keylkeys stat_type_kl] { if {$stat_name != $stat_required && $stat_required != "all" } { continue } set stat_name_kl [keylget stat_type_kl $stat_name] foreach {time_stamp} $stat_name_kl { foreach {key value} $time_stamp { if {$key == ""} { set key N/A } if {$value == ""} { set value N/A } puts -nonewline [format \ "%10s %10s %40s" $stat_handle $stat_type $stat_name] puts [format "%15s %15s" $key $value] } } } } } } ################################################################################ # Print server statistics ################################################################################ set stat_required "all" puts "Server STATISTICS:" foreach {stat_handle} [keylkeys server_stats_result] { if {$stat_handle != "status"} { set stat_handle_kl [keylget server_stats_result $stat_handle] foreach {stat_type} [keylkeys stat_handle_kl] { set stat_type_kl [keylget stat_handle_kl $stat_type] foreach {stat_name} [keylkeys stat_type_kl] { if {$stat_name != $stat_required && $stat_required != "all" } { continue } set stat_name_kl [keylget stat_type_kl $stat_name] foreach {time_stamp} $stat_name_kl { foreach {key value} $time_stamp { if {$key == ""} { set key N/A } if {$value == ""} { set value N/A } puts -nonewline [format \ "%10s %10s %40s" $stat_handle $stat_type $stat_name] puts [format "%15s %15s" $key $value] } } } } } } } error set cleanup_status [::ixia::cleanup_session ] if {[keylget cleanup_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget cleanup_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"