################################################################################# # Version 1 $Revision: 1 $ # $Author: RCsutak $ # # Copyright © 1997 - 2014 by IXIA # All Rights Reserved. # # Revision Log: # 11-20-2014 RCsutak - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample connects to an IxNetwork client and, using the HL API, # # adds cards to a virtual chassis and modifies some options or card # # configurations. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set chassis_ip 10.205.23.219 set ixnetwork_tcl_server localhost set test_name [info script] set test_name_folder [file dirname $test_name] set virtual_chassis 10.205.23.219 set cards [list 10.205.23.215 10.205.23.216 10.205.23.134 10.205.23.136 10.205.23.208 10.205.23.194] ################################################################################ # START - Connect to IxN client ################################################################################ set res [ixiangpf::connect \ -reset \ -vport_count 1 \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ ] if {[keylget res status] != $::SUCCESS} { puts "Connect failed: $res" return 0 } puts "Deleting all cards from chassis ...\n" set clear_chassis [::ixiangpf::ixvm_config \ -mode delete_all \ -virtual_chassis $virtual_chassis \ ] if {[keylget clear_chassis status] != $::SUCCESS} { puts "Delete failed: $clear_chassis" return 0 } puts "Creating first card, with 1 port ...\n" puts "====> CARD no 1\n" set keep_alive 250 set mtu 2000 set promisc_mode 1 set virtual_intf_count 1 set card_no 4 set card4 [::ixiangpf::ixvm_config \ -mode create \ -virtual_chassis $chassis_ip \ -management_ip [lindex $cards 3] \ -keep_alive $keep_alive \ -mtu $mtu \ -promiscuous_mode $promisc_mode \ -virtual_interface_count $virtual_intf_count \ -card_no $card_no \ ] if {[keylget card4 status] != $::SUCCESS} { puts "Card failed: $card4" return 0 } puts "Adding another 8 ports, using a list ...\n" set port_no [list 2 4 6 8 3 5 7] set mtu_list [list 1550 1660 2000] set add_ports [::ixiangpf::ixvm_config \ -mode modify \ -virtual_chassis $chassis_ip \ -port_action add \ -management_ip [lindex $cards 3] \ -virtual_interface_count [llength $port_no] \ -port_no $port_no \ -card_no $card_no \ -mtu $mtu_list \ -promiscuous_mode 1 \ ] if {[keylget add_ports status] != $::SUCCESS} { puts "Add ports FAILED: $add_ports" return 0 } puts "Creating card with virtual_interface_list, 5 ports ...\n" puts "====> CARD no 13\n" set keep_alive5 1500 set mtu5 3000 set promisc_mode5 0 set intf_list [list eth1 eth2 eth3 eth7 eth9] set card_no5 13 set card5 [::ixiangpf::ixvm_config \ -mode create \ -virtual_chassis $chassis_ip \ -management_ip [lindex $cards 4] \ -keep_alive $keep_alive5 \ -mtu $mtu5 \ -promiscuous_mode $promisc_mode5 \ -virtual_interface_list $intf_list \ -card_no $card_no5 \ ] if {[keylget card5 status] != $::SUCCESS} { puts "Card failed: $card5" return 0 } puts "Modifying card by adding ports ...\n" set mtu5 [list 1550 1660 1770] set port_no5 [list 6 8 7] set add_ports [::ixiangpf::ixvm_config \ -mode modify \ -virtual_chassis $chassis_ip \ -port_action add \ -card_no $card_no5 \ -virtual_interface_count 3 \ -port_no $port_no5 \ -mtu $mtu5 \ ] if {[keylget add_ports status] != $::SUCCESS} { puts "Add ports FAILED: $add_ports" return 0 } puts "Creating card with both virtual_interface_list and count ...\n" puts "====> CARD no 6\n" set mtu6 1800 set promisc_mode6 1 set intf_list6 [list eth1 eth3 eth5 eth7 eth8 eth9] set intf_count6 2 set card6 [::ixiangpf::ixvm_config \ -mode create \ -virtual_chassis $chassis_ip \ -management_ip [lindex $cards 5] \ -mtu $mtu6 \ -promiscuous_mode $promisc_mode6 \ -virtual_interface_list $intf_list6 \ -virtual_interface_count $intf_count6 \ ] if {[keylget card6 status] != $::SUCCESS} { puts "Card failed: $card6" return 0 } puts "Script has finished SUCCESSFULLY!\n" return 1