################################################################################# # Version 1 $Revision: 1 $ # $Author: RCsutak $ # # Copyright © 1997 - 2014 by IXIA # All Rights Reserved. # # Revision Log: # 11-20-2014 RCsutak - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample connects to an IxNetwork client and, using the HL API, # # deletes all cards present on a virtual chassis and rebuilds a topology # # from the devices discovered over the network. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set chassis_ip 10.205.23.219 set ixnetwork_tcl_server localhost set test_name [info script] set test_name_folder [file dirname $test_name] set virtual_chassis 10.205.23.219 ################################################################################ # START - Connect to IxN client ################################################################################ set res [ixiangpf::connect \ -reset \ -vport_count 1 \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ ] if {[keylget res status] != $::SUCCESS} { puts "Connect failed: $res" return 0 } puts "Deleting all cards from chassis ...\n" set clear_chassis [::ixiangpf::ixvm_config \ -mode delete_all \ -virtual_chassis $virtual_chassis \ ] if {[keylget clear_chassis status] != $::SUCCESS} { puts "Delete failed: $clear_chassis" return 0 } puts "Rebuilding topology from discovered devices ...\n" set rebuild [::ixiangpf::ixvm_config \ -mode create \ -virtual_chassis $chassis_ip \ -rediscover 1 \ -rebuild_from_discovery 1 \ ] if {[keylget rebuild status] != $::SUCCESS} { puts "Card failed: $rebuild" return 0 } puts "Script has finished SUCCESSFULLY!\n" return 1