################################################################################# # Version 1 $Revision: 1 $ # $Author: RCsutak $ # # Copyright © 1997 - 2014 by IXIA # All Rights Reserved. # # Revision Log: # 08-20-2014 RCsutak - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample connects to an IxNetwork client and to a virtual chassis. # # Using 18 virtual ports, the script sets different speeds from all the # # options available in the documentation. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set chassis_ip "ip of the vm chassis" # use an 18 ports list set port_list [list 1/1 1/2 1/3 1/4 1/5 1/6 1/7 1/8 1/9 2/1 2/2 2/3 2/4 2/5 2/6 2/7 2/8 2/9] set tcl_server localhost set ixnetwork_tcl_server localhost set test_name [info script] set test_name_folder [file dirname $test_name] set license_type subscription_tier3 set license_server "the ip/hostname of a server that has the appropriate license type" ################################################################################ # START - Connect to the chassis and Load IxNetwork config ################################################################################ set res [ixia::connect \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -tcl_server $tcl_server \ -device $chassis_ip \ -port_list $port_list \ -reset 1 \ ] if {[keylget res status] != $::SUCCESS} { puts "connect failed: $res" return 0 } puts stderr [::ixia::keylprint $res] set port_list [keylget res vport_list] set 100_port_list [lrange $port_list 0 3] set 1000_port_list [lindex $port_list 4] set 2000_port_list [lindex $port_list 5] set 3000_port_list [lindex $port_list 6] set 4000_port_list [lindex $port_list 7] set 5000_port_list [lindex $port_list 8] set 6000_port_list [lindex $port_list 9] set 7000_port_list [lrange $port_list 10 12] set 8000_port_list [lindex $port_list 13] set 9000_port_list [lrange $port_list 14 16] set 10000_port_list [lindex $port_list 17] set final_list [list $100_port_list $1000_port_list $2000_port_list $3000_port_list $4000_port_list $5000_port_list $6000_port_list $7000_port_list $8000_port_list $9000_port_list $10000_port_list] set speed_list [list ether100vm ether1000vm ether2000vm ether3000vm ether4000vm ether5000vm ether6000vm ether7000vm ether8000vm ether9000vm ether10000vm] set final_list_no [llength $final_list] foreach ports $final_list speed $speed_list { puts "Setting speed $speed on ports $ports\n" set port_speed_$speed [ixia::interface_config \ -port_handle $ports \ -speed $speed \ ] if {[keylget port_speed_$speed status] != $::SUCCESS} { puts "connect failed: $port_speed_$speed" return 0 } puts "Passed!\n" } puts "SUCCESS - [clock format [clock seconds] -format {%D %X}]" return 1