################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Mircea Hasegan $ # # Copyright © 1997 - 2007 by IXIA # All Rights Reserved. # # Revision Log: # 9-12-2008 Mircea Hasegan # 3-17-2009 Adrian Iliesiu ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample creates a BACK-TO-BACK setup. # # # # It configures two IPv4 Ethernet interfaces and configures Ethernet OAM # # using sequence_id and sequence_id_step parameters # # Module: # # The sample was tested on a TXS4 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 1/1 1/2] # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -ixnetwork_tcl_server localhost \ -device $chassisIP \ -port_list $port_list ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set port_0 [lindex $port_handle 0] set port_1 [lindex $port_handle 1] puts "Ixia port handles are $port_handle " ######################################## # L1 configurations # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_0 \ -mode config \ -speed auto \ -duplex auto \ -phy_mode copper \ -autonegotiation 1 ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return } set interface_status [::ixia::interface_config \ -port_handle $port_1 \ -mode config \ -speed auto \ -duplex auto \ -phy_mode copper \ -autonegotiation 1 ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return } ########################################################################## # Configure Ethernet OAM port, Information and Event Notification OAMPDU # ########################################################################## puts "\nConfiguring Ethernet OAM" set efm_status [::ixia::emulation_efm_config \ -port_handle $port_0 \ -oam_mode active \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -size 512 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } set efm_status [::ixia::emulation_efm_config \ -port_handle $port_0 \ -oam_mode active \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -size 512 \ -sequence_id 15 \ -sequence_id_step 10 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } set efm_status [::ixia::emulation_efm_config \ -port_handle $port_0 \ -oam_mode active \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -size 512 \ -sequence_id 50 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } set efm_status [::ixia::emulation_efm_config \ -port_handle $port_1 \ -oam_mode passive \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -size 512 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } set efm_status [::ixia::emulation_efm_config \ -port_handle $port_1 \ -oam_mode passive \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -sequence_id 13 \ -sequence_id_step 10 \ -size 512 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } set efm_status [::ixia::emulation_efm_config \ -port_handle $port_1 \ -oam_mode passive \ -link_events \ -variable_retrieval \ -error_frame_count 5 \ -error_frame_period_count 6 \ -error_frame_period_threshold 66 \ -error_frame_period_window 660 \ -error_frame_threshold 55 \ -error_frame_window 550 \ -error_frame_summary_count 7 \ -error_frame_summary_threshold 77 \ -error_frame_summary_window 770 \ -error_symbol_period_count 8 \ -error_symbol_period_threshold 88 \ -error_symbol_period_window 880 \ -sequence_id 100 \ -size 512 \ ] if {[keylget efm_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_status log]" return } return "SUCCESS - $test_name - [clock format [clock seconds]]"