################################################################################ # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2009 by IXIA # All Rights Reserved. # # Revision Log: # 07-08-2007 LRaicea - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures Ethernet OAM on the Ixia port. # # Ixia port is connected to Cisco 7200 Router. # # EFM is started on the Ixia port and statistics are collected. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested with HLTSET50. # # # ################################################################################ ################################################################################ # # # DUT configuration: # # # configure terminal # # default interface GigabitEthernet0/2 # # interface GigabitEthernet0/2 # no shutdown # ethernet oam # ethernet oam mode active # ethernet oam link-monitor supported # ethernet oam link-monitor on # ethernet oam link-monitor frame window 600 # ethernet oam link-monitor frame threshold high 3 # ethernet oam link-monitor receive-crc window 300 # ethernet oam link-monitor receive-crc threshold high 12 # ip address 192.168.1.1 255.255.255.0 # exit # end ################################################################################ set env(IXIA_VERSION) HLTSET50 if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set test_name [info script] ################################################################################ # Connect to the chassis ################################################################################ puts "Start connecting to chassis ..." update idletasks set chassis_ip 10.205.17.50 set port_list [list 2/1] set connect_status [::ixia::connect \ -reset \ -device $chassis_ip \ -port_list $port_list \ -break_locks 1 \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassis_ip.$port} \ temp_port]} { lappend port_handle $temp_port } } set i 0 puts "Ixia port handles are:" foreach port $port_handle { set port_$i $port puts $port # Initialize per port variables set interface_handles_$port "" incr i } puts "End connecting to chassis ..." update idletasks ################################################################################ # START - Interface configuration ################################################################################ puts "Start interface configuration ..." update idletasks set interface_status [::ixia::interface_config \ -port_handle $port_0 \ -mode config \ -intf_mode ethernet \ -autonegotiation 1 \ -speed auto \ -duplex auto \ -src_mac_addr 00aa.00bb.cc01 \ -intf_ip_addr 192.168.1.100 \ -gateway 192.168.1.1 \ -netmask 255.255.255.0 \ -ipv6_intf_addr 100::2 \ -ipv6_prefix_length 64 \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return } lappend interface_handles_$port_0 [keylget interface_status interface_handle] puts "End interface configuration ..." update idletasks ################################################################################ # Additional procedures ################################################################################ proc printStats {keyedList} { set statsList { statistics.mac_remote "Remote MAC Address" statistics.oam_mode "OAM Mode" statistics.unidir_enabled "Unidirectional Support" statistics.remote_loopback_enabled "Loopback Support" statistics.link_events_enabled "Link Events Support" statistics.variable_retrieval_enabled "Variable Retrieval Support" statistics.oampdu_size "Max OAM PDU size" statistics.oampdu_count.information_tx "EOAM Information PDUs Sent" statistics.oampdu_count.information_rx "EOAM Information PDUs Received" statistics.oampdu_count.event_notification_rx "EOAM Event Notification PDUs Received" statistics.oampdu_count.loopback_control_rx "EOAM Loopback Control PDUs Received" statistics.oampdu_count.organization_rx "EOAM Organization PDUs Received" statistics.oampdu_count.variable_request_rx "EOAM Variable Request PDUs Received" statistics.oampdu_count.variable_response_rx "EOAM Variable Response PDUs Received" statistics.oampdu_count.unsupported_rx "EOAM Unsupported PDUs Received" statistics.oampdu_count.total_rx "EOAM Total PDUs Received" statistics.oui_value "OUI" statistics.vsi_value "Vendor Specific Information" } puts "Statistics for Port Handle [keylget keyedList port_handle]:" foreach {statKey statName} $statsList { puts "\t[format {%-45s%-25s} $statName [keylget keyedList $statKey]]" } puts "\n\n" } ################################################################################ # START - EFM configuration ################################################################################ puts "Start EFM configuration ..." update idletasks set efm_config_status [::ixia::emulation_efm_config \ -api_used ixprotocol \ -port_handle $port_0 \ -error_frame_period_threshold 30 \ -error_frame_period_window 300 \ -error_frame_summary_threshold 30 \ -error_frame_summary_window 300 \ -error_frame_threshold 40 \ -error_frame_window 400 \ -error_symbol_period_threshold 50 \ -error_symbol_period_window 500 \ -oam_mode passive \ -oui_value 00aabb \ -size 256 \ -vsi_value 00aabbcc \ -disable_information_pdu_tx 0 \ -disable_non_information_pdu_tx 0 \ -enable_loopback_response 1 \ -enable_variable_response 1 \ -event_interval 1 \ -error_frame_count 40 \ -error_frame_period_count 30 \ -error_frame_summary_count 30 \ -error_symbol_period_count 50 \ -information_pdu_rate 1 \ -link_event_tx_mode periodic \ -local_lost_link_timer 5 \ -loopback_cmd enable_oam_remote_loopback \ -loopback_timeout 10 \ -supports_remote_loopback 0 \ -supports_unidir_mode 0 \ -variable_response_timeout 1 \ -link_events 1 \ -variable_retrieval 0 \ -os_oampdu_data_oui 0x000000 \ ] if {[keylget efm_config_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget efm_config_status log]" return 0 } ###################### # Start Ethernet OAM # ###################### puts "\nStarting Ethernet OAM" set control_status [::ixia::emulation_efm_control \ -api_used ixprotocol \ -port_handle $port_0 \ -action start \ ] if {[keylget control_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget control_status log]" return 0 } ############################################################## # Get and print Ethernet OAM statistics while OAM is running # ############################################################## set retry_count 5 for {set retry_iteration 0} {$retry_iteration < $retry_count} {incr retry_iteration} { after 5000 puts "\nRetry iteration $retry_iteration - port $port_0" set pass_break 1 set stat_status1 [::ixia::emulation_efm_stat \ -api_used ixprotocol \ -port_handle $port_0 \ -action get \ ] if {[keylget stat_status1 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget stat_status1 log]" return 0 } printStats $stat_status1 if {[keylget stat_status1 statistics.oam_mode] != "active"} { set errMsg "FAIL - $test_name - OAM Mode error.\nExpected: active\ \nActual:[keylget stat_status1 statistics.oam_mode]" set pass_break 0 } if {[keylget stat_status1 statistics.link_events_enabled] != "Supported"} { set errMsg "FAIL - $test_name - Link Events error.\nExpected: Supported\ \nActual:[keylget stat_status1 statistics.link_events_enabled]" set pass_break 0 } if {[keylget stat_status1 statistics.variable_retrieval_enabled] != "Not Supported"} { set errMsg "FAIL - $test_name - Variable Retrieval error.\nExpected: Not Supported\ \nActual:[keylget stat_status1 statistics.variable_retrieval_enabled]" set pass_break 0 } if {$pass_break} { break } } if {!$pass_break} { puts $errMsg return 0 } ############################################################## # EFM was negotiated with DUT. Send Link Events. # ############################################################## puts "\nSend Ethernet OAM Event Notifications." set control_status [::ixia::emulation_efm_control \ -api_used ixprotocol \ -port_handle $port_0 \ -action start_event \ ] if {[keylget control_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget control_status log]" return 0 } after 50000 puts "\nStop Send Ethernet OAM Event Notifications." set control_status [::ixia::emulation_efm_control \ -api_used ixprotocol \ -port_handle $port_0 \ -action stop_event \ ] if {[keylget control_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget control_status log]" return 0 } ############################################################## # Check if event notificatoins were sent. # ############################################################## set stat_status1 [::ixia::emulation_efm_stat \ -api_used ixprotocol \ -port_handle $port_0 \ -action get \ ] if {[keylget stat_status1 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget stat_status1 log]" return 0 } set stats_check_list { statistics.oampdu_count.event_notification_tx "Event Notifications sent" statistics.alarms.errored_symbol_period_events_tx "Errored Symbol Period Event Running Total Tx" statistics.alarms.errored_symbol_period_errors_tx "Errored Symbol Period Error Running Total Tx" statistics.alarms.errored_frame_events_tx "Errored Frame Event Running Total Tx" statistics.alarms.errored_frame_errors_tx "Errored Frame Error Running Total Tx" statistics.alarms.errored_frame_period_events_tx "Errored Frame Period Event Running Total Tx" statistics.alarms.errored_frame_period_errors_tx "Errored Frame Period Error Running Total Tx" statistics.alarms.errored_frame_seconds_summary_events_tx "Errored Frame SS Event Running Total Tx" statistics.alarms.errored_frame_seconds_summary_errors_tx "Errored Frame SS Error Running Total Tx" } foreach {stat_key stat_desc} $stats_check_list { if {[keylget stat_status1 $stat_key] == 0} { puts "FAIL - $test_name - OAM $stat_key error.\n\ $stat_desc is 0." return 0 } } ###################### # Stop Ethernet OAM # ###################### puts "\nStopping Ethernet OAM" set control_status [::ixia::emulation_efm_control \ -api_used ixprotocol \ -port_handle $port_0 \ -action stop \ ] if {[keylget control_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget control_status log]" return 0 } puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1