################################################################################ # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2009 by IXIA # All Rights Reserved. # # Revision Log: # 07-08-2007 LRaicea - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates PBB bridges with custom TLVs and trunks, # # starts the protocol and retrieves learned information. # # The setup used are two ixia port connected back-to-back. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested with HLTSET51. # # # ################################################################################ set env(IXIA_VERSION) HLTSET51 if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set test_name [info script] set bridge_count 3 set trunk_count 2 set mr_count 2 ################################################################################ # Connect to the chassis ################################################################################ puts "Start connecting to chassis ..." update idletasks set chassis_ip 10.205.17.50 set port_list [list 2/1 2/2] # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -ixnetwork_tcl_server localhost \ -device $chassis_ip \ -port_list $port_list \ -break_locks 1 \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassis_ip.$port} \ temp_port]} { lappend port_handle $temp_port } } set i 0 puts "Ixia port handles are:" foreach port $port_handle { set port_$i $port puts $port # Initialize per port variables set interface_handles_$port "" incr i } puts "End connecting to chassis ..." update idletasks ################################################################################ # Interface configuration - L1 ################################################################################ puts "Start interface configuration L1 ..." update idletasks set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -mode config \ -intf_mode ethernet \ -autonegotiation 1 \ -speed auto \ -duplex auto \ -phy_mode copper \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return 0 } puts "End interface configuration L1 ..." update idletasks ################################################################################ # PBB bridge configuration ################################################################################ puts "\n### Start PBB bridge configuration ..." update idletasks set port 1 foreach port_h $port_handle { foreach {ch ca po} [split $port_h /] {} set bridge_id [format %02x $ch]:[format %02x $ca]:[format %02x $po]:00:AA:01 set mac_address_init [format %02x $ch]:[format %02x $ca]:[format %02x $po]:BB:00:01 set pbb_config_status [::ixia::emulation_pbb_config \ -mode create \ -port_handle $port_h \ -bridge_id $bridge_id \ -bridge_id_step 00:00:00:02:00:00 \ -count $bridge_count \ -enable_optional_tlv_validation 0 \ -enable_out_of_sequence_detection 1 \ -ether_type 8902 \ -mac_address_init $mac_address_init \ -mac_address_step 00:00:00:00:02:00 \ -receive_ccm 1 \ -send_ccm 1 \ -vlan_id 100 \ -vlan_id_step 2 \ -vlan_user_priority 3 \ ] if {[keylget pbb_config_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget pbb_config_status log]" return 0 } set pbb_handles_$port [keylget pbb_config_status handle] puts "Ixia pbb_bridge handles for port $port are: " update idletasks foreach pbb_handle [set pbb_handles_$port] { puts $pbb_handle update idletasks } incr port } ################################################################################ # PBB trunk configuration ################################################################################ puts "\n### Start PBB trunk configuration ..." update idletasks set port 1 set dst_mac_address_list {} set src_mac_address_list {} for {set i 1} {$i <= $bridge_count} {incr i} { lappend dst_mac_address_list aa:bb:00:00:1$i:01 lappend src_mac_address_list cc:dd:00:00:1$i:01 } array set rev_port_mac_address_list [list \ $port_0,dst dst_mac_address_list \ $port_0,src src_mac_address_list \ $port_1,src dst_mac_address_list \ $port_1,dst src_mac_address_list \ ] foreach port_h $port_handle { set bridge_handles [set pbb_handles_$port] set bridge 1 set dst_mac_address_list_temp [set $rev_port_mac_address_list($port_h,dst)] set src_mac_address_list_temp [set $rev_port_mac_address_list($port_h,src)] foreach bridge_handle $bridge_handles { set pbb_trunk_config_status [::ixia::emulation_pbb_trunk_config \ -bridge_handle $bridge_handle \ -mode create \ -count $trunk_count \ -dst_mac_address [lindex $dst_mac_address_list_temp [expr $bridge - 1]] \ -src_mac_address [lindex $src_mac_address_list_temp [expr $bridge - 1]] \ -add_ccm_custom_tlvs 1 \ -add_data_tlv 1 \ -add_interface_status_tlv 1 \ -add_lbm_custom_tlvs 1 \ -add_lbr_custom_tlvs 1 \ -add_ltm_custom_tlvs 1 \ -add_ltr_custom_tlvs 1 \ -add_organization_specific_tlv 1 \ -add_port_status_tlv 1 \ -add_sender_id_tlv 1 \ -auto_dm_iteration 100 \ -auto_dm_timeout 5 \ -auto_dm_timer 30 \ -auto_lb_iteration 200 \ -auto_lb_timeout 5 \ -auto_lb_timer 40 \ -auto_lt_iteration 300 \ -auto_lt_timeout 6 \ -auto_lt_timer 50 \ -b_vlan_id 100 \ -b_vlan_priority 3 \ -b_vlan_tp_id 9100 \ -cci_interval 10msec \ -ccm_priority 1 \ -chassis_id 00:00:00:00:00:11 \ -chassis_id_length 6 \ -chassis_id_step 00:00:00:00:00:a1 \ -chassis_id_sub_type chassis_component \ -data_tlv_length 4 \ -data_tlv_step 00:00:00:03 \ -data_tlv_value 11:22:33:44 \ -dmm_priority 4 \ -enable_auto_dm 1 \ -enable_auto_lb 1 \ -enable_auto_lt 1 \ -enable_reverse_bvlan 1 \ -lbm_priority 2 \ -ltm_priority 7 \ -management_address a1:a2:a3:a3:a4:a5 \ -management_address_domain 4d:61:6e:61:67:65:6d:65:6e:74:20:41:64:64:72:20:44:6f:6d:61:69:6e \ -management_address_domain_length 22 \ -management_address_domain_step 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:01 \ -management_address_length 6 \ -md_level_id 3 \ -md_name IxiaUser \ -md_name_format string \ -mep_id ${port}${bridge}0 \ -mr_count $mr_count \ -mr_inner_count $mr_count \ -mr_enable_vlan 1 \ -mr_i_tagi_sid 10 \ -mr_start_mac_address 00:00:00:aa:00:01 \ -mr_mac_inter_range_step 00:00:00:00:01:50 \ -mr_mac_inter_trunk_step 00:00:00:a1:00:00 \ -mr_mac_step 00:00:00:00:00:02 \ -mr_s_vlan_id 20 \ -mr_s_vlan_priority 5 \ -mr_s_vlan_tp_id 8100 \ -mr_stacked_vlan_id_step 12 \ -mr_stacked_vlan_inter_trunk_step 15 \ -mr_type single \ -mr_vlan_id_step 2 \ -mr_vlan_inter_trunk_step 100 \ -organization_specific_tlv_length 5 \ -organization_specific_tlv_value 00:00:00:ff:ee \ -override_vlan_priority 1 \ -reverse_bvlan_id 1000 \ -short_ma_name "ixia-user" \ -short_ma_name_format char_string \ -ttl 64 \ ] if {[keylget pbb_trunk_config_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget pbb_trunk_config_status log]" return 0 } set PB $port/$bridge set pbb_trunk_handles_$PB [keylget pbb_trunk_config_status trunk_handle] puts "Ixia pbb trunk handles for port/bridge $PB are: " update idletasks foreach pbb_trunk_handle [set pbb_trunk_handles_$PB] { puts $pbb_trunk_handle update idletasks } incr bridge } incr port } ################################################################################ # PBB custom TLV configuration ################################################################################ puts "\n### Start PBB custom TLV configuration ..." update idletasks set port 1 foreach port_h $port_handle { set bridge_handles [set pbb_handles_$port] set bridge 1 foreach bridge_handle $bridge_handles { set pbb_custom_tlv_config_status [::ixia::emulation_pbb_custom_tlv_config \ -bridge_handle $bridge_handle \ -mode create \ -count 3 \ -include_in_ccm 1 \ -include_in_lbm 1 \ -include_in_lbr 1 \ -include_in_ltm 1 \ -include_in_ltr 1 \ -length 3 \ -reset 1 \ -type 70 \ -value 11:22:aa \ -value_step 0a:11:00 \ ] if {[keylget pbb_custom_tlv_config_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget pbb_custom_tlv_config_status log]" return 0 } set PB $port/$bridge set pbb_custom_tlv_handles_$PB [keylget pbb_custom_tlv_config_status handle] puts "Ixia pbb custom tlv handles for port/bridge $PB are: " update idletasks foreach pbb_custom_tlv_handle [set pbb_custom_tlv_handles_$PB] { puts $pbb_custom_tlv_handle update idletasks } incr bridge } incr port } ################################################################################ # Start protocol ################################################################################ puts "\n### Starting PBB-TE protocol" update idletasks set protocol_status [::ixia::emulation_pbb_control \ -mode start \ -port_handle $port_handle \ ] if {[keylget protocol_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget protocol_status log]" return 0 } puts "\nSUCCESS protocol started!" update idletasks after 30000 ################################################################################ # Collect statistics ################################################################################ puts "\n###Collecting statistics ..." update idletasks ######################### #SHOW STATS PROCEDURE # ######################### proc show_stats var { set level [expr [info level] - 1] foreach key [keylkeys var] { if {$key == "status"} {continue} set indent [string repeat " " $level] puts -nonewline $indent if {[catch {keylkeys var $key}]} { puts "$key: [keylget var $key]" continue } else { puts $key puts "$indent[string repeat "-" [string length $key]]" } show_stats [keylget var $key] } } set port 1 foreach port_h $port_handle { set bridge_handles [set pbb_handles_$port] set bridge 1 puts "\n### periodic_oam_dm stats for bridges on port $port_h" foreach handle $bridge_handles { set pbb_info_status_1 [::ixia::emulation_pbb_info \ -mode set_filters \ -handle $handle \ -user_bvlan all_vlan_id \ -user_delay_type dvm \ -user_dst_type mep_mac_all \ -user_mdlevel all_md \ -user_src_type mep_mac_all \ -user_transaction_id 1 \ -user_ttl_interval 64 \ -user_usability_option manual \ ] if {[keylget pbb_info_status_1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pbb_info_status_1 log]" return 0 } set pbb_info_status_1 [::ixia::emulation_pbb_info \ -mode get_all_learned_info \ -handle $handle \ ] if {[keylget pbb_info_status_1 status] != $::SUCCESS} { return "FAIL - $test_name - [keylget pbb_info_status_1 log]" return 0 } puts "#Statistics for bridge $handle:" show_stats $pbb_info_status_1 } } ################################################################################ # Stop protocol ################################################################################ set protocol_status [::ixia::emulation_pbb_control \ -mode stop \ -port_handle $port_handle \ ] if {[keylget protocol_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget protocol_status log]" return 0 } puts "\nSUCCESS protocol stopped!" puts "\nEnd test ..." puts "\nSUCCESS - $test_name - [clock format [clock seconds]]" return 1