################################################################################# # Version 1 $Revision: 3 $ # $Author: MChakravarthy $ # # Copyright © 1997 - 2013 by IXIA # All Rights Reserved. # # Revision Log: # 05-23-2013 Mchakravarthy - created sample # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample loads ixnetwork config file with ELMI protocol configured on # # ports and retreives all the handles using session resume # # Module: # # The sample was tested on a LM1000TXS4 module. # # # ################################################################################ if {[catch {package require Ixia} retCode]} { puts "FAIL - [info script] - $retCode" return 0 } ################################################################################ # General script variables ################################################################################ set test_name [info script] set test_name_folder [file dirname $test_name] set ixn_cfg [file join $test_name_folder ELMI_b2b.ixncfg] ################################################################################ # START - Connect to the chassis ################################################################################ puts "Starting - $test_name - [clock format [clock seconds]]" puts "Start connecting to chassis ..." set tcl_server 127.0.0.1 set ixnetwork_tcl_server 127.0.0.1 set chassis_ip 10.206.27.55 set port_list [list 8/1 8/2] set connect_status [ixia::connect \ -mode connect \ -config_file $ixn_cfg \ -ixnetwork_tcl_server $ixnetwork_tcl_server \ -tcl_server $tcl_server ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return 0 } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassis_ip.$port} \ temp_port]} { lappend port_handle $temp_port } } set i 0 puts "Ixia port handles are:" foreach port $port_handle { set port_$i $port puts $port incr i } puts "Connect to the chassis complete." ################################################################################ # END - Connect to the chassis ################################################################################ ################################################################################ # Retreive elmi config handles using session info ################################################################################ set rval_1 [ixia::session_info \ -mode get_session_keys \ -session_keys_include_filter {emulation_elmi_config} \ -port_handle $port_0 ] if {[keylget rval_1 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget rval_1 log]" return 0 } set uni_handles_0 [keylget rval_1 $port_0.emulation_elmi_config.uni_handles] puts "Port: $port_0 - UNI Handle - $uni_handles_0" set rval_2 [ixia::session_info \ -mode get_session_keys \ -session_keys_include_filter {emulation_elmi_config} \ -port_handle $port_1 ] if {[keylget rval_2 status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget rval_2 log]" return 0 } set uni_handles_1 [keylget rval_2 $port_1.emulation_elmi_config.uni_handles] set evc_handles_1 [lsort [keylget rval_2 $port_1.emulation_elmi_config.evc_handles]] set uni_status_handles_1 [keylget rval_2 $port_1.emulation_elmi_config.uni_status_handles] set bw_profile_handles_1 [lsort [keylget rval_2 $port_1.emulation_elmi_config.bw_profile_handles]] set ce_vlan_id_range_handles_1 [lsort [keylget rval_2 $port_1.emulation_elmi_config.ce_vlan_id_range_handles]] puts "Port: $port_1 - UNI Handle - $uni_handles_1" puts "Port: $port_1 - EVC Handles - $evc_handles_1" puts "Port: $port_1 - UNI Status Handles - $uni_status_handles_1" puts "Port: $port_1 - BW Profile Handles - $bw_profile_handles_1" puts "Port: $port_1 - CE Vlan Id Range Handles - $ce_vlan_id_range_handles_1" ############################### SUCCESS or FAILURE ############################# puts "SUCCESS - $test_name - [clock format [clock seconds]]" return 1