################################################################################ # Version 1.0 $Revision: 1 $ # $Author: T. Kong $ # # $Workfile: ISIS_topology_create_grid.tcl $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 2-17-2005 create. # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates an ISIS router and configures a grid network behind # # the ISIS session router. Then modifies the topology. # # # # Module: # # The sample was tested on a LM100TXS8 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP 127.0.0.1 set port_list [list 10/1] ################################################################################ # START TEST # ################################################################################ # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [ ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [keylget connect_status port_handle.$chassisIP.$port_list] ##################################################### # Configure 10 ISIS L1L2 neighbors interface # ##################################################### set isis_router_status [::ixia::emulation_isis_config \ -mode create \ -reset \ -port_handle $port_handle \ -intf_ip_addr 22.1.1.1 \ -gateway_ip_addr 22.1.1.2 \ -intf_ip_prefix_length 24 \ -intf_type ptop \ -mac_address_init 0000.0000.0001 \ -count 10 \ -wide_metrics 1 \ -discard_lsp 1 \ -attach_bit 0 \ -partition_repair 1 \ -overloaded 0 \ -lsp_refresh_interval 10 \ -lsp_life_time 777 \ -max_packet_size 1492 \ -intf_metric 0 \ -routing_level L1L2 \ -te_enable 1 \ -te_router_id 198.0.0.1 \ -te_max_bw 10 \ -te_max_resv_bw 20 \ -te_unresv_bw_priority0 0 \ -te_unresv_bw_priority1 10 \ -te_unresv_bw_priority2 20 \ -te_unresv_bw_priority3 30 \ -te_unresv_bw_priority4 40 \ -te_unresv_bw_priority5 50 \ -te_unresv_bw_priority6 60 \ -te_unresv_bw_priority7 70 \ -te_metric 10] if {[keylget isis_router_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget isis_router_status log]" } #Get the list of ISIS router handle form the keye list returned set isis_router_handle_list [keylget isis_router_status handle] ############################################################## # Configure a grid network behind the isis session router # ############################################################## set isis_router_handle [lindex $isis_router_handle_list 0] puts "isis_router_handle = $isis_router_handle" #foreach isis_router_handle [lindex $isis_router_handle_list 0] /{ set route_config_status [::ixia::emulation_isis_topology_route_config \ -mode create \ -handle $isis_router_handle \ -type grid \ -ip_version 4_6 \ -grid_start_system_id AABBCCDDEEFF \ -grid_system_id_step 00000000000A \ -router_id 44.0.0.1 \ -router_area_id 000001 000002 112233 \ -grid_row 5 \ -grid_col 5 \ -grid_stub_per_router 10 \ -grid_router_id 77.0.0.1 \ -grid_router_id_step 0.0.1.0 \ -grid_ip_start 33.0.0.1 \ -grid_ip_pfx_len 24 \ -grid_ip_step 0.0.1.0 \ -grid_ipv6_start 5001:0:0:1::0 \ -grid_ipv6_pfx_len 84 \ -grid_ipv6_step 0:0:0:1::0 \ -grid_connect 2 2 \ -grid_interface_metric 23 \ -grid_link_type ptop \ -grid_router_metric 10 \ -grid_router_up_down_bit 1 \ -grid_router_origin external \ -grid_te 1 \ -grid_start_te_ip 55.0.0.1 \ -grid_te_ip_step 0.0.1.0 \ -grid_te_metric 20 \ -grid_te_admin 1234 \ -grid_te_max_bw 9999 \ -grid_te_max_resv_bw 10000 \ -grid_te_unresv_bw_priority0 0 \ -grid_te_unresv_bw_priority1 1 \ -grid_te_unresv_bw_priority2 2 \ -grid_te_unresv_bw_priority3 3 \ -grid_te_unresv_bw_priority4 4 \ -grid_te_unresv_bw_priority5 5 \ -grid_te_unresv_bw_priority6 6 \ -grid_te_unresv_bw_priority7 7 \ ] if {[keylget route_config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget route_config_status log]" } set elem_handle [keylget route_config_status elem_handle] #/} ########################### # Modify Topology # ########################### set route_config_status [::ixia::emulation_isis_topology_route_config \ -mode modify \ -handle $isis_router_handle \ -elem_handle $elem_handle \ -type grid \ -ip_version 4_6 \ -grid_start_system_id 112233445566 \ -grid_system_id_step 000000000005 \ -router_id 44.0.0.7 \ -router_area_id AA0001 BB0002 CC2233 \ -grid_row 15 \ -grid_col 15 \ -grid_stub_per_router 15 \ -grid_router_id 55.0.0.1 \ -grid_router_id_step 0.0.1.0 \ -grid_ip_start 66.0.0.1 \ -grid_ip_pfx_len 24 \ -grid_ip_step 0.0.1.0 \ -grid_connect 5 5 \ -grid_interface_metric 30 \ -grid_link_type broadcast \ -grid_router_metric 10 \ -grid_router_up_down_bit 1 \ -grid_router_origin stub \ -grid_te 1 \ -grid_start_te_ip 33.0.0.1 \ -grid_te_ip_step 0.0.1.0 \ ] if {[keylget route_config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget route_config_status log]" } ###################### # START ISIS # ###################### set isis_emulation_status [::ixia::emulation_isis_control \ -port_handle $port_handle \ -mode start ] if {[keylget isis_emulation_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget isis_emulation_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"