################################################################################ # Version 1.0 $Revision: 1 $ # $Author: LRaicea $ # # Copyright © 1997 - 2008 by IXIA # All Rights Reserved. # # Revision Log: # 03-20-2008 LRaicea - created sample # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample creates a LDP router and an LDP VC Range. # # # # Module: # # The sample was tested on a LM1000STXS4 module. # # The sample was tested using HLTSET29. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP sylvester set port_list [list 2/1] ################################################################################ # Connect to the chassis, reset to factory defaults ################################################################################ # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser \ -break_locks 1 \ ] if {[keylget connect_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget connect_status log]" return } set port_handle [list] foreach port $port_list { if {![catch {keylget connect_status port_handle.$chassisIP.$port} \ temp_port]} { lappend port_handle $temp_port } } set port_0 [lindex $port_handle 0] ################################################################################ # Set L1 configuration ################################################################################ set interface_status [::ixia::interface_config \ -port_handle $port_0 \ -autonegotiation 1 \ -duplex auto \ -speed auto \ ] if {[keylget interface_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget interface_status log]" return } ################################################################################ # LDP router configuration ################################################################################ set ldp_routers_status [::ixia::emulation_ldp_config \ -mode create \ -port_handle $port_0 \ -count 1 \ -intf_ip_addr 30.30.30.2 \ -intf_prefix_length 24 \ -gateway_ip_addr 30.30.30.1 \ -loopback_ip_addr 3.3.3.2 \ -lsr_id 3.3.3.2 \ -remote_ip_addr 3.3.3.1 \ -label_space 0 \ -peer_discovery targeted_martini \ -hello_interval 5 \ -hello_hold_time 15 \ -keepalive_interval 10 \ -keepalive_holdtime 30 \ -discard_self_adv_fecs 0 \ -enable_l2vpn_vc_fecs 1 \ -enable_explicit_include_ip_fec 0 \ -enable_remote_connect 1 \ -enable_vc_group_matching 0 \ -targeted_hello_hold_time 45 \ -targeted_hello_interval 15 \ ] if {[keylget ldp_routers_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget ldp_routers_status log]" return } set ldp_router [keylget ldp_routers_status handle] ################################################################################ # LDP VC Range configuration ################################################################################ set ldp_route_status [::ixia::emulation_ldp_route_config \ -mode create \ -handle $ldp_router \ -fec_type vc \ -fec_vc_type eth_vpls \ -fec_vc_count 3 \ -fec_vc_group_id 1 \ -fec_vc_group_count 1 \ -fec_vc_cbit 0 \ -fec_vc_id_start 332 \ -fec_vc_id_step 1 \ -fec_vc_id_count 1 \ -fec_vc_intf_mtu_enable 1 \ -fec_vc_intf_mtu 1500 \ -fec_vc_intf_desc "ixia_ldp_vc" \ -packing_enable 0 \ -fec_vc_label_mode increment_label \ -fec_vc_label_value_start 332 \ -fec_vc_label_value_step 1 \ -fec_vc_peer_address 3.3.3.1 \ -fec_vc_ce_ip_addr 3.3.3.2 \ -fec_vc_ip_range_enable 1 \ -fec_vc_ip_range_addr_count 5 \ -fec_vc_ip_range_addr_start 11.11.11.2 \ -fec_vc_ip_range_addr_inner_step 0.0.0.1 \ -fec_vc_ip_range_addr_outer_step 0.0.1.0 \ -fec_vc_ip_range_prefix_len 24 \ ] if {[keylget ldp_route_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget ldp_route_status log]" return } set lsp_vc_range_handles [keylget ldp_route_status lsp_vc_range_handles] set lsp_vc_ip_range_handles [keylget ldp_route_status lsp_vc_ip_range_handles] ################################################################################ # LDP VC Range modify ################################################################################ set ldp_route_status [::ixia::emulation_ldp_route_config \ -mode modify \ -handle $ldp_router \ -lsp_handle [lindex $lsp_vc_ip_range_handles 0] \ -fec_vc_ip_range_addr_start 22.22.22.2 \ ] if {[keylget ldp_route_status status] != $::SUCCESS} { puts "FAIL - $test_name - [keylget ldp_route_status log]" return } puts "SUCCESS - $test_name - [clock format [clock seconds]]" return