################################################################################ # Version 1.0 $Revision: 2 $ # $Author: Lavinia Raicea $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 26/5-2005 Lavinia Raicea # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ############################################################################### ################################################################################ # # # Description: # # This sample performes various operations. It creates RIPv1, RIPv2 and # # RIPng routers on three different ports. It adds route ranges to the # # routers. It modifies routers and route ranges, deletes routers and # # route ranges. It deisables, enables, starts and stops routers. It # # advertises and withdraws route ranges. # # # Module: # # The sample was tested on a LM100TXS8 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP 127.0.0.1 set port_list1 10/1 set port_list2 10/2 set port_list3 10/3 # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list1 \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle1 [keylget connect_status port_handle.$chassisIP.$port_list1] ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle1 \ -autonegotiation 1 \ -duplex full \ -speed ether100 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } #################################################### # Configure interfaces and create RIP v1 sessions # #################################################### set rip_status [::ixia::emulation_rip_config \ -port_handle $port_handle1 \ -mode create \ -session_type ripv1 \ -reset \ -count 5 \ -intf_ip_addr 11.0.0.100 \ -intf_prefix_length 24 \ -update_interval 50 \ -update_interval_offset 5 \ -update_mode no_horizon \ -mac_address_init 0000.0000.0001] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } set ripv1_routers [keylget rip_status handle] set ripv1_route_ranges [list ] set i 15 # Creates 2 route ranges for each router => a total of 6 route ranges foreach ripv1_router $ripv1_routers { # Create first route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripv1_router \ -mode create \ -reset \ -num_prefixes 5 \ -prefix_start $i.0.0.0 \ -prefix_length 8 \ -metric 2 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripv1_route_ranges [keylget rip_status route_handle] # Create second route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripv1_router \ -mode create \ -num_prefixes 5 \ -prefix_start 1$i.1$i.0.0 \ -prefix_length 16 \ -metric 2 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripv1_route_ranges [keylget rip_status route_handle] incr i 10 } # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list2 \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle2 [keylget connect_status port_handle.$chassisIP.$port_list2] ######################################## # Configure interface in the test # # IPv4 # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle2 \ -autonegotiation 1 \ -duplex full \ -speed ether100 ] ################################################### # Configure interfaces and create RIPv2 sessions # ################################################### set rip_status [::ixia::emulation_rip_config \ -port_handle $port_handle2 \ -mode create \ -reset \ -intf_ip_addr 12.0.0.100 \ -intf_prefix_length 24 \ -update_interval 50 \ -update_interval_offset 5 \ -update_mode no_horizon \ -authentication_mode text \ -password abcde \ -send_type broadcast_v2 \ -receive_type v1_v2 \ -count 5 \ -mac_address_init 0000.0000.0004 ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } set ripv2_routers [keylget rip_status handle] set ripv2_route_ranges [list ] set i 20 foreach ripv2_router $ripv2_routers { # Create first route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripv2_router \ -mode create \ -reset \ -num_prefixes 5 \ -prefix_start $i.0.0.0 \ -prefix_length 8 \ -metric 2 \ -next_hop 12.0.0.$i \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripv2_route_ranges [keylget rip_status route_handle] # Create second route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripv2_router \ -mode create \ -num_prefixes 5 \ -prefix_start \ [mpexpr 10 + $i].[mpexpr 10 + $i].0.0 \ -prefix_length 16 \ -metric 2 \ -route_tag 100 \ -next_hop 12.0.0.[mpexpr 10 + $i] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripv2_route_ranges [keylget rip_status route_handle] incr i 20 } # Connect to the chassis, reset to factory defaults and take ownership set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list3 \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle3 [keylget connect_status port_handle.$chassisIP.$port_list3] ######################################## # Configure interface in the test # ######################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle3 \ -autonegotiation 1 \ -duplex full \ -speed ether100 ] ################################################### # Configure interfaces and create RIPng sessions # ################################################### set ripng_status [::ixia::emulation_rip_config \ -port_handle $port_handle3 \ -mode create \ -reset \ -session_type ripng \ -intf_ip_addr 30:30:30:30:0:0:0:1 \ -intf_ip_addr_step 0:0:0:1:0:0:0:0 \ -intf_prefix_length 64 \ -update_interval 50 \ -update_interval_offset 5 \ -update_mode no_horizon \ -receive_type store \ -interface_metric 2 \ -time_period 100 \ -num_routes_per_period 10 \ -router_id 20 \ -router_id_step 10 \ -count 5 \ -mac_address_init 0000.0000.0007] if {[keylget ripng_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget ripng_status log]" } set ripng_routers [keylget ripng_status handle] set ripng_route_ranges [list ] set i 5 # Creates three route ranges for each router => a total of 9 routes foreach ripng_router $ripng_routers { # Create first route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripng_router \ -mode create \ -reset \ -num_prefixes 2 \ -prefix_start 1$i:10:0:0:0:0:0:0 \ -prefix_length 32 \ -prefix_step 0:1000:0:0:0:0:0:0 \ -metric 2 \ -next_hop FE80:0:0:0:$i:$i:$i:$i \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripng_route_ranges [keylget rip_status route_handle] # Create second route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripng_router \ -mode create \ -num_prefixes 2 \ -prefix_start 2$i:2$i:20:0:0:0:0:0 \ -prefix_length 48 \ -metric 2 \ -route_tag 100 \ -next_hop FE81:0:0:0:$i:$i:$i:$i \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripng_route_ranges [keylget rip_status route_handle] # Create third route range set rip_status [::ixia::emulation_rip_route_config \ -handle $ripng_router \ -mode create \ -num_prefixes 2 \ -prefix_start 4$i:4$i:4$i:40:0:0:0:0 \ -prefix_length 64 \ -metric 2 \ -route_tag 100 \ -next_hop FE82:0:0:0:$i:$i:$i:$i \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } lappend ripng_route_ranges [keylget rip_status route_handle] incr i } set rip_all_routers [concat \ $ripv1_routers \ $ripv2_routers \ $ripng_routers ] set rip_all_routes [concat \ $ripv1_route_ranges \ $ripv2_route_ranges \ $ripng_route_ranges ] # Modify all sessions set rip_status [::ixia::emulation_rip_config \ -mode modify \ -handle $rip_all_routers \ -update_interval 29 \ -update_interval_offset 2 \ -update_mode poison_reverse \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Modify all routes set rip_status [::ixia::emulation_rip_route_config \ -mode modify \ -route_handle $rip_all_routes \ -metric 1 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Delete sessions set rip_status [::ixia::emulation_rip_config \ -mode delete \ -handle [list \ [lindex $ripv1_routers 2] \ [lindex $ripv2_routers 2] \ [lindex $ripng_routers 2]] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Remove deleted routers from the lists set ripv1_routers [lreplace $ripv1_routers 2 2] set ripv2_routers [lreplace $ripv2_routers 2 2] set ripng_routers [lreplace $ripng_routers 2 2] # Remove corresponding route from the lists set ripv1_route_ranges [lreplace $ripv1_route_ranges 4 5] set ripv2_route_ranges [lreplace $ripv2_route_ranges 4 5] set ripng_route_ranges [lreplace $ripng_route_ranges 6 8] # Disable sessions set rip_status [::ixia::emulation_rip_config \ -mode disable \ -handle [concat \ [lrange $ripv1_routers 1 2] \ [lrange $ripv2_routers 1 2] \ [lrange $ripng_routers 1 2]] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Start protocols on ports set rip_status [::ixia::emulation_rip_control \ -mode start \ -port_handle [list $port_handle1 \ $port_handle2 \ $port_handle3] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Stop protocols on ports set rip_status [::ixia::emulation_rip_control \ -mode stop \ -port_handle [list $port_handle1 \ $port_handle2 \ $port_handle3] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Enable sessions and start protocols set rip_status [::ixia::emulation_rip_control \ -mode start \ -handle [concat \ [lrange $ripv1_routers 1 2] \ [lrange $ripv2_routers 1 2] \ [lrange $ripng_routers 1 2]] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Stop protocols on ports set rip_status [::ixia::emulation_rip_control \ -mode stop \ -port_handle [list $port_handle1 \ $port_handle2 \ $port_handle3] \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Modify router - this modification will not affect the router # because authentication is only valid for RIPv2 set rip_status [::ixia::emulation_rip_config \ -mode modify \ -handle [lindex $ripv1_routers 2] \ -authentication_mode text \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Delete route ranges set rip_status [::ixia::emulation_rip_route_config \ -route_handle [list \ [lindex $ripv1_route_ranges 5] \ [lindex $ripv1_route_ranges 7] \ [lindex $ripv2_route_ranges 5] \ [lindex $ripv2_route_ranges 7] \ [lindex $ripng_route_ranges 8] \ [lindex $ripng_route_ranges 11]] \ -mode delete \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Remove corresponding routes from the lists set ripv1_route_ranges [lreplace $ripv1_route_ranges 5 5] set ripv1_route_ranges [lreplace $ripv1_route_ranges 6 6] set ripv2_route_ranges [lreplace $ripv2_route_ranges 5 5] set ripv2_route_ranges [lreplace $ripv2_route_ranges 6 6] set ripng_route_ranges [lreplace $ripng_route_ranges 8 8] set ripng_route_ranges [lreplace $ripng_route_ranges 10 10] # Create another route range set rip_status [::ixia::emulation_rip_route_config \ -handle [lindex $ripng_routers end] \ -mode create \ -num_prefixes 5 \ -prefix_start 50:50:59:50:0:0:0:0 \ -prefix_length 64 \ -metric 2 \ -route_tag 100 \ -next_hop FE83:0:0:0:1:1:1:1 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } set ripng_route_ranges [concat $ripng_route_ranges \ [keylget rip_status route_handle]] # Withdraw route ranges set rip_status [::ixia::emulation_rip_control -withdraw \ [lrange $ripng_route_ranges 1 5]] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Start protocols on port set rip_status [::ixia::emulation_rip_control \ -mode start \ -port_handle $port_handle3 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Advertise route ranges set rip_status [::ixia::emulation_rip_control -advertise \ [lrange $ripng_route_ranges 1 5]] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } # Stop protocols on port set rip_status [::ixia::emulation_rip_control \ -mode stop \ -port_handle $port_handle3 \ ] if {[keylget rip_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rip_status log]" } return "SUCCESS - $test_name - [clock format [clock seconds]]"