################################################################################ # Version 1.0 $Revision: 1 $ # $Author: Hasmik $ # # Copyright © 1997 - 2005 by IXIA # All Rights Reserved. # # Revision Log: # 07-19-2004 Hasmik # 04-1-2005 T.Kong - updated for HLTAPI V4.0 spec # # Description: # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample creates a RSVP neigbor and configures it as Ingress LSR. # # # # Module: # # The sample was tested on a LM100TXS8 module. # # # ################################################################################ package require Ixia set test_name [info script] set chassisIP 127.0.0.1 set port_list [list 10/1] # Connect to the chassis, reset to factory defaults and take ownership # When using P2NO HLTSET, for loading the IxTclNetwork package please # provide –ixnetwork_tcl_server parameter to ::ixia::connect set connect_status [::ixia::connect \ -reset \ -device $chassisIP \ -port_list $port_list \ -username ixiaApiUser ] if {[keylget connect_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget connect_status log]" } set port_handle [keylget connect_status port_handle.$chassisIP.$port_list] ############################################################################## # Configure interface in the test # IPv4 ############################################################################## set interface_status [::ixia::interface_config \ -port_handle $port_handle \ -autonegotiation 1 \ -duplex full \ -speed ether100 ] if {[keylget interface_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget interface_status log]" } ############################################################################## # Configure a RSVP neighbor ############################################################################## set rsvp_config_status [::ixia::emulation_rsvp_config \ -mode create \ -reset \ -port_handle $port_handle \ -count 2 \ -refresh_reduction 1 \ -reliable_delivery 1 \ -bundle_msgs 0 \ -hello_msgs 1 \ -hello_interval 200 \ -hello_retry_count 4 \ -refresh_interval 20 \ -srefresh_interval 1000 \ -egress_label_mode imnull \ -path_state_refresh_timeout 77 \ -path_state_timeout_count 5 \ -record_route 1 \ -resv_confirm 1 \ -resv_state_timeout_count 5 \ -resv_state_refresh_timeout 5 \ -min_label_value 20 \ -max_label_value 30 \ -vlan 1 \ -vlan_id 300 \ -vlan_id_mode fixed \ -vlan_id_step 2 \ -mac_address_init 0000.0000.0001 \ -intf_prefix_length 24 \ -ip_version 4 \ -intf_ip_addr 3.3.3.100 \ -intf_ip_addr_step 0.0.1.0 \ -neighbor_intf_ip_addr 3.3.3.1 \ -neighbor_intf_ip_addr_step 0.0.1.0 \ -writeFlag nowrite ] if {[keylget rsvp_config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rsvp_config_status log]" } set handle [lindex [keylget rsvp_config_status handles] 0] ################################################################################ # Configure a RSVP Destination Range along with Sender Range # handle - retured from the previous call # rsvp_behavior - rsvpIngress ################################################################################ set handleList [list] set egress_ip_addr 2.2.2.100 set sender_ip_addr 4.4.4.100 set rro_ipv4_list {101.0.0.1 202.0.0.1} set rro_label_list {11 22} set rro_ctype_list {33 44} set rro_flags_list {9 12} set ero_ipv4_list {33.0.0.1 44.0.0.1} set ero_as_num_list {33 44} set ero_flags_list {9 11} set ero_pfxlen_list {1 1} set ero_loose_list {1 0} # Add numDests Destination Ranges set rsvp_tunnel_config_status [::ixia::emulation_rsvp_tunnel_config \ -mode create \ -handle $handle \ -rsvp_behavior rsvpIngress \ -count 3 \ -egress_ip_addr $egress_ip_addr \ -egress_ip_step 0.1.0.0 \ -ingress_ip_addr $sender_ip_addr \ -ingress_ip_step 0.1.0.0 \ -ingress_bandwidth 1000 \ -sender_tspec_token_bkt_rate 10 \ -sender_tspec_token_bkt_size 10 \ -sender_tspec_peak_data_rate 10 \ -sender_tspec_min_policed_size 5 \ -sender_tspec_max_pkt_size 580 \ -session_attr_bw_protect 1 \ -session_attr_se_style 1 \ -session_attr_local_protect 1 \ -session_attr_label_record 0 \ -session_attr_setup_priority 2 \ -session_attr_hold_priority 2 \ -session_attr_resource_affinities 1 \ -session_attr_ra_include_all 0x11223344 \ -lsp_id_start 100 \ -tunnel_id_start 5 \ -tunnel_id_count 2 \ -tunnel_id_step 10 \ -ero_mode loose \ -ero_dut_pfxlen 16 \ -rro 1 \ -rro_list_type label \ -rro_list_ipv4 $rro_ipv4_list \ -rro_list_label $rro_label_list \ -rro_list_flags $rro_flags_list \ -rro_list_ctype $rro_ctype_list \ -ero 1 \ -ero_list_type ipv4 \ -ero_list_loose $ero_loose_list \ -ero_list_ipv4 $ero_ipv4_list \ -ero_list_pfxlen $ero_pfxlen_list\ -ero_list_as_num $ero_as_num_list\ -fast_reroute 1 \ -fast_reroute_bandwidth 1000 \ -fast_reroute_exclude_any aabbccdd \ -fast_reroute_holding_priority 1 \ -fast_reroute_hop_limit 5 \ -fast_reroute_setup_priority 7 \ -one_to_one_backup 1 \ -send_detour 1 \ -plr_id 11.0.0.1 \ -avoid_node_id 22.0.0.1 \ -session_attr_name MyAttr \ -writeFlag write ] if {[keylget rsvp_tunnel_config_status status] != $::SUCCESS} { return "FAIL - $test_name - [keylget rsvp_tunnel_config_status log]" } lappend handleList [keylget rsvp_tunnel_config_status tunnel_handle] return "SUCCESS - $test_name - [clock format [clock seconds]]"