# # Setup script for Perl sample tests. # # This file is imported by all IxLoad sample Perl test scripts, # and provides a convenient central place to change the # chassis, port, and card that the tests will run on. # # Users should also avoid names beginning with Ix or ix. # package setup_simple; use warnings; use strict; use base qw(Exporter); our @EXPORT = qw(remoteServer chassisName clientPort1 serverPort1); # set remoteServer to IP address of IxLoad client machine running # the remoteScriptingService script or daemon. The value is ignored # when running a script locally on a use constant remoteServer => '1.2.3.4'; # set chassis and ports # both clientPort and serverPort are assumed to be on a single chassis use constant chassisName => '400-amit'; use constant clientPort1 => '1.7.1'; use constant serverPort1 => '1.7.2'; 1