# # setup path and load IxLoad package # source ../setup_simple.tcl # # Initialize IxLoad # #----------------------------------------------------------------------- # Connect #----------------------------------------------------------------------- # IxLoad onnect should always be called, even for local scripts ::IxLoad connect $::IxLoadPrivate::SimpleSettings::remoteServer # once we've connected, make sure we disconnect, even if there's a problem if [catch { # Loads plugins for specific protocols configured in this test # global ixAppPluginManager $ixAppPluginManager load "nessus" # setup logger set logtag "IxLoad-api" set logName "simplevulnerabilityattacksclient" set logger [::IxLoad new ixLogger $logtag 1] set logEngine [$logger getEngine] $logEngine setLevels $::ixLogger(kLevelDebug) $::ixLogger(kLevelInfo) $logEngine setFile $logName 2 256 1 #----------------------------------------------------------------------- # Build Chassis Chain #----------------------------------------------------------------------- set chassisChain [::IxLoad new ixChassisChain] $chassisChain addChassis $::IxLoadPrivate::SimpleSettings::chassisName #----------------------------------------------------------------------- # Build client and server Network #----------------------------------------------------------------------- set clnt_network [::IxLoad new ixNetworkGroup $chassisChain] $clnt_network config \ -name "clnt_network" $clnt_network globalPlugins.clear set Filter [::IxLoad new ixNetFilterPlugin] # ixNet objects needs to be added in the list before they are configured! $clnt_network globalPlugins.appendItem -object $Filter $Filter config \ -name "Filter" set GratArp [::IxLoad new ixNetGratArpPlugin] # ixNet objects needs to be added in the list before they are configured! $clnt_network globalPlugins.appendItem -object $GratArp $GratArp config \ -enabled true \ -name "GratArp" set TCP [::IxLoad new ixNetTCPPlugin] # ixNet objects needs to be added in the list before they are configured! $clnt_network globalPlugins.appendItem -object $TCP $TCP config \ -tcp_tw_recycle true \ -tcp_keepalive_time 75 \ -tcp_keepalive_intvl 7200 \ -tcp_wmem_default 4096 \ -tcp_port_min 1024 \ -tcp_port_max 65535 \ -tcp_window_scaling false \ -name "TCP" \ -tcp_rmem_default 4096 set DNS [::IxLoad new ixNetDnsPlugin] # ixNet objects needs to be added in the list before they are configured! $clnt_network globalPlugins.appendItem -object $DNS $DNS config \ -name "DNS" $DNS hostList.clear $DNS searchList.clear $DNS nameServerList.clear set Settings [::IxLoad new ixNetIxLoadSettingsPlugin] # ixNet objects needs to be added in the list before they are configured! $clnt_network globalPlugins.appendItem -object $Settings $Settings config \ -name "Settings" set Ethernet__PHY_1 [$clnt_network getL1Plugin] set my_ixNetEthernetELMPlugin [::IxLoad new ixNetEthernetELMPlugin] $my_ixNetEthernetELMPlugin config $Ethernet__PHY_1 config \ -name "Ethernet /PHY-1" \ -cardElm $my_ixNetEthernetELMPlugin $Ethernet__PHY_1 childrenList.clear set MAC_VLAN_1 [::IxLoad new ixNetL2EthernetPlugin] # ixNet objects needs to be added in the list before they are configured! $Ethernet__PHY_1 childrenList.appendItem -object $MAC_VLAN_1 $MAC_VLAN_1 config \ -name "MAC/VLAN-1" $MAC_VLAN_1 childrenList.clear set IP_1 [::IxLoad new ixNetIpV4V6Plugin] # ixNet objects needs to be added in the list before they are configured! $MAC_VLAN_1 childrenList.appendItem -object $IP_1 $IP_1 config \ -name "IP-1" $IP_1 childrenList.clear $IP_1 extensionList.clear $MAC_VLAN_1 extensionList.clear $Ethernet__PHY_1 extensionList.clear ################################################# # Setting the ranges starting with the plugin on top of the stack ################################################# $IP_1 rangeList.clear set ip_1 [::IxLoad new ixNetIpV4V6Range] # ixNet objects needs to be added in the list before they are configured! $IP_1 rangeList.appendItem -object $ip_1 $ip_1 config \ -count 100 \ -name "ip-1" \ -gatewayAddress "0.0.0.0" \ -autoMacGeneration true \ -prefix 16 \ -mss 100 \ -ipAddress "198.18.0.1" set mac_1 [$ip_1 getLowerRelatedRange "MacRange"] $mac_1 config \ -count 100 \ -mac "00:C6:12:02:01:00" \ -name "mac-1" set vlan_1 [$ip_1 getLowerRelatedRange "VlanIdRange"] $vlan_1 config \ -name "vlan-1" \ -idIncrMode 1 \ -priority 0 \ -innerPriority 0 $clnt_network portList.appendItem \ -chassisId 1 \ -cardId $::IxLoadPrivate::SimpleSettings::clientPort(CARD_ID)\ -portId $::IxLoadPrivate::SimpleSettings::clientPort(PORT_ID) #----------------------------------------------------------------------- # Construct Client Traffic #----------------------------------------------------------------------- set expected "clnt_traffic" set clnt_traffic [::IxLoad new ixClientTraffic -name $expected] $clnt_traffic agentList.appendItem \ -name "my_attacks_client" \ -protocol "nessus" \ -type "Client" # please Look at the following section. $clnt_traffic agentList(0).pm.targets.appendItem \ -id "TargetHost" \ -destinationHost "198.18.0.101" $clnt_traffic agentList(0).pm.attackSelection.selectedAttacksTable.appendItem \ -attackSelected 1 \ -attackID 14259 \ -attackName "Nmap (NASL wrapper)" #----------------------------------------------------------------------- # Create a client mapping and bind into the # network and traffic that they will be employing #----------------------------------------------------------------------- set clnt_t_n_mapping [::IxLoad new ixClientTrafficNetworkMapping \ -network $clnt_network \ -traffic $clnt_traffic \ -objectiveType $::ixObjective(kObjectiveTypeSimulatedUsers) \ -objectiveValue 1 \ -rampUpValue 1 \ -sustainTime 60 \ -rampDownTime 20 ] #----------------------------------------------------------------------- # Create the test and bind in the network-traffic mapping it is going # to employ. #----------------------------------------------------------------------- set test [::IxLoad new ixTest \ -name "my_test" \ -statsRequired 1 \ -enableResetPorts 0 \ -enableForceOwnership 1 \ ] $test clientCommunityList.appendItem -object $clnt_t_n_mapping #----------------------------------------------------------------------- # Create a test controller bound to the previosuly allocated # chassis chain. This will eventually run the test we created earlier. #----------------------------------------------------------------------- set testController [::IxLoad new ixTestController -outputDir 1] $testController setResultDir "[pwd]/RESULTS/simpleVulnerabilityAttacksClient" $testController run $test vwait ::ixTestControllerMonitor puts $::ixTestControllerMonitor #----------------------------------------------------------------------- # Cleanup #----------------------------------------------------------------------- $testController releaseConfigWaitFinish ::IxLoad delete $logger ::IxLoad delete $logEngine ::IxLoad delete $chassisChain ::IxLoad delete $clnt_network ::IxLoad delete $clnt_traffic ::IxLoad delete $clnt_t_n_mapping ::IxLoad delete $test ::IxLoad delete $testController #----------------------------------------------------------------------- # Disconnect #----------------------------------------------------------------------- }] { puts $errorInfo } # # Disconnect/Release application lock # ::IxLoad disconnect