# # Setup script for simple*.tcl tests. # # This file is sourced by all IxLoad sample tcl test scripts, # and provides a convenient central place to change the # chassis, port, and card that the tests will run on. # # # Set up paths to IxLoad tcl code relative to sample directory. # (ignored for non-windows machines) # source ../setup_ixload_paths.tcl # # Define the main IxLoad command # package require IxLoad # IxLoad's reservered namespace # Users should also avoid names beginning with Ix or ix. namespace eval ::IxLoadPrivate {} # A namespace for settings defined in this file # and used by all simple*.tcl example scripts. namespace eval ::IxLoadPrivate::SimpleSettings {} # set remoteServer to IP address of IxLoad client machine running # the remoteScriptingService script or daemon. The value is ignored # when running a script locally on a variable ::IxLoadPrivate::SimpleSettings::remoteServer 192.168.4.137 # both clientPort and serverPort are assumed to be on a single chassis variable ::IxLoadPrivate::SimpleSettings::chassisName 400-amit array set ::IxLoadPrivate::SimpleSettings::clientPort { CARD_ID "3" PORT_ID "1" } array set ::IxLoadPrivate::SimpleSettings::serverPort { CARD_ID "3" PORT_ID "2" } # most tests require 2 ports, but some can use up to 6 # Change numPorts to run tests that require more set ::IxLoadPrivate::SimpleSettings::numPorts 2 array set ::IxLoadPrivate::SimpleSettings::port3 { CARD_ID "2" PORT_ID "7" } array set ::IxLoadPrivate::SimpleSettings::port4 { CARD_ID "2" PORT_ID "8" } array set ::IxLoadPrivate::SimpleSettings::port5 { CARD_ID "2" PORT_ID "2" } array set ::IxLoadPrivate::SimpleSettings::port6 { CARD_ID "2" PORT_ID "3" }