#------------------------------------------------------------------------------ # Name : test.sample_script_twamp.tcl # Author : Indranil Acharya # Purpose : To check TWAMP Statistics (Per Session /Per Range and Global) # Code Flow : 1. Configure IXIA Ports # 2. Start TWAMP # 3. Verify TWAMP Protocol Stats # 4. Verify Per Session/Range Stats # 5. Stop TWAMP # 6. Clean IXIA Ports # Test Setup : B2B # ixncfg used : Yes (config.sample_script_twamp.ixncfg) # Scriptgen used: No #------------------------------------------------------------------------------ source $env(IXNETWORK_SAMPLE_SCRIPT_DIR)/IxNetwork/TestRun/config.tcl proc Action {portData1 portData2} { # Initialize return value set FAILED 1 set PASSED 0 # Source the Utility Files set isError [catch {source $::pwd/twampTrafficUtils.tcl source $::pwd/twampUtils.tcl} errorMsg] if {$isError} { log "Error in sourcing the file $errorMsg" ixNetCleanUp return $FAILED } # Get port info 1 set chassisIp1 [lindex $portData1 0] set card1 [lindex $portData1 1] set port1 [lindex $portData1 2] set client1 [lindex $portData1 3] set tcpPort1 [lindex $portData1 4] # Get port info 2 set chassisIp2 [lindex $portData2 0] set card2 [lindex $portData2 1] set port2 [lindex $portData2 2] set client2 [lindex $portData2 3] set tcpPort2 [lindex $portData2 4] set version "5.40" # Connect to IxNetwork TCL-Server/Client if {$client1 == $client2} { log "Connecting to client $client1" if {[ixNet connect $client1 -port $tcpPort1 -version $version] != \ "::ixNet::OK" } { log "Unable to connect to IxNetwork Tcl Server !!!" ixNetCleanUp return $FAILED } } else { log "Use the same client !!!" ixNetCleanUp return $FAILED } log "Connection to the Client successful !!!" # Clean up all the existing configurations from client log "Cleaning up the client" ixNetCleanUp log "Executing from [pwd]" # Load config file set configFileName "config.sample_script_twamp.ixncfg" if {[ixNet exec loadConfig [ixNet readFrom \ "$::pwd/$configFileName"]] != "::ixNet::OK"} { log "Loading IxNetwork config file : Failed " ixNetCleanUp return $FAILED } # Get the virtual port list log "getting virtual ports ...." set vPorts [ixNet getList [ixNet getRoot] vport] set vPort1 [lindex $vPorts 0] set vPort2 [lindex $vPorts 1] log "Virtual ports are = $vPorts" # Get the real port list set realPortsList [list [list $chassisIp1 $card1 $port1]\ [list $chassisIp2 $card2 $port2] ] # Assign virtual ports to real ports log "Assign virtual ports to real ports ..." set force true set status [ixTclNet::AssignPorts $realPortsList {} $vPorts force] ixNet commit log "Assigned: $status" if {[string equal [lindex $status 0] $vPort1] != 1 || \ [string equal [lindex $status 1] $vPort2] != 1} { ixNetCleanUp return $FAILED } ixTclNet::CheckLinkState $vPorts doneList log "Waiting for 10 sec before starting ..." after 10000 # Start TWAMP on both ports set ethernet1 [lindex [ixNet getList $vPort1/protocolStack ethernet] 0] set ipEndpoint1 [lindex [ixNet getList $ethernet1 ipEndpoint] 0] set ethernet2 [lindex [ixNet getList $vPort2/protocolStack ethernet] 0] set ipEndpoint2 [lindex [ixNet getList $ethernet2 ipEndpoint] 0] log "Starting TWAMP on the ports" if {[ixNet exec start $ipEndpoint2] != "::ixNet::OK"} { log "Unable to start TWAMP at 2nd Port" ixNetCleanUp return $FAILED } log "TWAMP started at 2nd Port successfully" after 5000 if {[ixNet exec start $ipEndpoint1] != "::ixNet::OK"} { log "Unable to start TWAMP at 1st Port" ixNetCleanUp return $FAILED } log "TWAMP started at 1st Port successfully" log "Waiting for 20 Sec..." after 20000 # TWAMP Stats Verification set completeStats {"TWAMP Server Control" {"Sessions Initiated" 7 \ "Sessions Succeeded" 7 \ "Sessions Failed" 0 \ "Active Sessions" 7 \ "Initiated Sessions Rate" 0 \ "Successful Sessions Rate" 0 \ "Failed Sessions Rate" 0 } \ "TWAMP Server Test" {"Initiated Sessions" 7 \ "Successful Sessions" 7 \ "Failed Sessions" 0 \ "Active Sessions" 0 \ "Initiated Sessions Rate" 0 \ "Successful Sessions Rate" 0 \ "Failed Sessions Rate" 0 } \ "TWAMP Server Data" {"Datagram Tx" 70 \ "Datagram Rx" 70 \ "Datagram Unexpected" 0 \ "Data Streams Initiated" 7 \ "Data Streams Successful" 7 \ "Data Streams Failed" 0 } \ "TWAMP Control" {"Sessions Initiated" 7 \ "Sessions Succeeded" 7 \ "Sessions Failed" 0 \ "Active Sessions" 7 \ "Initiated Sessions Rate" 0 \ "Successful Sessions Rate" 0 \ "Failed Sessions Rate" 0 } \ "TWAMP Test" {"Initiated Sessions" 7 \ "Successful Sessions" 7 \ "Failed Sessions" 0 \ "Active Sessions" 0 \ "Initiated Sessions Rate" 0 \ "Successful Sessions Rate" 0 \ "Failed Sessions Rate" 0 } \ "TWAMP Data" {"Datagram Tx" 70 \ "Datagram Rx" 70 \ "Datagram Lost" 0 \ "Datagram Unexpected" 0 \ "Data Streams Initiated" 7 \ "Data Streams Successful" 7 \ "Data Streams Failed" 0 } \ } foreach {captionView completeStat} $completeStats { if {[checkAllTwampStats $captionView $completeStat 1] == 1} { log "Failure: Did not get the expected value for the stats" ixNetCleanUp return $FAILED } log "$captionView: Got the expected value for all the stats" } # Verifying Per Session Stats log "Verifying Per Session Stats ....." set expectedPerSessionStat {"1 1 0 0 10 10 0 1 1 0 0 1000 0" \ "1 1 0 0 10 10 0 1 1 0 1 1000 0" \ "1 1 0 0 10 10 0 1 1 0 2 1000 0" \ "1 1 0 0 10 10 0 1 1 0 3 1000 0" \ "1 1 0 0 10 10 0 1 1 0 4 1000 0"} if {[designL23TrafficPerSession perSession $expectedPerSessionStat] == 1} { log "Fail: The Per session stats are not correct" ixNetCleanUp return $FAILED } log "Pass: The Per session stats are correct" # Verify Per Range Stats log "Verifying Per Range Stats ....." set expectedPerRangeStat {"0 5 5 0 5 5 5 0 0 50 50 0 0 5 5 0"} if {[designL23TrafficPerSession perRange $expectedPerRangeStat] == 1} { log "Fail: The Per Range stats are not correct" ixNetCleanUp return $FAILED } log "Pass: The Per Range stats are correct" # Stop TWAMP log "Stopping TWAMP on the both ports" if {[ixNet exec stop $ipEndpoint1] != "::ixNet::OK"} { log "Unable to stop TWAMP at 1st Port" ixNetCleanUp return $FAILED } log "TWAMP stopped at 1st Port successfully" if {[ixNet exec stop $ipEndpoint2] != "::ixNet::OK"} { log "Unable to stop TWAMP at 2nd Port" ixNetCleanUp return $FAILED } log "TWAMP stopped at 2nd Port successfully" ixNetCleanUp return $PASSED } #-----------------------------------------------------------------------------# # Execute the Action procedure defined above # #-----------------------------------------------------------------------------# Execute_Action