################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how IxNetwork-IxReporter API can be # # used in order to generate a detailed pdf report using a custom template # # Module: # # The sample was tested on an XMVDC16 module. # ################################################################################ set IXN_TCL_SERVER 10.200.113.27 set CHASSIS_IP 10.200.113.61 set PORT_LIST [list {1 11} {1 12}] puts " load ixNetwork Tcl API package" package req IxTclNetwork puts " connect to ixNetwork Tcl server" ixNet connect $IXN_TCL_SERVER -port 8009 -version 6.0 puts " load the binary config with 2 ports pre configured with traffic" ixNet exec loadConfig [ixNet readFrom "ixReporter.ixncfg"] puts " creating variables for the list of virtual ports and also for each virtual port" set vport_list [ixNet getList [ixNet getRoot] vport] set vport1 [lindex $vport_list 0] set card1 [lindex [lindex $PORT_LIST 0] 0] set port1 [lindex [lindex $PORT_LIST 0] 1] set vport2 [lindex $vport_list 1] set card2 [lindex [lindex $PORT_LIST 1] 0] set port2 [lindex [lindex $PORT_LIST 1] 1] puts " assign the virtual ports to real ports" ixTclNet::AssignPorts [list [list $CHASSIS_IP $card1 $port1] [list $CHASSIS_IP $card2 $port2]] {} [list $vport1 $vport2] force after 10000 puts " starting ospf" ixNet exec startAllProtocols after 10000 puts " configuring reporter settings" ixNet setMultiAttrs [ixNet getRoot]/reporter/testParameters \ -testCategory "Ixia Demo IxReporter API" \ -testDUTName "No DUT just Ixia ports" \ -testerName "Ixia tester" \ -testHighlights "Ixia test summary pdf report sample" \ -testName "an Ixia sample" \ -testObjectives "to demo the IxReporter API" ixNet commit set template_path [ixNet getAttr [ixNet getRoot]/reporter/generate -templatePath] set template_dir [file dirname $template_path] set template_name "OSPF-Detailed.repx" set template_path [file join $template_dir $template_name] puts " using $template_path template" ixNet setMultiAttrs [ixNet getRoot]/reporter/generate \ -outputFormat pdf \ -outputPath {c:\detailedReport.pdf} \ -templatePath $template_path ixNet commit puts " saving detailed results" ixNet exec saveDetailedResults [ixNet getRoot]/reporter/saveResults while {[ixNet getAttribute [ixNet getRoot]/reporter/saveResults -state] != "done"} { after 1000 } puts " generating report" ixNet exec generateReport [ixNet getRoot]/reporter/generate while {[ixNet getAttribute [ixNet getRoot]/reporter/generate -state] != "done"} { after 1000 } puts "report c:\\detailedReport.pdf generation done" puts "TEST END ." puts " " puts " " puts " for more info on IxNetwork-IxReporter API please refer to the user manual or the build-in help" puts " " puts "ixNet help [ixNet getRoot]/reporter" puts "[ixNet help [ixNet getRoot]/reporter]" puts " " puts "ixNet help [ixNet getRoot]/reporter/testParameters" puts "[ixNet help [ixNet getRoot]/reporter/testParameters]" puts " " puts "ixNet help [ixNet getRoot]/reporter/generate" puts "[ixNet help [ixNet getRoot]/reporter/generate]" puts " " puts "ixNet help [ixNet getRoot]/reporter/saveResults" puts "[ixNet help [ixNet getRoot]/reporter/saveResults]"