################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ source $env(IXNETWORK_SAMPLE_SCRIPT_DIR)/IxNetwork/Classic/Tcl/TestRun/config.tcl #------------------------------------------------------------------------------ # PROCEDURE : Action # PURPOSE : Encapsulating all of your testing actions # INPUT : (1) [list $chassis1 $card1 $port1 $client1 $tcpPort1] # (2) [list $chassis2 $card2 $port2 $client2 $tcpPort2] # (3) home; (the current directory) # RETURN VALUE : FAILED (1) or PASSED (0) #------------------------------------------------------------------------------ proc Action {portData1 portData2} { source $::pwd/ldpUtilsQa.tcl # initialize return value set FAILED 1 set PASSED 0 # get port info 1 set chassisIp1 [lindex $portData1 0] set card1 [lindex $portData1 1] set port1 [lindex $portData1 2] set client1 [lindex $portData1 3] set tcpPort1 [lindex $portData1 4] # get port info 2 set chassisIp2 [lindex $portData2 0] set card2 [lindex $portData2 1] set port2 [lindex $portData2 2] set client2 [lindex $portData2 3] set tcpPort2 [lindex $portData2 4] if {$client1 == $client2} { set status "" puts "Connecting to client $client1" if {[catch {set status [ixNet connect $client1 -port $tcpPort1]} error]} { puts "Unable to connect to ixNetwork" return $FAILED } if {[string equal $status "::ixNet::OK"] != 1} { puts "connection to client unsuccessful" return $FAILED } } else { puts "Try to use the same client" return $FAILED } # clean up all the existing configurations from client puts "cleaning up the client" ixNetCleanUp puts "Executing from [pwd]" #Creating New Config ixNet exec newConfig puts "loading ixncfg file ..." # load config files if {[ixNet exec loadConfig [ixNet readFrom "$::pwd/config.ldp_PW-status_stats.ixncfg"]] != "::ixNet::OK"} { puts "Error in sourcing the file config.refreshCfmCcmLearnedInfo.ixncfg" return $FAILED } else { # For stand alone test puts "Loading IxNetwork config file : passed" } # Assign real ports to virtual ports puts "getting virtual ports ...." set vPorts [ixNet getList [ixNet getRoot] vport] set vPort1 [lindex $vPorts 0] set vPort2 [lindex $vPorts 1] puts "Virtual ports are = $vPorts" set realPortsList [list [list $chassisIp1 $card1 $port1]\ [list $chassisIp2 $card2 $port2]] # Assign virtual ports to real ports puts "Assign virtual ports to real ports ..." set force true set status [ixTclNet::AssignPorts $realPortsList {} $vPorts force] puts "Assigned: $status" ixNet commit if {[string equal [lindex $status 0] $vPort1] != 1 || \ [string equal [lindex $status 1] $vPort2] != 1} { ixNetCleanUp return $flag } # get ldp from protocol management set portList1 [list [list $chassisIp1 $card1 $port1]] set ldpProtocolMgmt1 "$vPort1/protocols/ldp" set ldpProtocolMgmt2 "$vPort2/protocols/ldp" set l2Vcrange1 [lindex [ixNet getList [lindex [ixNet getList \ [lindex [ixNet getList $ldpProtocolMgmt1 router] 0] l2Interface] 0] l2VcRange] 0] set l2Vcrange2 [lindex [ixNet getList [lindex [ixNet getList \ [lindex [ixNet getList $ldpProtocolMgmt2 router] 0] l2Interface] 0] l2VcRange] 0] set pwstatustlvoption1 [ixNet getAtt $l2Vcrange1 -enablePwStatusTlv] set pwstatustlvoption2 [ixNet getAtt $l2Vcrange2 -enablePwStatusTlv] if {$pwstatustlvoption1 && $pwstatustlvoption2 == "true"} { ixNet exec start $ldpProtocolMgmt1 ixNet exec start $ldpProtocolMgmt2 puts "LDP started" puts "LDP started" puts "waiting for 35 seconds for down interval" after 35000 set expectedStat {"LDP Basic Sessions Up" 1 \ "LDP Targeted Sessions Up" 1 \ "LDP Targeted Sessions Configured" 1 \ "LDP PW Status Down" 1 \ "LDP Aggregated PW Status Notification Tx" 1 \ "LDP Aggregated PW Status Notification Rx" 1} set status [checkAllLdpStats $portList1 $expectedStat] if {$status != 0} { ixNetCleanUp set flag 1 return $flag } puts "waiting for 40 seconds for up interval" after 40000 set expectedStat {"LDP Basic Sessions Up" 1 \ "LDP Targeted Sessions Up" 1 \ "LDP Targeted Sessions Configured" 1 \ "LDP PW Status Down" 0 \ "LDP Aggregated PW Status Notification Tx" 1 \ "LDP Aggregated PW Status Notification Rx" 1 \ "LDP Aggregated PW Status Cleared Tx" 1 \ "LDP Aggregated PW Status Cleared Rx" 1} set status [checkAllLdpStats $portList1 $expectedStat] if {$status != 0} { ixNetCleanUp set flag 1 return $flag } } else { puts "PW-Status is not enabled: FAILED " ixNetCleanUp return $flag } ixNetCleanUp set flag 0 return $flag } #-----------------------------------------------------------------------------# # Execute the Action procedure defined above # #-----------------------------------------------------------------------------# Execute_Action