################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # Procedure : generateApplyTraffic # Purpose : To Generate and Apply Traffic # Parameters : None # Return : (Bool) 0 - Applied Traffic 1 - Failed to Apply Traffic ################################################################################ proc generateApplyTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic # Generate Traffic set genTraffic [ixNet setAtt $traffic -refreshLearnedInfoBeforeApply true] if {$genTraffic != "::ixNet::OK"} { puts "Not able to generate the traffic.." return $flag } after 10000 puts "Appling the traffic...." set appTraffic [::ixNet exec apply $traffic] if {$appTraffic != "::ixNet::OK"} { puts "Not able to apply the traffic.." return $flag } after 10000 set flag 0 return $flag } ################################################################################ #Procedure : startTraffic #Purpose : To Start the Traffic #Parameters : None #Return : (Bool) 0 - Started Traffic Successfully 1 - Failed to Start the Traffic ################################################################################ proc startTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic puts "Starting the traffic..." set startTraffic [::ixNet exec start $traffic] if {$startTraffic != "::ixNet::OK"} { puts "Not able to start the traffic.." return $flag } set flag 0 return $flag } ################################################################################ #Procedure :stopTraffic #Purpose : To Stop the Traffic #Parameters : None #Return : (Bool) 0 - Stopped Traffic Successfully 1 - Failed to Stop the Traffic ################################################################################ proc stopTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic puts "Stopping the traffic...." set stopTraffic [::ixNet exec stop $traffic] if {$stopTraffic != "::ixNet::OK"} { puts "Not able to stop the traffic.." return $flag } after 10000 set flag 0 return $flag } ################################################################################ #Procedure : captureMode #Purpose : To change the mode of the Port p2 to Capture Mode #Parameters : port (port) #Return : None ################################################################################ proc captureMode {port} { ixNet setAttribute $port -rxMode capture ixNet setAttribute $port/capture -hardwareEnabled true ixNet commit after 5000 } ################################################################################ #Procedure : measureMode #Purpose : To change the mode of the port p2 to measure flow mode #Parameters : port (port ) #Return : None ################################################################################ proc measureMode {port} { ixNet setAttribute $port -rxMode measure ixNet setAttribute $port/capture -hardwareEnabled false ixNet commit after 5000 } ################################################################################ #Procedure : TxRxCalculation #Purpose : To calculate the Tx - Rx Rate and to check if the Rx rate is equal to expected Rx Rate #Parameters : TxFrame Value RxFrame Value #Return : (Bool) 0 - If the Rx Frame is greater than or equal to delta percentage the value of Tx Frame ################################################################################ proc TxRxCalculation {TxFrame RxFrame {tolerance 15} } { set flag 1 set minRxFrame [expr ($TxFrame - ($TxFrame * $tolerance)/100)] puts "Frames Received: $RxFrame Frames Transmitted: $TxFrame (considering 15%% tolerence $minRxFrame)" if {$RxFrame < $minRxFrame} { puts "Frames Received is less than Frames Transmitted (considering 15%% tolerence)" return $flag } set flag 0 return $flag } ################################################################################ #Procedure : checkAllTrafficStats #Purpose : To verify Traffic Stats for specified tolerance #Parameters : pageMax, rowPerPage, tolerance #Return : (Bool) 0 - If the no. of Rx Frames is less than or equal to no. of Tx Frames within tolerance. ################################################################################ proc checkAllTrafficStats {{tolerance 0} {rowPerPage 50} {pageList "all"}} { set flag 1 set statistic [ixNet getRoot]/statistics set statsViewList [ixNet getList $statistic trafficStatViewBrowser] set indexOftrafficStats [lsearch -regexp $statsViewList "Traffic Statistics"] set trafficStatsView [lindex $statsViewList $indexOftrafficStats] ixNet setAttr $trafficStatsView -enabled true ixNet setAttr $trafficStatsView -pageSize $rowPerPage ixNet commit set pageMax [ixNet getAttr $trafficStatsView -totalPages] puts "Actual Number of pages available: $pageMax" set pagesToBrowse {} for {set page 1} {$page <= $pageMax} {incr page} { lappend pagesToBrowse $page } if {$pageList != "all"} { set pagesToBrowse $pageList } # Verify TxFrames and RxFrames for all the flows foreach page $pagesToBrowse { if {$page > $pageMax} { puts "Can't browse for $page, max Page available is $pageMax" return $flag } ixNet setAttr $trafficStatsView -currentPageNumber $page ixNet commit after 3000 # check if Stats are ready before verifying them set count 0 set isComplete false puts "check if Traffic Stats are ready..." while { $isComplete != true } { set isComplete [ixNet getAttr $trafficStatsView -isReady] puts "isComplete --> $isComplete" after 1000 incr count if { $count > 30 } { puts "Traffic Stats are still not ready ..." return $flag } } puts "Traffic Stats are ready ..." set indexMax [llength [ixNet getList $trafficStatsView row]] puts "Page $page :: Number of rows $indexMax" for {set index 0} {$index < $indexMax} {incr index} { set row [lindex [ixNet getList $trafficStatsView row] $index] set stats [ixNet getList $row cell] set RxFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats {Rx Frames}]] -statValue] set TxFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats {Tx Frames}]] -statValue] set minRxFrames [expr ($TxFrames - ($TxFrames * $tolerance)/100)] if {($TxFrames <= 0) || ($RxFrames <= 0) || ($RxFrames < $minRxFrames) || ($RxFrames > $TxFrames)} { puts "Stats are not proper for Page $page and Row $index " return $flag } puts "Page No=$page : Row No=$index Traffic Stats correct" } puts "Page: $page Traffic Stats Verification completed...." } set flag 0 return $flag } ################################################################################ #Procedure : checkConditionalTrafficStats #Purpose : To verify Conditional Traffic Stats #Parameters : sortStatName needCols maxResults performerType showBestPerformers deadFlowTimeout tolerance #Return : (Bool) 0 - If the conditional stats are fine ################################################################################ proc checkConditionalTrafficStats {sortStatName needCols {maxResults 50} {performerType showBestPerformers} {deadFlowTimeout 5} {tolerance 0}} { set flag 1 puts "Creating conditional flows" set viewCaption [ixTclNet::CreateConditionalFlowDetectiveView $maxResults $performerType $sortStatName $deadFlowTimeout] puts "\nviewCaption = $viewCaption" ixTclNet::GetFilteredSnapshotData $viewCaption $needCols StatValueArray 20 1 parray StatValueArray puts "Entering flowDetective to fetch information" set flowDetective [ixNet getRoot]/statistics/drilldown/flowDetective # There will be always one view that's why we consider index always 0 in the lindex command set conditionalTrafficStatsView [ixNet getList $flowDetective view] set conditionalTrafficStatsView1 [lindex $conditionalTrafficStatsView 0] ixNet setAttribute $conditionalTrafficStatsView1 -enabled True ixNet commit # Check if Conditional Traffic Stats is ready set count 0 set isComplete false puts "Check if Conditional Traffic Stats are ready..." while {$isComplete != true} { set isComplete [ixNet getAttr $conditionalTrafficStatsView1 -isReady] puts "isComplete --> $isComplete" after 1000 incr count if { $count > 30 } { puts "Conditional Traffic Stats are still not ready ..." return $flag } } puts "Conditional Traffic Stats are ready ..." for {set index 0} {$index < $maxResults} {incr index} { set row [lindex [ixNet getList $conditionalTrafficStatsView1 row] $index] set stats [ixNet getList $row cell] set RxFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats {"Rx Frames"}]] -statValue] set TxFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats {"Tx Frames"}]] -statValue] set minRxFrames [expr ($TxFrames - ($TxFrames * $tolerance)/100)] if {($TxFrames <= 0) || ($RxFrames <= 0) || ($RxFrames < $minRxFrames) || ($RxFrames > $TxFrames)} { puts "Stats are not proper for Row $index " return $flag } puts "Row No=$index Conditional Traffic Stats correct" } puts "Conditional Traffic Stats verified sucessfully" set flag 0 return $flag }