################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ #------------------------------------------------------------------------------- # PURPOSE OF THE SCRIPT: # PBBTE periodic learned info check and Protocol Stat and Packet structure # Varification. # # SCRIPT-GEN USED : Yes # config.pbbte.tcl # Configure 1 Bridge in each port with 1 Trunk. # Periodic LinkTrace , LoopBack,Delay Measurement is enabled # with 2 iteration with interval of 5 sec. # # # IXNCFG USED : No # # # Sequence of events being carried out by the script # 1) Load the config file # 2) Start the capture in the second port # 3) Start PBBTE protocol & Wait for some time # 4) Varify the periodic learned information # 5) Check the Stats of the PBBTE Protocol # 6) Start The Traffic and wait for some time # 7) Stop The Traffic # 8) Check the hex format of the received Packet # 9) Start The Traffic and wait for some time # 10) Stop The Traffic # 11) Varify wheather traffic is received in the second Port # # #------------------------------------------------------------------------------- #------------------------------------------------------------------------------ # Standard package to include all IxNetwork APIs #------------------------------------------------------------------------------ source $env(IXNETWORK_SAMPLE_SCRIPT_DIR)/IxNetwork/Classic/Tcl/TestRun/config.tcl #------------------------------------------------------------------------------ # PROCEDURE : Action # PURPOSE : Encapsulating all of your testing actions # INPUT : (1) [list $chassis1 $card1 $port1 $client1 $tcpPort1] # (2) [list $chassis2 $card2 $port2 $client2 $tcpPort2] # (3) home; (the current directory) # RETURN VALUE : FAILED (1) or PASSED (0) #------------------------------------------------------------------------------ proc Action {portData1 portData2} { # initialize return value set FAILED 1 set PASSED 0 source $::pwd/pbbteCommonUtils.tcl source $::pwd/pbbteTrfficUtils.tcl source $::pwd/Stat.tcl # get port info 1 set chassisIp1 [lindex $portData1 0] set card1 [lindex $portData1 1] set port1 [lindex $portData1 2] set client1 [lindex $portData1 3] set tcpPort1 [lindex $portData1 4] # get port info 2 set chassisIp2 [lindex $portData2 0] set card2 [lindex $portData2 1] set port2 [lindex $portData2 2] set client2 [lindex $portData2 3] set tcpPort2 [lindex $portData2 4] if {$client1 == $client2} { set status "" puts "Connecting to client $client1" if {[catch {set status [ixNet connect $client1 -port $tcpPort1]} error]} { puts "Unable to connect to ixNetwork" return $FAILED } if {[string equal $status "::ixNet::OK"] != 1} { puts "connection to client unsuccessful" return $FAILED } } else { puts "Try to use the same client" return $FAILED } # clean up all the existing configurations from client puts "cleaning up the client" ixNetCleanUp puts "Executing from [pwd]" # load config files if {[catch {source "$::pwd/config.sample_script.pbbte.tcl"} err]} { puts $err puts "Loading Scriptgen config file : FAILED " ixNetCleanUp return $FAILED } puts "Loading Scriptgen config file : passed" # get the virtual port list puts "getting virtual ports ...." set vPorts [ixNet getList [ixNet getRoot] vport] set vPort1 [lindex $vPorts 0] set vPort2 [lindex $vPorts 1] puts "Virtual ports are = $vPorts" # getting the real port list set realPortsList [list [list $chassisIp1 $card1 $port1] \ [list $chassisIp2 $card2 $port2] ] puts "realPortsList = $realPortsList" # Assign virtual ports to real ports puts "Assign virtual ports to real ports ..." set force true set status [ixTclNet::AssignPorts $realPortsList {} $vPorts force] ixNet commit puts "Assigned: $status" if {[string equal [lindex $status 0] $vPort1] != 1 || \ [string equal [lindex $status 1] $vPort2] != 1} { ixNetCleanUp return $FAILED } ixTclNet::CheckLinkState $vPorts doneList puts "Waiting for 30 sec before starting ..." after 30000 # capture cleanup if {[catch {ixNet exec closeAllTabs} err] == 1} { puts "Failed to close existing analyser tabs " } after 2000 #Start the capture puts "Start Capturing packets" if {[catch {ixNet exec startCapture} err] == 1} { puts "Failed to start packet capture " ixNetCleanUp return $FAILED } puts "Starting Pbbte on both the ports.." ixNet exec start $vPort1/protocols/cfm ixNet exec start $vPort2/protocols/cfm # Expecting 2 LTM/LBM/DM having 5 sec interval (10 Sec) puts "Waiting for 15 Sec..." after 15000 set brobj [lindex [ixNet getList $vPort1/protocols/cfm bridge] 0] # First checking the periodic-LTM Learned information set checkInLearntInfoList {{"1" "VLANID 1 TPID 0x8100 Priority 0" "2" \ "00:00:00:00:00:02" "2" "0" "0" "0" "1" \ "00 00 00 00 00 02" "Complete Reply" "00:00:00:00:00:01"}} if {[checkPbbtePeriodicOAMLTLearnedInfo $brobj $checkInLearntInfoList]==1} { puts "All the attributes did not matched" return $FAILED } # Second checking the periodic-LBM Learned information set checkInLearntInfoList {{"VLANID 1 TPID 0x8100 Priority 0" "00:00:00:00:00:02" \ "2" "0" "0" "true" "00:00:00:00:00:01"}} if {[checkPbbtePeriodicOAMLBLearnedInfo $brobj $checkInLearntInfoList] == 1} { puts "All the attributes did not matched" return $FAILED } #Third checking the periodic-DM Learned information set checkInLearntInfoList {{"VLANID 1 TPID 0x8100 Priority 0" "2" "00:00:00:00:00:02" \ "0" "0" "00:00:00:00:00:01"}} if {[checkPbbtePeriodicOAMDMLearnedInfo $brobj $checkInLearntInfoList]==1} { puts "All the attributes did not matched" return $FAILED } #Checking the PBBTE Stats puts "%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%" set completeStats { "CFM Number Of Bridges Configured" 1 \ "CFM Number Of Bridges Running" 1 \ "MEPs Configured" 0 \ "MEPs Running" 0 \ "MAs Configured" 1 \ "MAs Running" 1 \ "Remote MEPs" 1 \ "Trunks Configured" 1 \ "Trunks Running" 1 \ "CFM LTM Tx" 2 \ "CFM LTM Rx" 2 \ "CFM LTR Tx" 2 \ "CFM LTR Rx" 2 \ "CFM LBM Tx" 2 \ "CFM LBM Rx" 2 \ "CFM LBR Tx" 2 \ "CFM LBR Rx" 2 \ "CFM AIS Tx" 0 \ "CFM AIS Rx" 0 \ "CFM DMM Tx" 2 \ "CFM DMM Rx" 2 \ "CFM DMR Tx" 2 \ "CFM DMR Rx" 2 \ "Invalid CCM Rx" 0 \ "Invalid LBM Rx" 0 \ "Invalid LBR Rx" 0 \ "Invalid LTM Rx" 0 \ "Invalid LTR Rx" 0 \ "Defective RMEPS" 0 \ "CCM Unexpected Period" 0 \ "Out of Sequence CCM Rx" 0 \ "RMEP Ok" 1 \ "RMEP Error NoDefect" 1 \ "RMEP Error Defect" 0 \ "MEP FNG Reset" 1 \ "MEP FNG DefectReported" 0 \ "MEP FNG DefectClearing" 0 \ "LR Respond" 2} # Varifying the stat for the first Port set portList [list $portData1] if {[checkAllCfmStats $portList $completeStats 1]} { puts "Failure: Did not get the expected value for the all stats" ixNetCleanUp return $FAILED } puts "Success: Got expected values for all the stats" # Traffic Start if [generateApplyTraffic] { puts "Failed to start traffic" ixNetCleanUp return $FAILED } puts "Traffic applied successfully" if [startTraffic] { puts "Failed to start the traffic" ixNetCleanUp return $FAILED } puts "Traffic started successfully" puts "Waiting for 10 seconds for running the traffic" after 10000 # Traffic Stop if [stopTraffic] { puts "Failed to stop traffic" ixNetCleanUp return $FAILED } puts "Stoping PBBTE ... " ixNet exec stop $vPort1/protocols/cfm ixNet exec stop $vPort2/protocols/cfm after 5000 # Stop the capture puts "Stopping the capture" if {[catch {ixNet exec stopCapture} err] == 1} { puts "Failed to stop packet capture " ixNetCleanUp return $FAILED } # Packet structure # 0 1 2 3 # 0+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | Destination MAC Address | # 4+ +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | | | # 8+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ + # | Source MAC Address | # 12+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | Ether Type | S-Vlan | # 16+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | CFM Ether Type |MD l | Version | Op Code = 1 | # 20+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | Flags | 1st TLV Octet | Transaction Identifier (e.g.-| # 24+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | - Sequence Number) | | # 28+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ + # | Maintenance Association Identifier | # + + # | | # 74+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | RESERVED Y.1731 | # 90+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | RESERVED | # +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | Optional TLV | # +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # | FCS | # +-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+-+ # # t. set matchFieldList {19 19 "03" \ 26 32 "03 00 04 44 61 74 61" \ 33 39 "1F 00 04 10 00 00 00"} if {[verifyCapturedPackets $chassisIp2 $card2 $port2 $matchFieldList] == 1} { puts "Expected field value match not found in capture buffer \ for the port $chassisIp2 $card2 $port2" ixNetCleanUp return $FAILED } puts "Wait for 10 sec" after 10000 #Disabling Capture on ports ixNet setAttribute $vPort1 -rxMode measure ixNet setAttribute $vPort1/capture -hardwareEnabled False ixNet setAttribute $vPort1/capture -softwareEnabled False ixNet setAttribute $vPort2 -rxMode measure ixNet setAttribute $vPort2/capture -hardwareEnabled False ixNet setAttribute $vPort2/capture -softwareEnabled False ixNet commit # Changing the port to Measure Mode puts "Changing the port to Measure Mode ..." if {[ixNet setAttribute $vPort2 -rxMode measure]!= "::ixNet::OK"} { puts "Failed to change the rxMode of the port to measure flow" ixNetCleanUp return $FAILED } ixNet commit after 5000 # Increase line rate to 100% from traffic api puts "Changing line rate to 100... " set traffic [ixNet getRoot]/traffic set lineRate [ixNet setAtt [lindex [ixNet getList \ $traffic trafficItem] 0]/rateOptions -lineRate 100] if {$lineRate != "::ixNet::OK"} { puts "Not able to change the line rate to 100..." ixNetCleanUp return $FAILED } ixNet commit after 3000 puts "Starting PBBTE ... " ixNet exec start $vPort1/protocols/cfm ixNet exec start $vPort2/protocols/cfm after 2000 # Traffic Start if [generateApplyTraffic] { puts "Failed to start traffic" ixNetCleanUp return $FAILED } if [startTraffic] { puts "Failed to start traffic" ixNetCleanUp return $FAILED } puts "Traffic started successfully" puts "Waiting for 5 seconds..." after 5000 # Traffic Stop if [stopTraffic] { puts "Failed to stop traffic" ixNetCleanUp return $FAILED } ixNet commit after 10000 #--------------------------------------------------------------------------- # First we are checking at least traffic statistics is comming in traffic # statistics view. What we will do to verify this is: Select a row from # the traffic statistics; and confirm that there is some non-zero stats. #--------------------------------------------------------------------------- puts "Checking traffic statistics" set statistic [ixNet getRoot]/statistics set statViewList [ixNet getList [ixNet getRoot]/statistics \ trafficStatViewBrowser] set indexOftraffStats [lsearch -regexp $statViewList "Traffic Statistics"] set trafficStats [lindex $statViewList $indexOftraffStats] ixNet setAttr $trafficStats -enabled true ixNet commit set rows [ixNet getList $trafficStats row] set row1 [lindex $rows 0] set stats [ixNet getList $row1 cell] set rxFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats \ {Rx Frames}]] -statValue] set txFrames [ixNet getAttr [lindex $stats [lsearch -regexp $stats \ {Tx Frames}]] -statValue] set txframes [expr ($txFrames / 20)] set txFrames $txFrames set txFramesLess [expr ($txFrames - $txframes)] set txFramesMore [expr ($txFrames + $txframes)] if {$rxFrames <= $txFramesMore && $rxFrames >= $txFramesLess} { puts "Trafffic is getting received on the other end" } else { puts "Traffic is not getting recieved on the other end" ixNetCleanUp return $FAILED } puts "Traffic stats checking successfull" ixNetCleanUp return $PASSED } #-----------------------------------------------------------------------------# # Execute the Action procedure defined above # #-----------------------------------------------------------------------------# Execute_Action