################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to create a custom view # # Module: # # The sample was tested on an XMVDC16 module. # ################################################################################ # edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.200.115.204 set ixTclPort 8009 set ports {{10.200.115.151 3 11} {10.200.115.151 3 12}} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 6.30 –setAttribute strict puts "Load the IxNetwork config" ixNet exec loadConfig [ixNet readFrom config.custom-views.ixncfg] set vPorts [ixNet getList [ixNet getRoot] vport] puts "Assigning virtual ports to real ports" ::ixTclNet::AssignPorts $::ixia::ports {} $vPorts force puts "Starting all protocols" ixNet exec startAllProtocols puts "Waiting for 30 sec" after 30000 puts "Add the custom view" set custom_view [ixNet add [ixNet getRoot]/statistics view] ixNet setAttr $custom_view -caption "protocols-access" ixNet setAttr $custom_view -type layer23ProtocolAuthAccess ixNet setAttr $custom_view -visible true ixNet commit set custom_view [lindex [ixNet remapIds $custom_view] 0] puts "Configure the protocol filter" set availableProtocolFilter [ixNet getList $custom_view availableProtocolFilter] ixNet setAttr $custom_view/layer23ProtocolAuthAccessFilter -protocolFilterIds [lindex $availableProtocolFilter 0] ixNet commit puts "Configure the port filter" set availablePortFilter [ixNet getList $custom_view availablePortFilter] ixNet setAttr $custom_view/layer23ProtocolAuthAccessFilter -portFilterIds [list [lindex $availablePortFilter 0]] ixNet commit puts "Enable only few stats columns to be disaplyed" set statsList [ixNet getList $custom_view statistic] foreach stat [lrange $statsList 0 5] { ixNet setAttr $stat -enabled true } ixNet commit puts "Get the custom view going and start retrieveing stats" ixNet setAttribute $custom_view -enabled true ixNet commit puts "TEST END." puts " " puts " " puts "For more info please refer to the user manual or the built-in help" puts " " puts "ixNet help ::ixNet::OBJ-/statistics/view" puts "[ixNet help ::ixNet::OBJ-/statistics/view]" puts " " puts "ixNet help ::ixNet::OBJ-/statistics/view/layer23ProtocolAuthAccessFilter" puts "[ixNet help ::ixNet::OBJ-/statistics/view/layer23ProtocolAuthAccessFilter]" puts " " puts "ixNet help ::ixNet::OBJ-/statistics/view/statistic" puts "[ixNet help ::ixNet::OBJ-/statistics/view/statistic]"