################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ #-----------------------------------------------------------------------------# # IF this file is already sourced; it should not be sourced once more # #-----------------------------------------------------------------------------# if {[info exists ::SETUP_ENV]} { # source only common utils path source $::COMMOM_UTILS_PATH/commonUtilities.tcl return } #-----------------------------------------------------------------------------# # Find the Ixia Installation Directory # #-----------------------------------------------------------------------------# set IXIA_INSTALL_DIR "C:/Program Files (x86)/Ixia/IxNetwork/$::IX_NETWORK" #-----------------------------------------------------------------------------# # Find the common utilities directory # #-----------------------------------------------------------------------------# set ::COMMOM_UTILS_PATH \ "$IXIA_INSTALL_DIR/SampleScripts/IxNetwork/Classic/Tcl/CommonUtils" #-----------------------------------------------------------------------------# # Find the registry key path of IXOS # #-----------------------------------------------------------------------------# set ixos $::IXOS_BUILD set registryKeyPath \ "HKEY_LOCAL_MACHINE\\Software\\Ixia Communications\\IxOS\\$ixos\\InstallInfo" #-----------------------------------------------------------------------------# # Load IXOS package (IxTclHAL) # #-----------------------------------------------------------------------------# if {$::tcl_platform(platform) == "windows"} { package require registry 1 set ::_IXOS_INSTALL_ROOT [registry get $registryKeyPath HOMEDIR] set ::_IXOS_PKG_DIR $::_IXOS_INSTALL_ROOT lappend ::auto_path $::_IXOS_PKG_DIR source "$::_IXOS_PKG_DIR\\TclScripts\\bin\\IxiaWish.tcl" if {[catch {package req IxTclHal} errorMsg]} { puts "Unable to load IxTclHal ...." puts "Make sure that IXOS BUILD is specified/installed properly" error "$errorMsg" } } #-----------------------------------------------------------------------------# # include the package IxTclNetwork # #-----------------------------------------------------------------------------# if {[catch {package req IxTclNetwork} errMsg]} { puts "unable to load package IxTclNetwork" error $errMsg } #-----------------------------------------------------------------------------# # include the package IxTclHal # #-----------------------------------------------------------------------------# if {[catch {package req IxTclHal} errMsg]} { puts "unable to load package IxTclHal" error $errMsg } #-----------------------------------------------------------------------------# # Withdraw the TK window # #-----------------------------------------------------------------------------# set isError [catch {wm withdraw .; update} errMsg] if {$isError} {puts "$errMsg"} #-----------------------------------------------------------------------------# # Source some test-management utility procedures # #-----------------------------------------------------------------------------# source $IXIA_INSTALL_DIR/SampleScripts/IxNetwork/Classic/Tcl/TestRun/wrapper.tcl #-----------------------------------------------------------------------------# # source the common utility files # #-----------------------------------------------------------------------------# source $::COMMOM_UTILS_PATH/commonUtilities.tcl #-----------------------------------------------------------------------------# # Rename old puts use new puts that will update puts statement immediately # # On the wish console # #-----------------------------------------------------------------------------# rename puts oldPuts proc puts {args} { lappend cmdString oldPuts foreach argument $args { lappend cmdString $argument } eval $cmdString unset cmdString update } #-----------------------------------------------------------------------------# # Define log functions (used extensively in test cases, same as puts) # #-----------------------------------------------------------------------------# proc log {str} {puts $str} #-----------------------------------------------------------------------------# # All the environment variables are sourced. Scripts must be able to get the # # following environment variables # # # # 1) $::IX_NETWORK --> IxNetwork build number # # 2) $::IXOS_BUILD --> IxOs build Number # # 3) $::COMMOM_UTILS_PATH --> Common utility file path # # 4) $::chassis --> Chassis IP # # 5) $::card1 --> Card 1 # # 6) $::card2 --> Card 2 # # 7) $::port1 --> Port 1 # # 8) $::port2 --> Port 2 # # 9) $::client --> Client IP # # 10) $::tcpPort --> TCP Port Number # # 11) $::argv0 --> the parent script name # #-----------------------------------------------------------------------------# set ::SETUP_ENV 1 update