################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # Procedure : generateApplyTraffic # Purpose : To Generate and Apply Traffic # Parameters : None # Return : (Bool) 0 - Applied Traffic 1 - Failed to Apply Traffic ################################################################################ proc generateApplyTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic # Generate Traffic set genTraffic [ixNet setAtt $traffic -refreshLearnedInfoBeforeApply true] if {$genTraffic != "::ixNet::OK"} { puts "Not able to generate the traffic.." return $flag } after 10000 puts "Appling the traffic...." set appTraffic [::ixNet exec apply $traffic] if {$appTraffic != "::ixNet::OK"} { puts "Not able to apply the traffic.." return $flag } after 10000 set flag 0 return $flag } ################################################################################ #Procedure : startTraffic #Purpose : To Start the Traffic #Parameters : None #Return : (Bool) 0 - Started Traffic Successfully 1 - Failed to Start the Traffic ################################################################################ proc startTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic puts "Starting the traffic..." set startTraffic [::ixNet exec start $traffic] if {$startTraffic != "::ixNet::OK"} { puts "Not able to start the traffic.." return $flag } set flag 0 return $flag } ################################################################################ #Procedure :stopTraffic #Purpose : To Stop the Traffic #Parameters : None #Return : (Bool) 0 - Stopped Traffic Successfully 1 - Failed to Stop the Traffic ################################################################################ proc stopTraffic {} { set flag 1 set traffic [ixNet getRoot]/traffic puts "Stopping the traffic...." set stopTraffic [::ixNet exec stop $traffic] if {$stopTraffic != "::ixNet::OK"} { puts "Not able to stop the traffic.." return $flag } after 10000 set flag 0 return $flag } ################################################################################ #Procedure : captureMode #Purpose : To change the mode of the Port p2 to Capture Mode #Parameters : port (port) #Return : None ################################################################################ proc captureMode {port} { ixNet setAttribute $port -rxMode capture ixNet setAttribute $port/capture -hardwareEnabled true ixNet commit after 5000 } ################################################################################ #Procedure : measureMode #Purpose : To change the mode of the port p2 to measure flow mode #Parameters : port (port ) #Return : None ################################################################################ proc measureMode {port} { ixNet setAttribute $port -rxMode measure ixNet setAttribute $port/capture -hardwareEnabled false ixNet commit after 5000 } ################################################################################ #Procedure : TxRxCalculation #Purpose : To calculate the Tx - Rx Rate and to check if the Rx rate is equal to expected Rx Rate #Parameters : TxFrame Value RxFrame Value #Return : (Bool) 0 - If the Rx Frame is greater than or equal to delta percentage the value of Tx Frame ################################################################################ proc TxRxCalculation {TxFrame RxFrame {tolerance 15} } { set flag 1 set minRxFrame [expr ($TxFrame - ($TxFrame * $tolerance)/100)] puts "Frames Received: $RxFrame Frames Transmitted: $TxFrame (considering 15%% tolerence $minRxFrame)" if {$RxFrame < $minRxFrame} { puts "Frames Received is less than Frames Transmitted (considering 15%% tolerence)" return $flag } set flag 0 return $flag } ################################################################################ # PACKET STRUCTURE VERIFICATION ################################################################################ #------------------------------------------------------------------------------- # PROCEDURE : verifyCapturedPackets # PURPOSE : Verifying expected field value in Captured Packets # PARAMETERS : chassis - # card - # port - # matchFieldList - list of {startIndex endIndex expectedVal} # expPktCnt - {default value 1} # RETURN : (BOOL) - 0 for Pass ~ 1 for Fail #------------------------------------------------------------------------------- proc verifyCapturedPackets {chassis card port matchFieldList {expPktCnt 1}} { set isError 1 puts "Initilizing thorugh IxTclHal...." ixInitialize $chassis chassis get $chassis set chassisId [chassis cget -id] port get $chassisId $card $port set putsinName [port cget -owner] ixLogin $putsinName puts "Logging in using the $putsinName" # Retrive captured packets captureBuffer get $chassisId $card $port set numCapturedPkts [captureBuffer cget -numFrames] puts "Captured $numCapturedPkts pkts (expected: $expPktCnt)" if {$numCapturedPkts < $expPktCnt} { return $isError } captureBuffer get $chassisId $card $port 1 $numCapturedPkts for {set f 1} {$f <= $numCapturedPkts} {incr f} { after 50 captureBuffer getframe $f after 50 set capframe [captureBuffer cget -frame] set mismatch 0 foreach {startIndex endIndex expectedVal} $matchFieldList { puts "Obtained: [lrange $capframe $startIndex $endIndex] \ Expected: $expectedVal" if {[lrange $capframe $startIndex $endIndex] != $expectedVal} { set mismatch 1 puts "Obtained: [lrange $capframe $startIndex $endIndex] \ Expected: $expectedVal ---> No Match" break } } if {$mismatch == 0} { puts "All Field Patterns Matched !!!" set isError 0 return $isError } } if {$mismatch == 1} { puts "Not all Field Patterns Matched !!!" return $isError } } proc pktFormat {packet} { set lenPkt [string length $packet] set cntr 00 puts "==========================================================" for {set i 0} {$i <= $lenPkt} {incr i 48} { if { $cntr < 100 } {puts -nonewline "00$cntr "} else {puts -nonewline "0$cntr "} puts -nonewline [string range $packet $i [expr $i+23]] puts -nonewline " " puts [string range $packet [expr $i+24] [expr $i+47]] set cntr [expr $cntr + 10] } puts "==========================================================" }