################################################################################# # Version 1.0 $Revision: 1 $ # $Author: Mario Dicu $ # # Copyright © 1997 - 2015 by IXIA # All Rights Reserved. # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures 10 IPv4 sessions on each of the two ports # # # ################################################################################ if 'py' not in dir(): class TestFailedError(Exception): pass class Py: pass py = Py() py.ports = [('10.205.15.62', 3, 5), ('10.205.15.62', 3, 6)] py.ixTclServer = '10.205.15.224' py.ixTclPort = 8009 ################################################################################ # Import the IxNet library ################################################################################ from IxNetwork import IxNet import time ixNet = IxNet() ################################################################################ # Connect to IxNet client ################################################################################ ixNet.connect(py.ixTclServer, '-port', py.ixTclPort, '-version', '7.40') ################################################################################ # Cleaning up IxNetwork ################################################################################ print "Cleaning up IxNetwork..." ixNet.execute('newConfig') ################################################################################ # Adding ports to configuration ################################################################################ print "Adding ports to configuration" root = ixNet.getRoot() ixNet.add(root, 'vport') ixNet.add(root, 'vport') ixNet.commit() vPorts = ixNet.getList(root, 'vport') vport1 = vPorts[0] vport2 = vPorts[1] ################################################################################ # Adding VXLAN Protocol ################################################################################ print "Add topologies" ixNet.add(root, 'topology') ixNet.add(root, 'topology') ixNet.commit() topo1 = ixNet.getList(root, 'topology')[0] topo2 = ixNet.getList(root, 'topology')[1] print "Add ports to topologies" ixNet.setAttribute(topo1, '-vports', vport1) ixNet.setAttribute(topo2, '-vports', vport2) ixNet.commit() print "Add device groups to topologies" ixNet.add(topo1, 'deviceGroup') ixNet.add(topo2, 'deviceGroup') ixNet.commit() dg1 = ixNet.getList(topo1, 'deviceGroup')[0] dg2 = ixNet.getList(topo2, 'deviceGroup')[0] print "Add Ethernet stacks to device groups" ixNet.add(dg1, 'ethernet') ixNet.add(dg2, 'ethernet') ixNet.commit() mac1 = ixNet.getList(dg1, 'ethernet')[0] mac2 = ixNet.getList(dg2, 'ethernet')[0] print "Add ipv4 stacks to Ethernets" ixNet.add(mac1, 'ipv4') ixNet.add(mac2, 'ipv4') ixNet.commit() ipv4_1 = ixNet.getList(mac1, 'ipv4')[0] ipv4_2 = ixNet.getList(mac2, 'ipv4')[0] print "Setting multi values for ipv4 addresses" ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-address') + '/counter', '-start', '22.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-gatewayIp') + '/counter', '-start', '22.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-address') + '/counter', '-start', '22.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-gatewayIp') + '/counter', '-start', '22.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.commit() print "Add VXLAN stacks to IPv4" ixNet.add(ipv4_1, 'vxlan') ixNet.add(ipv4_2, 'vxlan') ixNet.commit() vxlan_1 = ixNet.getList(ipv4_1, 'vxlan')[0] vxlan_2 = ixNet.getList(ipv4_2, 'vxlan')[0] ixNet.setMultiAttribute(ixNet.getAttribute(vxlan_1, '-vni') + '/counter', '-start', '1100', '-step', '1') ixNet.setMultiAttribute(ixNet.getAttribute(vxlan_1, '-ipv4_multicast') + '/counter', '-start', '225.0.0.1', '-step', '1.0.0.0') ixNet.setMultiAttribute(ixNet.getAttribute(vxlan_2, '-vni') + '/counter', '-start', '1100', '-step', '1') ixNet.setMultiAttribute(ixNet.getAttribute(vxlan_2, '-ipv4_multicast') + '/counter', '-start', '225.0.0.1', '-step', '1.0.0.0') print "Add Inner Device Groups to the Outer Device Groups" ixNet.add(dg1, 'deviceGroup') ixNet.add(dg2, 'deviceGroup') ixNet.commit() dg3 = ixNet.getList(dg1, 'deviceGroup')[0] dg4 = ixNet.getList(dg2, 'deviceGroup')[0] print "Add Ethernet stacks to the inner device groups" ixNet.add(dg3, 'ethernet') ixNet.add(dg4, 'ethernet') ixNet.commit() mac3 = ixNet.getList(dg3, 'ethernet')[0] mac4 = ixNet.getList(dg4, 'ethernet')[0] print "Add a connector between the Ethernet and VXLAN" ixNet.add(mac3, 'connector') ixNet.add(mac4, 'connector') ixNet.commit() connector1 = ixNet.getList(mac3, 'connector')[0] connector2 = ixNet.getList(mac4, 'connector')[0] ixNet.setAttribute(connector1, '-connectedTo', vxlan_1) ixNet.setAttribute(connector2, '-connectedTo', vxlan_2) ixNet.commit() print "Add IPv4 stacks to inner Ethernets" ixNet.add(mac3, 'ipv4') ixNet.add(mac4, 'ipv4') ixNet.commit() ipv4_3 = ixNet.getList(mac3, 'ipv4')[0] ipv4_4 = ixNet.getList(mac4, 'ipv4')[0] print "Setting multi values for inner IPv4 addresses" ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_3, '-address') + '/counter', '-start', '5.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_3, '-gatewayIp') + '/counter', '-start', '5.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_3, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_4, '-address') + '/counter', '-start', '5.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_4, '-gatewayIp') + '/counter', '-start', '5.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_4, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.commit() ################################################################################ # Assign ports ################################################################################ vports = ixNet.getList(ixNet.getRoot(), 'vport') print "Assigning ports to " + str(vports) + " ..." assignPorts = ixNet.execute('assignPorts', py.ports, [], ixNet.getList("/","vport"), True) if assignPorts != vports: raise TestFailedError("FAILED assigning ports. Got %s" %assignPorts) else: print("PASSED assigning ports. Got %s" %assignPorts) ################################################################################ # Start All Protocols ################################################################################ print "Starting All Protocols" ixNet.execute('startAllProtocols') print "Sleep 30sec for protocols to start" time.sleep(30)