# -*- coding: cp1252 -*- ################################################################################ # Version 1.0 $Revision: 1 $ # # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # # Revision Log: # # 29/06/2018 - Rupkatha Guha - created sample # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to configure ESMC topology # # # # About Topology: # # # # On the port, configure an ESMC topology with extended Quality Level # # enabled. # # # # Script Flow: # # 1. Configuration of protocols as described in topology. # # 2. Start the ESMC protocol. # # 3. Retrieve protocol statistics. # # 4. Stop all protocols. # # # # Ixia Software: # # IxOS 9.10 EB # # IxNetwork 9.10 EB # # # ################################################################################ import os import sys import time def assignPorts (ixNet, realPort1) : chassis1 = realPort1[0] card1 = realPort1[1] port1 = realPort1[2] root = ixNet.getRoot() vport1 = ixNet.add(root, 'vport') ixNet.commit() vport1 = ixNet.remapIds(vport1)[0] chassisObj1 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj1, '-hostname', chassis1) ixNet.commit() chassisObj1 = ixNet.remapIds(chassisObj1)[0] cardPortRef1 = chassisObj1 + '/card:%s/port:%s' % (card1,port1) ixNet.setMultiAttribute(vport1, '-connectedTo', cardPortRef1, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 001') ixNet.commit() # end def assignPorts ################################################################################ # Either feed the ixNetwork library path in the sys.path as below, or put the # IxNetwork.pm file somewhere else where we python can autoload it. # "IxNetwork.pm" is available in \API\Python ################################################################################ ixNetPath = r'/home/lacp/regress-test/linux-run' sys.path.append(ixNetPath) import IxNetwork ################################################################################# # Give chassis/client/ixNetwork server port/ chassis port HW port information # below ################################################################################# ixTclServer = '10.39.50.134' ixTclPort = '8779' ports = [('10.39.50.126', '1', '3',)] # get IxNet class ixNet = IxNetwork.IxNet() print("connecting to IxNetwork client") ixNet.connect(ixTclServer, '-port', ixTclPort, '-version', '9.10', '-setAttribute', 'strict') print("cleaning up the old configfile, and creating an empty config") ixNet.execute('newConfig') # assigning ports assignPorts(ixNet, ports[0]) time.sleep(5) root = ixNet.getRoot() vportTx = ixNet.getList(root, 'vport')[0] print("adding topologies") ixNet.add(root, 'topology', '-vports', vportTx) ixNet.commit() topologies = ixNet.getList(ixNet.getRoot(), 'topology') topo1 = topologies[0] print "Adding 2 device groups" ixNet.add(topo1, 'deviceGroup') ixNet.commit() t1devices = ixNet.getList(topo1, 'deviceGroup') t1dev1 = t1devices[0] print("Configuring the multipliers (number of sessions)") ixNet.setAttribute(t1dev1, '-multiplier', '1') ixNet.commit() print("Adding ethernet/mac endpoints") ixNet.add(t1dev1, 'ethernet') ixNet.commit() mac1 = ixNet.getList(t1dev1, 'ethernet')[0] print("Configuring the mac addresses %s" % (mac1)) ixNet.setMultiAttribute(ixNet.getAttribute(mac1, '-mac') + '/counter', '-direction', 'increment', '-start', '00:11:01:00:00:01', '-step', '00:00:00:00:00:01') ixNet.commit() print("Add esmc") ixNet.add(mac1, 'esmc') ixNet.commit() esmc1 = ixNet.getList(mac1, 'esmc')[0] print("Renaming the topologies and the device groups") ixNet.setAttribute(topo1, '-name', 'ESMC Topology') ixNet.commit() print("Enabling Extended Quality Level") customSyncE = ixNet.getAttribute(esmc1, '-extendedQlTlvEnable') customSyncE_enable = customSyncE + '/singleValue' ixNet.setMultiAttribute(customSyncE_enable, '-value', 'true') ixNet.commit() print("Setting the Quality Level to EEEC option1") ql = ixNet.getAttribute(esmc1, '-qualityLevel') qllevel = ql + '/singleValue' ixNet.setMultiAttribute(qllevel, '-value', 'ql_eeec_op1') ixNet.commit() print"Enabling Custom SyncE CLock Identity for topo1" customSyncE = ixNet.getAttribute(esmc1, '-enableCustomSyncEclockIdentity') customSyncE_enable = customSyncE + '/singleValue' ixNet.setMultiAttribute(customSyncE_enable, '-value', 'true') ixNet.commit() print("Setting the SyncE clock Identiy") custsync = ixNet.getAttribute(esmc1, '-customSyncEclockIdentity') custsync1 = custsync + '/singleValue' ixNet.setMultiAttribute(custsync1, '-value', '2202AAFD000006') ixNet.commit() print"Enabling Mixed EECs for topo1" mixed_eecs = ixNet.getAttribute(esmc1, '-mixedEECs') mixed_eecs_1 = mixed_eecs + '/singleValue' ixNet.setMultiAttribute(mixed_eecs_1, '-value', 'true') ixNet.commit() print"Enabling Partial Chain for topo1" partial_chain = ixNet.getAttribute(esmc1, '-partialChain') partial_Chain_1 = partial_chain + '/singleValue' ixNet.setMultiAttribute(partial_Chain_1, '-value', 'true') ixNet.commit() print("Configuring the number of cascased EECs") caseecs = ixNet.getAttribute(esmc1, '-numberOfCascadedEecs') caseecs1 = caseecs + '/singleValue' ixNet.setMultiAttribute(caseecs1, '-value', '4') ixNet.commit() print"Configuring the number of Cascaded eEECs" cascaded_Eeecs = ixNet.getAttribute(esmc1, '-numberOfCascadedEeecs') cascaded_Eeecs_1 = cascaded_Eeecs + '/singleValue' ixNet.setMultiAttribute(cascaded_Eeecs_1, '-value', '20') ixNet.commit() ################################################################################ # 2. Start all protocols and wait for 30 seconds ################################################################################ print("Starting protocols and waiting for 60 seconds for protocols to come up") ixNet.execute('startAllProtocols') time.sleep(30) ################################################################################ # 3. Retrieve protocol statistics. ################################################################################ print ("Fetching all Protocol Summary Stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"ESMC Per Port"/page' statcap = ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in ixNet.getAttribute(viewPage, '-rowValues') : for statVal in statValList : print("***************************************************") index = 0 for satIndv in statVal : print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 # end for # end for # end for print("***************************************************") ################################################################################ # 4. Stop all protocols ################################################################################ print ('Stopping protocols') ixNet.execute('stopAllProtocols') print ('!!! Test Script Ends !!!')