# -*- coding: cp1252 -*- ################################################################################ # Version 1.0 $Revision: 1 $ # # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use Low Level Python APIs to # # import BGP IPv4 Routes in Ixia csv format. # # 1. It will create 2 BGP topologies. # # 2. Generate Statistical IPv4 routes in topology2. # # 3. Start the BGP protocol. # # 4. Retrieve protocol statistics. # # 5. Retrieve protocol learned info. # # 6. Stop all protocols. # # # ################################################################################ import os import sys import time import generateIpMacCsv import overLay1Bit def assignPorts (ixNet, realPort1, realPort2) : chassis1 = realPort1[0] chassis2 = realPort2[0] card1 = realPort1[1] card2 = realPort2[1] port1 = realPort1[2] port2 = realPort2[2] root = ixNet.getRoot() vport1 = ixNet.add(root, 'vport') ixNet.commit() vport1 = ixNet.remapIds(vport1)[0] vport2 = ixNet.add(root, 'vport') ixNet.commit() vport2 = ixNet.remapIds(vport2)[0] chassisObj1 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj1, '-hostname', chassis1) ixNet.commit() chassisObj1 = ixNet.remapIds(chassisObj1)[0] if (chassis1 != chassis2) : chassisObj2 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj2, '-hostname', chassis2) ixNet.commit() chassisObj2 = ixNet.remapIds(chassisObj2)[0] else : chassisObj2 = chassisObj1 # end if cardPortRef1 = chassisObj1 + '/card:%s/port:%s' % (card1,port1) ixNet.setMultiAttribute(vport1, '-connectedTo', cardPortRef1, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 001') ixNet.commit() cardPortRef2 = chassisObj2 + '/card:%s/port:%s' % (card2,port2) ixNet.setMultiAttribute(vport2, '-connectedTo', cardPortRef2, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 002') ixNet.commit() # end def assignPorts ################################################################################ # Either feed the ixNetwork library path in the sys.path as below, or put the # # IxNetwork.py file somewhere else where we python can autoload it # # "IxNetwork.py" is available in \API\Python # ################################################################################ ixNetPath = r'C:\Program Files (x86)\Ixia\IxNetwork\8.20-EA\API\Python' sys.path.append(ixNetPath) import IxNetwork ################################################################################# # Give chassis/client/ixNetwork server port/ chassis port HW port information # # below # ################################################################################# ixTclServer = '10.216.108.113' ixTclPort = '8074' ports = [('10.216.108.96', '6', '3',), ('10.216.108.96', '6', '4',)] # get IxNet class ixNet = IxNetwork.IxNet() print("connecting to IxNetwork client %s %s" % (ixTclServer, ixTclPort)) ixNet.connect(ixTclServer, '-port', ixTclPort, '-version', '8.20', '-setAttribute', 'strict') # cleaning up the old configfile, and creating an empty config print("cleaning up the old configfile, and creating an empty config") ixNet.execute('newConfig') # assigning ports assignPorts(ixNet, ports[0], ports[1]) time.sleep(5) root = ixNet.getRoot() vportTx = ixNet.getList(root, 'vport')[0] vportRx = ixNet.getList(root, 'vport')[1] multiplier = 100 csvPath1 = './scaleStack.csv' csvPath2 = './myOneBit.csv' print("adding topologies") ixNet.add(root, 'topology', '-vports', vportTx) ixNet.add(root, 'topology', '-vports', vportRx) ixNet.commit() ############################################################################### # Add topologies ############################################################################### topologies = ixNet.getList(ixNet.getRoot(), 'topology') topo1 = topologies[0] topo2 = topologies[1] print ("Adding 2 device groups") ixNet.add(topo1, 'deviceGroup') ixNet.add(topo2, 'deviceGroup') ixNet.commit() ############################################################################### # Add device group ############################################################################### t1devices = ixNet.getList(topo1, 'deviceGroup') t2devices = ixNet.getList(topo2, 'deviceGroup') t1dev1 = t1devices[0] t2dev1 = t2devices[0] print("Configuring the multipliers (number of sessions)") ixNet.setAttribute(t1dev1, '-multiplier', multiplier) ixNet.setAttribute(t2dev1, '-multiplier', multiplier) ixNet.commit() ################################################################################ # Adding ethernet/mac endpoints ################################################################################ print("Adding ethernet/mac endpoints") ixNet.add(t1dev1, 'ethernet') ixNet.add(t2dev1, 'ethernet') ixNet.commit() mac1 = ixNet.getList(t1dev1, 'ethernet')[0] mac2 = ixNet.getList(t2dev1, 'ethernet')[0] ############################################################################### # Create a multivalue CSV ############################################################################### myMultiValueCsv = generateIpMacCsv.MultivalueCsv(csvPath1, multiplier) myMultiValueCsv.generate() ################################################################################ # Read MAC address from .csv file for port 1 ################################################################################ macAddrMv1 = ixNet.getAttribute(mac1, '-mac') valueListMv1 = ixNet.add(macAddrMv1, 'valueList') ixNet.execute('import', valueListMv1, ixNet.readFrom(csvPath1), "csv", '0') ixNet.commit() ################################################################################ # Read MAC address from .csv file port 2 ################################################################################ macAddrMv2 = ixNet.getAttribute(mac2, '-mac') valueListMv2 = ixNet.add(macAddrMv2, 'valueList') ixNet.execute('import', valueListMv2, ixNet.readFrom(csvPath1), "csv", '1') ixNet.commit() ################################################################################# # Adding IPv4 Layer ################################################################################# print("Add ipv4") ixNet.add(mac1, 'ipv4') ixNet.add(mac2, 'ipv4') ixNet.commit() ip1 = ixNet.getList(mac1, 'ipv4')[0] mvAdd1 = ixNet.getAttribute(ip1, '-address') mvIpAddValuelist1 = ixNet.add(mvAdd1, 'valueList') mvGw1 = ixNet.getAttribute(ip1, '-gatewayIp') mvGwAddValuelist1 = ixNet.add(mvGw1, 'valueList') ixNet.execute('import', mvIpAddValuelist1, ixNet.readFrom(csvPath1), "csv", '4') ixNet.execute('import', mvGwAddValuelist1, ixNet.readFrom(csvPath1), "csv", '5') ixNet.commit() ip2 = ixNet.getList(mac2, 'ipv4')[0] mvAdd2 = ixNet.getAttribute(ip2, '-address') mvIpAddValuelist2 = ixNet.add(mvAdd2, 'valueList') mvGw2 = ixNet.getAttribute(ip2, '-gatewayIp') mvGwAddValuelist2 = ixNet.add(mvGw2, 'valueList') ixNet.execute('import', mvIpAddValuelist2, ixNet.readFrom(csvPath1), "csv", '5') ixNet.execute('import', mvGwAddValuelist2, ixNet.readFrom(csvPath1), "csv", '4') ixNet.commit() ################################################################################# # Adding OSPFv2 ################################################################################# print("Adding OSPFv2") ixNet.add(ip1, 'ospfv2') ixNet.add(ip2, 'ospfv2') ixNet.commit() ospfv2Router1 = ixNet.getList(ip1, 'ospfv2')[0] ospfv2Router2 = ixNet.getList(ip2, 'ospfv2')[0] networkTypeMv1 = ixNet.getAttribute(ospfv2Router1, '-networkType') ixNet.setAttribute(networkTypeMv1 + '/singleValue', '-value', 'pointtopoint') ixNet.commit() networkTypeMv2 = ixNet.getAttribute(ospfv2Router2, '-networkType') ixNet.setAttribute(networkTypeMv2 + '/singleValue', '-value', 'pointtopoint') ixNet.commit() ################################################################################# # Generate boolean valuelist ################################################################################# myOneBitValue = overLay1Bit.OneBitValue(csvPath2, 10, 10) myOneBitValue.generate() activeBitMv = ixNet.getAttribute(ospfv2Router1, '-active') activeBitMvValueList = ixNet.add(activeBitMv, 'valueList') ixNet.execute('import', activeBitMvValueList, ixNet.readFrom(csvPath2), "csv", '0') ixNet.commit()