# -*- coding: cp1252 -*- ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF BFDv6 API # # It will create 2 BFDv4 topologies over VXLAN, it will start the emulation # # and than it will retrieve and display few statistics # # Module: # # The sample was tested on an XMVDC16 module. # # # ################################################################################ import os import sys import time def assignPorts (ixNet, realPort1, realPort2) : chassis1 = realPort1[0] chassis2 = realPort2[0] card1 = realPort1[1] card2 = realPort2[1] port1 = realPort1[2] port2 = realPort2[2] root = ixNet.getRoot() vport1 = ixNet.add(root, 'vport') ixNet.commit() vport1 = ixNet.remapIds(vport1)[0] vport2 = ixNet.add(root, 'vport') ixNet.commit() vport2 = ixNet.remapIds(vport2)[0] chassisObj1 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj1, '-hostname', chassis1) ixNet.commit() chassisObj1 = ixNet.remapIds(chassisObj1)[0] if (chassis1 != chassis2) : chassisObj2 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj2, '-hostname', chassis2) ixNet.commit() chassisObj2 = ixNet.remapIds(chassisObj2)[0] else : chassisObj2 = chassisObj1 # end if cardPortRef1 = chassisObj1 + '/card:%s/port:%s' % (card1,port1) ixNet.setMultiAttribute(vport1, '-connectedTo', cardPortRef1, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 001') ixNet.commit() cardPortRef2 = chassisObj2 + '/card:%s/port:%s' % (card2,port2) ixNet.setMultiAttribute(vport2, '-connectedTo', cardPortRef2, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 002') ixNet.commit() # end def assignPorts ################################################################################ # Either feed the ixNetwork library path in the sys.path as below, or put the # # IxNetwork.py file somewhere else where we python can autoload it # # "IxNetwork.py" is available in \API\Python # ################################################################################ ixNetPath = r'C:\Program Files (x86)\Ixia\IxNetwork\8.20.0.219-EB\API\Python' sys.path.append(ixNetPath) import IxNetwork ################################################################################# # Give chassis/client/ixNetwork server port/ chassis port HW port information # # below # ################################################################################# ixTclServer = '10.39.50.134' ixTclPort = '8100' ports = [('10.39.50.251', '7', '15',), ('10.39.50.251', '7', '16',)] # get IxNet class ixNet = IxNetwork.IxNet() print("connecting to IxNetwork client") ixNet.connect(ixTclServer, '-port', ixTclPort, '-version', '8.20', '-setAttribute', 'strict') # cleaning up the old configfile, and creating an empty config print("cleaning up the old configfile, and creating an empty config") ixNet.execute('newConfig') # assigning ports assignPorts(ixNet, ports[0], ports[1]) time.sleep(5) root = ixNet.getRoot() vportTx = ixNet.getList(root, 'vport')[0] vportRx = ixNet.getList(root, 'vport')[1] print("adding topologies") ixNet.add(root, 'topology', '-vports', vportTx) ixNet.add(root, 'topology', '-vports', vportRx) ixNet.commit() topologies = ixNet.getList(ixNet.getRoot(), 'topology') topo1 = topologies[0] topo2 = topologies[1] print ("Adding 2 device groups") ixNet.add(topo1, 'deviceGroup') ixNet.add(topo2, 'deviceGroup') ixNet.commit() t1devices = ixNet.getList(topo1, 'deviceGroup') t2devices = ixNet.getList(topo2, 'deviceGroup') t1dev1 = t1devices[0] t2dev1 = t2devices[0] print("Configuring the multipliers (number of sessions)") ixNet.setAttribute(t1dev1, '-multiplier', '1') ixNet.setAttribute(t2dev1, '-multiplier', '1') ixNet.commit() print("Adding ethernet/mac endpoints") ixNet.add(t1dev1, 'ethernet') ixNet.add(t2dev1, 'ethernet') ixNet.commit() mac1 = ixNet.getList(t1dev1, 'ethernet')[0] mac2 = ixNet.getList(t2dev1, 'ethernet')[0] print("Configuring the mac addresses %s" % (mac1)) ixNet.setMultiAttribute(ixNet.getAttribute(mac1, '-mac') + '/counter', '-direction', 'increment', '-start', '18:03:73:C7:6C:B1', '-step', '00:00:00:00:00:01') ixNet.setAttribute(ixNet.getAttribute(mac2, '-mac') + '/singleValue', '-value', '18:03:73:C7:6C:01') ixNet.commit() print ('ixNet.help(\'::ixNet::OBJ-/topology/deviceGroup/ethernet\')') print (ixNet.help('::ixNet::OBJ-/topology/deviceGroup/ethernet')) print("Add ipv4") ixNet.add(mac1, 'ipv4') ixNet.add(mac2, 'ipv4') ixNet.commit() ip1 = ixNet.getList(mac1, 'ipv4')[0] ip2 = ixNet.getList(mac2, 'ipv4')[0] mvAdd1 = ixNet.getAttribute(ip1, '-address') mvAdd2 = ixNet.getAttribute(ip2, '-address') mvGw1 = ixNet.getAttribute(ip1, '-gatewayIp') mvGw2 = ixNet.getAttribute(ip2, '-gatewayIp') print("configuring ipv4 addresses") ixNet.setAttribute(mvAdd1 + '/singleValue', '-value', '20.20.20.2') ixNet.setAttribute(mvAdd2 + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(mvGw1 + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(mvGw2 + '/singleValue', '-value', '20.20.20.2') ixNet.setAttribute(ixNet.getAttribute(ip1, '-prefix') + '/singleValue', '-value', '24') ixNet.setAttribute(ixNet.getAttribute(ip2, '-prefix') + '/singleValue', '-value', '24') ixNet.setMultiAttribute(ixNet.getAttribute(ip1, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.setMultiAttribute(ixNet.getAttribute(ip2, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.commit() print ('ixNet.help(\'::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4\')') print (ixNet.help('::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4')) ########################################################################### #Add and Configure VXLAN Interface ########################################################################### print("Adding BFDv4 and Configuring") ixNet.add(ip1, 'vxlan') ixNet.add(ip2, 'vxlan') ixNet.commit() vxlan1 = ixNet.getList(ip1, 'vxlan')[0] vxlan2 = ixNet.getList(ip2, 'vxlan')[0] vni2 = ixNet.getAttribute(vxlan2, '-vni') ipv4_multicast = ixNet.getAttribute(vxlan2, '-ipv4_multicast') ixNet.setAttribute(vni2 + '/singleValue', '-value', '1000') ixNet.setAttribute(ipv4_multicast + '/singleValue', '-value', '225.0.1.1') ########################################################################### #Add and Configure BFDv4 Interface ########################################################################### print("Adding BFDv4 and Configuring") ixNet.add(vxlan1, 'bfdv4Interface') ixNet.add(vxlan2, 'bfdv4Interface') ixNet.commit() bfdv41 = ixNet.getList(vxlan1, 'bfdv4Interface')[0] bfdv42 = ixNet.getList(vxlan2, 'bfdv4Interface')[0] bfdv4session1 = ixNet.getList(bfdv41, 'bfdv4Session')[0] bfdv4session2 = ixNet.getList(bfdv42, 'bfdv4Session')[0] remoteIP1 = ixNet.getAttribute(bfdv4session1, '-remoteIp4') remoteIP2 = ixNet.getAttribute(bfdv4session2, '-remoteIp4') remoteMac1 = ixNet.getAttribute(bfdv4session1, '-remoteMac') remoteMac2 = ixNet.getAttribute(bfdv4session2, '-remoteMac') ovsdb1 = ixNet.getAttribute(bfdv4session1, '-enableOVSDBCommunication') ovsdb2 = ixNet.getAttribute(bfdv4session2, '-enableOVSDBCommunication') ixNet.setAttribute(remoteIP1 + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(remoteIP2 + '/singleValue', '-value', '20.20.20.2') ixNet.setAttribute(remoteMac1 + '/singleValue', '-value', '18:03:73:C7:6C:01') ixNet.setAttribute(remoteMac2 + '/singleValue', '-value', '18:03:73:C7:6C:B1') ixNet.commit() txInterval1 = ixNet.getAttribute(bfdv41, '-txInterval') txInterval2 = ixNet.getAttribute(bfdv42, '-txInterval') minRxInterval1 = ixNet.getAttribute(bfdv41, '-minRxInterval') minRxInterval2 = ixNet.getAttribute(bfdv42, '-minRxInterval') ixNet.setAttribute(txInterval1 + '/singleValue', '-value', '2000') ixNet.setAttribute(txInterval2 + '/singleValue', '-value', '2000') ixNet.setAttribute(minRxInterval1 + '/singleValue', '-value', '2000') ixNet.setAttribute(minRxInterval2 + '/singleValue', '-value', '2000') ixNet.setAttribute(ovsdb1 + '/singleValue', '-value', 'false') ixNet.setAttribute(ovsdb2 + '/singleValue', '-value', 'false') ixNet.setAttribute(bfdv41, '-aggregateBfdSession', 'false') ixNet.setAttribute(bfdv42, '-aggregateBfdSession', 'false') ixNet.commit() print('ixNet.help(\'::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4/bfdv4Interface\')') print (ixNet.help('::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4/bfdv4Interface')) ################################################################################ # Start BFD protocol and wait for 45 seconds # ################################################################################ print("Starting protocols and waiting for 45 seconds for protocols to come up") ixNet.execute('startAllProtocols') time.sleep(45) ################################################################################ # Retrieve protocol statistics # ################################################################################ print ("Fetching all Protocol Summary Stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"Protocols Summary"/page' statcap = ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in ixNet.getAttribute(viewPage, '-rowValues') : for statVal in statValList : print("***************************************************") index = 0 for satIndv in statVal : print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 # end for # end for # end for ############################################################################ ##On The Fly Section ############################################################################ print("Deactivating and Activating BFDv4 Interface On the fly") activation = ixNet.getAttribute(bfdv41, '-active') ixNet.setAttribute(activation +'/singleValue', '-value', 'false') ixNet.commit() globalObj = ixNet.getRoot() + '/globals' topology = globalObj + '/topology' print ("Applying changes on the fly") try : ixNet.execute('applyOnTheFly', topology) except : print("error in applying on the fly change") time.sleep(10) ixNet.setAttribute(activation +'/singleValue', '-value', 'true') ixNet.commit() globalObj = ixNet.getRoot() + '/globals' topology = globalObj + '/topology' print ("Applying changes on the fly") try : ixNet.execute('applyOnTheFly', topology) except : print("error in applying on the fly change") # end try/expect time.sleep(10) ############################################################################### # Retrieve protocol learned info # ############################################################################### print("Fetching BFD learned info") ixNet.execute('getLearnedInfo', bfdv41, '1') time.sleep(5) linfo = ixNet.getList(bfdv41, 'learnedInfo')[0] values = ixNet.getAttribute(linfo, '-values') print("***************************************************") for v in values : print(v) # end for print("***************************************************") ################################################################################ # Stop all protocols # ################################################################################ print ('Stopping protocols') ixNet.execute('stopAllProtocols') print ('!!! Test Script Ends !!!')