# -*- coding: cp1252 -*- #!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF BGP EPE API # # It will create 2 BGP EPE topologies, it will start the emulation and # # than it will retrieve and display few statistics # ################################################################################ import os import sys import time def assignPorts (ixNet, realPort1, realPort2) : chassis1 = realPort1[0] chassis2 = realPort2[0] card1 = realPort1[1] card2 = realPort2[1] port1 = realPort1[2] port2 = realPort2[2] root = ixNet.getRoot() vport1 = ixNet.add(root, 'vport') ixNet.commit() vport1 = ixNet.remapIds(vport1)[0] vport2 = ixNet.add(root, 'vport') ixNet.commit() vport2 = ixNet.remapIds(vport2)[0] chassisObj1 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj1, '-hostname', chassis1) ixNet.commit() chassisObj1 = ixNet.remapIds(chassisObj1)[0] if (chassis1 != chassis2) : chassisObj2 = ixNet.add(root + '/availableHardware', 'chassis') ixNet.setAttribute(chassisObj2, '-hostname', chassis2) ixNet.commit() chassisObj2 = ixNet.remapIds(chassisObj2)[0] else : chassisObj2 = chassisObj1 # end if cardPortRef1 = chassisObj1 + '/card:%s/port:%s' % (card1,port1) ixNet.setMultiAttribute(vport1, '-connectedTo', cardPortRef1, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 001') ixNet.commit() cardPortRef2 = chassisObj2 + '/card:%s/port:%s' % (card2,port2) ixNet.setMultiAttribute(vport2, '-connectedTo', cardPortRef2, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 002') ixNet.commit() # end def assignPorts ################################################################################ # Either feed the ixNetwork library path in the sys.path as below, or put the # # IxNetwork.py file somewhere else where we python can autoload it # # "IxNetwork.py" is available in \API\Python # ################################################################################ ixNetPath = r'C:\Program Files (x86)\Ixia\IxNetwork\7.40-EA\API\Python' sys.path.append(ixNetPath) import IxNetwork ################################################################################# # Give chassis/client/ixNetwork server port/ chassis port HW port information # # below # ################################################################################# ixTclServer = '10.39.43.12' ixTclPort = '8072' ports = [('10.39.50.123', '5', '7',), ('10.39.50.123', '5', '8',)] # get IxNet class ixNet = IxNetwork.IxNet() print("connecting to IxNetwork client") ixNet.connect(ixTclServer, '-port', ixTclPort, '-version', '7.40', '-setAttribute', 'strict') # cleaning up the old configfile, and creating an empty config print("cleaning up the old configfile, and creating an empty config") ixNet.execute('newConfig') ################################################################################ # protocol configuration section # ################################################################################ assignPorts(ixNet, ports[0], ports[1]) time.sleep(5) root = ixNet.getRoot() vportTx = ixNet.getList(root, 'vport')[0] vportRx = ixNet.getList(root, 'vport')[1] print("adding topologies") ixNet.add(root, 'topology', '-vports', vportTx) ixNet.add(root, 'topology', '-vports', vportRx) ixNet.commit() topologies = ixNet.getList(ixNet.getRoot(), 'topology') topo1 = topologies[0] topo2 = topologies[1] print ("Adding 2 device groups") ixNet.add(topo1, 'deviceGroup') ixNet.add(topo2, 'deviceGroup') ixNet.commit() t1devices = ixNet.getList(topo1, 'deviceGroup') t2devices = ixNet.getList(topo2, 'deviceGroup') t1dev1 = t1devices[0] t2dev1 = t2devices[0] print("Configuring the multipliers (number of sessions)") ixNet.setAttribute(t1dev1, '-multiplier', '1') ixNet.setAttribute(t2dev1, '-multiplier', '1') ixNet.commit() print("Adding ethernet/mac endpoints") ixNet.add(t1dev1, 'ethernet') ixNet.add(t2dev1, 'ethernet') ixNet.commit() mac1 = ixNet.getList(t1dev1, 'ethernet')[0] mac2 = ixNet.getList(t2dev1, 'ethernet')[0] print("Configuring the mac addresses %s" % (mac1)) ixNet.setMultiAttribute(ixNet.getAttribute(mac1, '-mac') + '/counter', '-direction', 'increment', '-start', '18:03:73:C7:6C:B1', '-step', '00:00:00:00:00:01') ixNet.setAttribute(ixNet.getAttribute(mac2, '-mac') + '/singleValue', '-value', '18:03:73:C7:6C:01') ixNet.commit() print ('ixNet.help(\'::ixNet::OBJ-/topology/deviceGroup/ethernet\')') print("Adding IPv4 protocol stack") ixNet.add(mac1, 'ipv4') ixNet.add(mac2, 'ipv4') ixNet.commit() ip1 = ixNet.getList(mac1, 'ipv4')[0] ip2 = ixNet.getList(mac2, 'ipv4')[0] mvAdd1 = ixNet.getAttribute(ip1, '-address') mvAdd2 = ixNet.getAttribute(ip2, '-address') mvGw1 = ixNet.getAttribute(ip1, '-gatewayIp') mvGw2 = ixNet.getAttribute(ip2, '-gatewayIp') print("Configuring IPv4 addresses") ixNet.setAttribute(mvAdd1 + '/singleValue', '-value', '20.20.20.2') ixNet.setAttribute(mvAdd2 + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(mvGw1 + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(mvGw2 + '/singleValue', '-value', '20.20.20.2') ixNet.setAttribute(ixNet.getAttribute(ip1, '-prefix') + '/singleValue', '-value', '24') ixNet.setAttribute(ixNet.getAttribute(ip2, '-prefix') + '/singleValue', '-value', '24') ixNet.setMultiAttribute(ixNet.getAttribute(ip1, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.setMultiAttribute(ixNet.getAttribute(ip2, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.commit() print("Adding BGP protocol stack over IP4") ixNet.add(ip1, 'bgpIpv4Peer') ixNet.add(ip2, 'bgpIpv4Peer') ixNet.commit() bgp1 = ixNet.getList(ip1, 'bgpIpv4Peer')[0] bgp2 = ixNet.getList(ip2, 'bgpIpv4Peer')[0] print("Setting IPs in BGP DUT IP tab") ixNet.setAttribute(ixNet.getAttribute(bgp1, '-dutIp') + '/singleValue', '-value', '20.20.20.1') ixNet.setAttribute(ixNet.getAttribute(bgp2, '-dutIp') + '/singleValue', '-value', '20.20.20.2') ixNet.commit() print ("Enabling BGP Link State Non-VPN Capability") cap1 = ixNet.getAttribute(bgp1, '-capabilityLinkStateNonVpn') cap2 = ixNet.getAttribute(bgp2, '-capabilityLinkStateNonVpn') sv1 = ixNet.getList(cap1, 'singleValue')[0] sv2 = ixNet.getList(cap2, 'singleValue')[0] ixNet.setAttribute(sv1, '-value', 'true') ixNet.setAttribute(sv2, '-value', 'true') ixNet.commit() print ("Enabling BGP Filter Link State") filter1 = ixNet.getAttribute(bgp1, '-filterLinkState') filter2 = ixNet.getAttribute(bgp2, '-filterLinkState') sv1 = ixNet.getList(filter1, 'singleValue')[0] sv2 = ixNet.getList(filter2, 'singleValue')[0] ixNet.setAttribute(sv1, '-value', 'true') ixNet.setAttribute(sv2, '-value', 'true') ixNet.commit() print ("Enable BGP EPE in Topology 1") ixNet.setAttribute(bgp1, '-noOfEpePeers', '3') ixNet.commit() bgpEpePeerList = ixNet.getList(bgp1, 'bgpEpePeerList')[0] bgpEpePeerLinkList = ixNet.getList(bgpEpePeerList, 'bgpEpePeerLinkList')[0] print ("Setting Number of Links for BGP EPE to 2 in Topology 1") ixNet.setAttribute(bgpEpePeerList, '-noOflinks', '2') ixNet.commit() print ("Setting Number of EPE Peer Set to 3 in Topology 1") ixNet.setAttribute(bgpEpePeerList, '-noOfPeerSet', '2') ixNet.commit() print ("Selection of Peer Set Group") peerSetGroup = ixNet.getAttribute(bgpEpePeerList, '-peerSetGroup') ixNet.setMultiAttribute(peerSetGroup, '-clearOverlays', 'true') activeOverlay = ixNet.add(peerSetGroup, 'overlay') activeOverlay =ixNet.add(peerSetGroup, 'singleValue') ixNet.setMultiAttribute(activeOverlay, '-value', 'peersetgroup1 peersetgroup2') ixNet.commit() print ("Setting BGP Remote Router ID as DUT IP of BGP Peer") ixNet.setAttribute(ixNet.getAttribute(bgpEpePeerList, '-bgpRemoteRouterId') + '/singleValue', '-value', '20.20.20.1') ixNet.commit() print ("Setting EPE Peer Links Peer-Adj-SID to True") ixNet.setAttribute(ixNet.getAttribute(bgpEpePeerLinkList, '-enablePeerAdjSid') + '/singleValue', '-value', 'True') ixNet.commit() print ("Setting EPE Peer Links Remote IPv4 Link Address") ixNet.setAttribute(ixNet.getAttribute(bgpEpePeerLinkList, '-remoteIpv4LinkAddress') + '/singleValue', '-value', '20.20.20.1') ixNet.commit() bgpLocalIp = ixNet.getAttribute(bgp1, '-localIpv4Ver2') print ("Setting EPE Peer Links Local IPv4 Link Address") ixNet.setAttribute(ixNet.getAttribute(bgpEpePeerLinkList, '-localIpv4LinkAddress') + '/singleValue', '-value', bgpLocalIp) ixNet.commit() print("Adding OSPFv2 over IP4 stacks") ospf1 = ixNet.add(ip1, 'ospfv2') ospf2 = ixNet.add(ip2, 'ospfv2') ixNet.commit() print("Changing OSPFv2 Network Type") networkTypeMultiValue1 = ixNet.getAttribute(ospf1, '-networkType') ixNet.setAttribute(ixNet.getAttribute(ospf1, '-networkType') + '/singleValue', '-value', 'pointtopoint') ixNet.commit() print("Changing OSPFv2 Network Type") networkTypeMultiValue1 = ixNet.getAttribute(ospf2, '-networkType') ixNet.setAttribute(ixNet.getAttribute(ospf2, '-networkType') + '/singleValue', '-value', 'pointtopoint') ixNet.commit() print("Renaming the topologies and the device groups") ixNet.setAttribute(topo1, '-name', 'BGP Topology 1') ixNet.setAttribute(topo2, '-name', 'BGP Topology 2') ixNet.setAttribute(t1dev1, '-name', 'BGP Topology 1 Router') ixNet.setAttribute(t2dev1, '-name', 'BGP Topology 2 Router') ixNet.commit() ################################################################################ # Start protocol and check statistics # ################################################################################ print("Starting protocols and waiting for 45 seconds for protocols to come up") ixNet.execute('startAllProtocols') time.sleep(45) print ("Fetching all Protocol Summary Stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"Protocols Summary"/page' statcap = ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in ixNet.getAttribute(viewPage, '-rowValues') : for statVal in statValList : print("***************************************************") index = 0 for satIndv in statVal : print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 # end for # end for # end for print("***************************************************") print ("Verifying BGP Peer related stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"BGP Peer Per Port"/page' statcap = ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in ixNet.getAttribute(viewPage, '-rowValues') : for statVal in statValList : print("***************************************************") index = 0 for satIndv in statVal : print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 # end for # end for # end for print("***************************************************") ############################################################################### # print learned info # ############################################################################### ixNet.execute('getLinkStateLearnedInfo', bgp2, '1') time.sleep(5) linfo = ixNet.getList(bgp2, 'learnedInfo')[0] linfoList = ixNet.getList(linfo, 'table') print("***************************************************") for table in linfoList : tableType = ixNet.getAttribute(table, '-type') print(tableType) print("=================================================") columns = ixNet.getAttribute(table, '-columns') print(columns) values = ixNet.getAttribute(table, '-values') for value in values : for word in values : print(word) #end for # end for # end for time.sleep(15) print ('Stopping protocols') ixNet.execute('stopAllProtocols') print ('!!! Test Script Ends !!!')