# -*- coding: cp1252 -*- #!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF OpenFlow Controller API# # It will create 1 topology of OpenFlow Controller, it will start the # emulation and then it will retrieve and display few statistics # It will also check detailed learned info and learned info after sending on# # demand message # ################################################################################ import sys import time ################################################################################ # Either feed the ixNetwork library path in the sys.path as below, or put the # # IxNetwork.py file somewhere else where we python can autoload it # # "IxNetwork.py" is available in \API\Python # ################################################################################ sys.path.append('C:\Program Files (x86)\Ixia\IxNetwork\8.10-EA\API\Python') import IxNetwork print("loaded successfully") #from lib import IxNetwork #import time class NgpfOpenFlowSwitch(object): ################################################################################ # Connecting to IxTCl server and cretaing new config # ################################################################################ def __init__(self, ix_tcl_server, ix_tcl_port, ix_version="8.10"): ixNet = IxNetwork.IxNet() print("connecting to IxNetwork client") ixNet.connect(ix_tcl_server, '-port', ix_tcl_port, '-version', ix_version, '-setAttribute', 'strict') # cleaning up the old configfile, and creating an empty config print("cleaning up the old configfile, and creating an empty config") ixNet.execute('newConfig') self.ixNet = ixNet self.root = ixNet.getRoot() def assignPorts(self, realPort1): chassis1 = realPort1[0] card1 = realPort1[1] port1 = realPort1[2] root = self.ixNet.getRoot() vport1 = self.ixNet.add(root, 'vport') self.ixNet.commit() vport1 = self.ixNet.remapIds(vport1)[0] chassisObj1 = self.ixNet.add(root + '/availableHardware', 'chassis') self.ixNet.setAttribute(chassisObj1, '-hostname', chassis1) self.ixNet.commit() chassisObj1 = self.ixNet.remapIds(chassisObj1)[0] cardPortRef1 = chassisObj1 + '/card:%s/port:%s' % (card1, port1) self.ixNet.setMultiAttribute(vport1, '-connectedTo', cardPortRef1, '-rxMode', 'captureAndMeasure', '-name', 'Ethernet - 001') self.ixNet.commit() ################################################################################ # Start protocol and check statistics # ################################################################################ def start_protocol_check_stats(self): print("Starting protocols and waiting for 45 seconds for protocols to come up") self.ixNet.execute('startAllProtocols') time.sleep(45) print ("Fetching all Protocol Summary Stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"Protocols Summary"/page' statcap = self.ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in self.ixNet.getAttribute(viewPage, '-rowValues'): for statVal in statValList: print("***************************************************") index = 0 for satIndv in statVal: print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 print("***************************************************") print ("Verifying OpenFlow Switch Per Port stats\n") viewPage = '::ixNet::OBJ-/statistics/view:"OF Switch Per Port"/page' statcap = self.ixNet.getAttribute(viewPage, '-columnCaptions') for statValList in self.ixNet.getAttribute(viewPage, '-rowValues'): for statVal in statValList: print("***************************************************") index = 0 for satIndv in statVal: print("%-30s:%s" % (statcap[index], satIndv)) index = index + 1 print("***************************************************") def on_the_fly(self, switch_disable_enable): for i in switch_disable_enable: ofSwitchActive = self.ixNet.getAttribute(switch_disable_enable, '-active') swActive = self.ixNet.add(ofSwitchActive, 'overlay') self.ixNet.setMultiAttribute(swActive, '-value', 'false') self.ixNet.commit() globalObj = self.ixNet.getRoot() + '/globals' topology = globalObj + '/topology' print ("Applying changes on the fly") try: self.ixNet.execute('applyOnTheFly', topology) except: print("error in applying on the fly change") time.sleep(10) for i in switch_disable_enable: ofSwitchActive = self.ixNet.getAttribute(switch_disable_enable, '-active') swActive = self.ixNet.add(ofSwitchActive, 'overlay') self.ixNet.setMultiAttribute(swActive, '-value', 'true') self.ixNet.commit() globalObj = self.ixNet.getRoot() + '/globals' topology = globalObj + '/topology' print ("Applying changes on the fly") try: self.ixNet.execute('applyOnTheFly', topology) except: print("error in applying on the fly change") time.sleep(10) def on_the_fly_port_number_ethernetaddress(self, sw_port): EthernetDestVal = self.ixNet.getAttribute(sw_port, '-etherAddr') print (EthernetDestVal) val = self.ixNet.getAttribute(EthernetDestVal, '-values')[0] print (val) self.ixNet.setMultiAttribute(EthernetDestVal, '-clearOverlays', 'false') self.ixNet.commit() EthernetDestValues = self.ixNet.add(EthernetDestVal, 'singleValue') self.ixNet.setMultiAttribute(EthernetDestValues, '-value', '56:00:00:00:00:1') self.ixNet.commit() time.sleep(20) PortVal = self.ixNet.getAttribute(sw_port, '-portNumber') self.ixNet.setMultiAttribute(PortVal, '-clearOverlays', 'false') self.ixNet.commit() PortSetValues = self.ixNet.add(PortVal, 'singleValue') self.ixNet.setMultiAttribute(PortSetValues, '-value', '5677888') self.ixNet.commit() globalObj = self.ixNet.getRoot() + '/globals' topology = globalObj + '/topology' print ("Applying changes on the fly") try: self.ixNet.execute('applyOnTheFly', topology) except: print("error in applying on the fly change") time.sleep(10) ############################################################################### # print learned info # ############################################################################### def print_learned_info(self, openFlowSwitch): self.ixNet.execute('getOFChannelLearnedInfo', openFlowSwitch, '1') time.sleep(5) print("Print OFSwitch Learned Info") linfo = self.ixNet.getList(openFlowSwitch, 'learnedInfo')[0] linfoList = self.ixNet.getList(linfo, 'table') print("***************************************************") for table in linfoList: tableType = self.ixNet.getAttribute(table, '-type') print(tableType) print("=================================================") columns = self.ixNet.getAttribute(table, '-columns') print(columns) values = self.ixNet.getAttribute(table, '-values') for value in values: for word in values: print(word) time.sleep(15) self.ixNet.execute('getOFSwitchFlowStatLearnedInfo', openFlowSwitch, '1') time.sleep(5) print ("Print OFswitch Flow Learned info") linfo = self.ixNet.getList(openFlowSwitch, 'learnedInfo')[0] linfoList = self.ixNet.getList(linfo, 'table') print("***************************************************") for table in linfoList: tableType = self.ixNet.getAttribute(table, '-type') print(tableType) print("=================================================") columns = self.ixNet.getAttribute(table, '-columns') print(columns) values = self.ixNet.getAttribute(table, '-values') for value in values: for word in values: print(word) time.sleep(15) print ('Stopping protocols') self.ixNet.execute('stopAllProtocols') ################################################################################ # protocol configuration section # ################################################################################ def main(self): self.assignPorts(ports[0]) root = self.ixNet.getRoot() vportTx = self.ixNet.getList(root, 'vport')[0] print("adding topologies") self.ixNet.add(root, 'topology', '-vports', vportTx) self.ixNet.commit() topologies = self.ixNet.getList(self.ixNet.getRoot(), 'topology') topo1 = topologies[0] print ("Adding 2 device groups") deviceGroup1 = self.ixNet.add(topo1, 'deviceGroup') self.ixNet.commit() t1devices = self.ixNet.getList(topo1, 'deviceGroup') t1dev1 = t1devices[0] print("Configuring the multipliers (number of sessions)") self.ixNet.setAttribute(t1dev1, '-multiplier', '1') self.ixNet.commit() print("Adding ethernet/mac endpoints") self.ixNet.add(t1dev1, 'ethernet') self.ixNet.commit() mac1 = self.ixNet.getList(t1dev1, 'ethernet')[0] print ('ixNet.help(\'::ixNet::OBJ-/topology/deviceGroup/ethernet\')') print("Add ipv4") self.ixNet.add(mac1, 'ipv4') self.ixNet.commit() ip1 = self.ixNet.getList(mac1, 'ipv4')[0] mvAdd1 = self.ixNet.getAttribute(ip1, '-address') mvGw1 = self.ixNet.getAttribute(ip1, '-gatewayIp') print("configuring ipv4 addresses") self.ixNet.setAttribute(mvAdd1 + '/singleValue', '-value', '1.1.1.2') self.ixNet.commit() self.ixNet.setAttribute(mvGw1 + '/singleValue', '-value', '1.1.1.1') self.ixNet.commit() self.ixNet.setAttribute(self.ixNet.getAttribute(ip1, '-prefix') + '/singleValue', '-value', '24') self.ixNet.commit() self.ixNet.setMultiAttribute(self.ixNet.getAttribute(ip1, '-resolveGateway') + '/singleValue', '-value', 'true') self.ixNet.commit() time.sleep(5) print (self.ixNet.help('::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4')) print("Adding Openflow Switch over IP4 stacks") self.ixNet.add(ip1, 'openFlowSwitch') self.ixNet.commit() openFlowSwitch1 = self.ixNet.getList(ip1, 'openFlowSwitch')[0] print (openFlowSwitch1) time.sleep(5) openflowSwitchchannels = self.ixNet.add(openFlowSwitch1, 'OFSwitchChannel') self.ixNet.commit() time.sleep(5) openflowchannellist = self.ixNet.getList(openFlowSwitch1, 'OFSwitchChannel')[0] self.ixNet.setMultiAttribute(openflowSwitchchannels, '-auxConnectionsPerChannel', '1') self.ixNet.commit() time.sleep(5) #openflowTablelist = self.ixNet.getList(ip1, 'switchTablesList')[0] self.ixNet.setMultiAttribute(openFlowSwitch1, '-numberOfTableRanges', '3') self.ixNet.commit() time.sleep(5) switchTableList = self.ixNet.getList(openFlowSwitch1, 'switchTablesList')[0] print (switchTableList) networkTopologyObj = self.ixNet.add(deviceGroup1, 'networkTopology') self.ixNet.commit() networkTopologyObjRing = self.ixNet.add(networkTopologyObj, 'netTopologyRing') self.ixNet.commit() self.start_protocol_check_stats() swtopology = self.ixNet.getList(self.ixNet.getRoot(), 'topology')[0] print (swtopology) deviceGroupSW = self.ixNet.getList(swtopology, 'deviceGroup')[0] ethernetSw = self.ixNet.getList(deviceGroupSW, 'ethernet')[0] ipv4Sw = self.ixNet.getList(ethernetSw, 'ipv4')[0] ofSw = self.ixNet.getList(ipv4Sw, 'openFlowSwitch')[0] print ("Now disable/Enable of switch on the fly") self.on_the_fly(ofSw) print ("Changing Ethernet Address, Port number on the fly!!!!!") swPortActive = self.ixNet.getList(ofSw, 'ofSwitchPorts')[0] print (swPortActive) self.on_the_fly_port_number_ethernetaddress(swPortActive) print ("Fetching Switch Learned info !!!!!") self.print_learned_info(ofSw) print ('!!! Test Script Ends !!!') ################################################################################# # Give chassis/client/ixNetwork server port/ chassis port HW port information # # below # ################################################################################# if __name__ == "__main__": ixTclServer = '10.214.101.141' ixTclPort = '8558' ports = [('12.0.1.253', '5', '10',)] version = '8.10' switch = NgpfOpenFlowSwitch(ixTclServer, ixTclPort, version) switch.main()